MCUXpresso SDK Documentation

ZPS_tsAfZdpEvent

ZPS_tsAfZdpEvent#

This structure is used when a ZPS_EVENT_APS_DATA_INDICATION event is generated containing a response which is destined for the ZDO at endpoint 0. The application can extract the response data from the event using the function ZPS_bAplZdpUnpackResponse() and this structure is used to receive the extracted data.

The ZPS_tsAfZdpEventstructure is detailed below.

typedef struct {
    uint8 u8SequNumber;
    uint16 u16ClusterId;
    union {
        ZPS_tsAplZdpDeviceAnnceReq sDeviceAnnce;
        ZPS_tsAplZdpMgmtNwkUpdateReq sMgmtNwkUpdateReq;
        ZPS_tsAplZdpMgmtPermitJoiningReq sPermitJoiningReq;
        ZPS_tsAplZdpDiscoveryCacheRsp sDiscoveryCacheRsp;
        ZPS_tsAplZdpDiscoveryStoreRsp sDiscoveryStoreRsp;
        ZPS_tsAplZdpNodeDescStoreRsp sNodeDescStoreRsp;
        ZPS_tsAplZdpActiveEpStoreRsp sActiveEpStoreRsp;
        ZPS_tsAplZdpSimpleDescStoreRsp sSimpleDescStoreRsp;
        ZPS_tsAplZdpRemoveNodeCacheRsp sRemoveNodeCacheRsp;
        ZPS_tsAplZdpEndDeviceBindRsp sEndDeviceBindRsp;
        ZPS_tsAplZdpBindRsp sBindRsp;
        ZPS_tsAplZdpUnbindRsp sUnbindRsp;
        ZPS_tsAplZdpReplaceDeviceRsp sReplaceDeviceRsp;
        ZPS_tsAplZdpStoreBkupBindEntryRsp sStoreBkupBindEntryRsp;
        ZPS_tsAplZdpRemoveBkupBindEntryRsp sRemoveBkupBindEntryRsp;
        ZPS_tsAplZdpBackupSourceBindRsp sBackupSourceBindRsp;
        ZPS_tsAplZdpMgmtLeaveRsp sMgmtLeaveRsp;
        ZPS_tsAplZdpMgmtDirectJoinRsp sMgmtDirectJoinRsp;
        ZPS_tsAplZdpMgmtPermitJoiningRsp sPermitJoiningRsp;
        ZPS_tsAplZdpNodeDescRsp sNodeDescRsp;
        ZPS_tsAplZdpPowerDescRsp sPowerDescRsp;
        ZPS_tsAplZdpSimpleDescRsp sSimpleDescRsp;
        ZPS_tsAplZdpNwkAddrRsp sNwkAddrRsp;
        ZPS_tsAplZdpIeeeAddrRsp sIeeeAddrRsp;
        ZPS_tsAplZdpUserDescConf sUserDescConf;
        ZPS_tsAplZdpSystemServerDiscoveryRsp sSystemServerDiscoveryRsp;
        ZPS_tsAplZdpPowerDescStoreRsp sPowerDescStoreRsp;
        ZPS_tsAplZdpUserDescRsp sUserDescRsp;
        ZPS_tsAplZdpActiveEpRsp sActiveEpRsp;
        ZPS_tsAplZdpMatchDescRsp sMatchDescRsp;
        ZPS_tsAplZdpComplexDescRsp sComplexDescRsp;
        ZPS_tsAplZdpFindNodeCacheRsp sFindNodeCacheRsp;
        ZPS_tsAplZdpExtendedSimpleDescRsp sExtendedSimpleDescRsp;
        ZPS_tsAplZdpExtendedActiveEpRsp sExtendedActiveEpRsp;
        ZPS_tsAplZdpBindRegisterRsp sBindRegisterRsp;
        ZPS_tsAplZdpBackupBindTableRsp sBackupBindTableRsp;
        ZPS_tsAplZdpRecoverBindTableRsp sRecoverBindTableRsp;
        ZPS_tsAplZdpRecoverSourceBindRsp sRecoverSourceBindRsp;
        ZPS_tsAplZdpMgmtNwkDiscRsp sMgmtNwkDiscRsp;
        ZPS_tsAplZdpMgmtLqiRsp sMgmtLqiRsp;
        ZPS_tsAplZdpMgmtRtgRsp sRtgRsp;
        ZPS_tsAplZdpMgmtBindRsp sMgmtBindRsp;
        ZPS_tsAplZdpMgmtCacheRsp sMgmtCacheRsp;
        ZPS_tsAplZdpMgmtNwkUpdateNotify sMgmtNwkUpdateNotify;
    }uZdpData;
    union {
        ZPS_tsAplZdpBindingTableEntry asBindingTable[5];
        ZPS_tsAplZdpNetworkDescr asNwkDescTable[5];
        ZPS_tsAplZdpNtListEntry asNtList[2];
        ZPS_tsAplDiscoveryCache aDiscCache[5];
        uint16 au16Data[34];
        uint8 au8Data[77];
        uint64 au64Data[9];
    }uLists;
}ZPS_tsAfZdpEvent;

where:

  • u8SequNumberis the sequence number of the ZDP request/response

  • u16ClusterIdis the ID of the cluster to which the request/response relates

  • uZdpDatais a union of the different ZDP request/response types:

    • sDeviceAnnceis a structure of the type ZPS_tsAplZdpDeviceAnnceReq, described in Section 9.2.2.3

  • sMgmtNwkUpdateReqis a structure of the type ZPS_tsAplZdpMgmtNwkUpdateReq, described in Section 9.2.2.41

  • sPermitJoiningReqis a structure of the type ZPS_tsAplZdpMgmtPermitJoiningReq, described in Section 9.2.3.39

  • sDiscoveryCacheRspis a structure of the type ZPS_tsAplZdpDiscoveryCacheRsp, described in Section 9.2.3.14

  • sDiscoveryStoreRspis a structure of the type ZPS_tsAplZdpDiscoveryStoreRsp, described in Section 9.2.3.15

  • sNodeDescStoreRspis a structure of the type ZPS_tsAplZdpNodeDescStoreRsp, described in Section 9.2.3.16

  • sActiveEpStoreRspis a structure of the type ZPS_tsAplZdpActiveEpStoreRsp, described in Section 9.2.3.19

  • sSimpleDescStoreRspis a structure of the type ZPS_tsAplZdpSimpleDescStoreRsp, described in Section 9.2.3.18

  • sRemoveNodeCacheRspis a structure of the type ZPS_tsAplZdpRemoveNodeCacheRsp, described in Section 9.2.3.21

  • sEndDeviceBindRspis a structure of the type ZPS_tsAplZdpEndDeviceBindRsp, described in Section 9.2.3.22

  • sBindRspis a structure of the type ZPS_tsAplZdpBindRsp, described in Section 9.2.3.23

  • sUnbindRspis a structure of the type ZPS_tsAplZdpUnbindRsp, described in Section 9.2.3.24

  • sReplaceDeviceRspis a structure of the type ZPS_tsAplZdpReplaceDeviceRsp, described in Section 9.2.3.26

  • sStoreBkupBindEntryRspis a structure of the type ZPS_tsAplZdpStoreBkupBindEntryRsp, described in Section9.2.2.27

  • sRemoveBkupBindEntryRspis a structure of the type ZPS_tsAplZdpRemoveBkupBindEntryRsp, described in Section9.2.2.28

  • sBackupSourceBindRspis a structure of the type ZPS_tsAplZdpBackupSourceBindRsp, described in Section 9.2.3.31

  • sMgmtLeaveRspis a structure of the type ZPS_tsAplZdpMgmtLeaveRsp, described in Section 9.2.3.37

  • sMgmtDirectJoinRspis a structure of the type ZPS_tsAplZdpMgmtDirectJoinRsp, described in Section 9.2.3.38

  • sPermitJoiningRspis a structure of the type ZPS_tsAplZdpMgmtPermitJoiningRsp, described in Section 9.2.3.39

  • sNodeDescRspis a structure of the type ZPS_tsAplZdpNodeDescRsp, described in Section 8.2.3.3

  • sPowerDescRspis a structure of the type ZPS_tsAplZdpPowerDescRsp, described in Section 9.2.3.4

  • sSimpleDescRspis a structure of the type ZPS_tsAplZdpSimpleDescRsp, described in Section 9.2.3.5

  • sNwkAddrRspis a structure of the type ZPS_tsAplZdpNwkAddrRsp, described in Section 9.2.3.1

  • sIeeeAddrRspis a structure of the type ZPS_tsAplZdpIeeeAddrRsp, described in Section 9.2.3.2

  • sUserDescConfis a structure of the type ZPS_tsAplZdpUserDescConf, described in Section 9.2.3.12

  • sSystemServerDiscoveryRspis a structure of the type ZPS_tsAplZdpSystemServerDiscoveryRsp, described in Section9.2.3.13

  • sPowerDescStoreRspis a structure of the type ZPS_tsAplZdpPowerDescStoreRsp, described in Section 9.2.3.17

  • sUserDescRspis a structure of the type ZPS_tsAplZdpUserDescRsp, described in Section 9.2.3.8

  • sActiveEpRspis a structure of the type ZPS_tsAplZdpActiveEpRsp, described in Section 9.2.3.10

  • sMatchDescRspis a structure of the type ZPS_tsAplZdpMatchDescRsp, described in Section 9.2.3.9

  • sComplexDescRspis a structure of the type ZPS_tsAplZdpComplexDescRsp, described in Section 9.2.3.7

  • sFindNodeCacheRspis a structure of the type ZPS_tsAplZdpFindNodeCacheRsp, described in Section 9.2.3.20

  • sExtendedSimpleDescRspis a structure of the type ZPS_tsAplZdpExtendedSimpleDescRsp, described in Section 9.2.3.6

  • sExtendedActiveEpRspis a structure of the type ZPS_tsAplZdpExtendedActiveEpRsp, described in Section 9.2.3.11

  • sBindRegisterRspis a structure of the type ZPS_tsAplZdpBindRegisterRsp, described in Section 9.2.3.25

  • sBackupBindTableRspis a structure of the type ZPS_tsAplZdpBackupBindTableRsp, described in Section 9.2.3.29

  • sRecoverBindTableRspis a structure of the type ZPS_tsAplZdpRecoverBindTableRsp, described in Section 9.2.3.30

  • sRecoverSourceBindRspis a structure of the type ZPS_tsAplZdpRecoverSourceBindRsp, described in Section 9.2.3.32

  • sMgmtNwkDiscRspis a structure of the type ZPS_tsAplZdpMgmtNwkDiscRsp, described in Section 9.2.3.33

  • sMgmtLqiRspis a structure of the type ZPS_tsAplZdpMgmtLqiRsp, described in Section 9.2.3.34

  • sRtgRspis a structure of the type ZPS_tsAplZdpMgmtRtgRsp, described in Section 9.2.3.35

  • sMgmtBindRspis a structure of the type ZPS_tsAplZdpMgmtBindRsp, described in Section 9.2.3.36

  • sMgmtCacheRspis a structure of the type ZPS_tsAplZdpMgmtCacheRsp, described in Section 9.2.3.40

  • sMgmtNwkUpdateNotifyis a structure of the type ZPS_tsAplZdpMgmtNwkUpdateNotify, described in Section 9.2.3.41

  • uListsis a union of the different arrays/tables which act as temporary storage for data elements used by the stack (and are therefore for internal use only)

Parent topic:Event structures