ezhv_linear2tiledYUV#
Overview#
This project shows how to use EZHV to convert linear YUV to tiled YUV.
Supported Boards#
MIMXRT700-EVK
Hardware requirements
Micro USB cable
MIMXRT700-EVK board
Personal Computer
RK055AHD091 MIPI panel (Not necessary if use other panel)
RK055MHD091 MIPI panel (Not necessary if use other panel)
Board settings
To use MIPI panel: Connect MIPI panel to J52.
Prepare the Demo
The demo use MIPI RK055MHD091 panel by default, to use MIPI RK055AHD091 panel, change the macro DEMO_PANEL to DEMO_PANEL_RK055AHD091 in mcux_config.h.
Connect a micro USB cable between the PC host and the USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs, you can see the decoded jpeg image is displayed on the
panel of RK055AHD091 or RK055MHD091.
JPEG decode and EZHV linear2tile conversion demo start.
FRDM-IMXRT700
Hardware requirements
Type-C USB cable
FRDM-IMXRT700 board
Personal Computer
RaspberryPi Panel
Board settings
To use Raspberry panel: Connect the panel to J8. Then connect the panel’s 5V pin to JP43-1, GND pin to JP43-2.
Prepare the Demo
The demo use MIPI Raspberry panel by default.
Connect a USB cable between the PC host and the USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs, you can see the decoded jpeg image is displayed on the
panel.
JPEG decode and EZHV linear2tile conversion demo start.