ZPS_tsAplZdpSimpleDescStoreRsp#
This structure is used to store Power_Desc_store_rsp message data - a response to a call to the function ZPS_eAplZdpSimpleDescStoreRequest(). This response indicates whether the sending node has successfully stored the received Simple descriptor in its primary discovery cache.
The ZPS_tsAplZdpSimpleDescStoreRspstructure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAplZdpSimpleDescStoreRsp;
where u8Statusis the return status for ZPS_eAplZdpSimpleDescStoreRequest().
Parent topic:ZDP response structures