ZPS_tsAplZdpReplaceDeviceRsp
This structure is used to store Replace_Device_rsp message data - a response to a call to the function ZPS_eAplZdpReplaceDeviceRequest(). This response indicates the status of the replace request.
The ZPS_tsAplZdpReplaceDeviceRspstructure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAplZdpReplaceDeviceRsp;
where u8Statusis the return status for ZPS_eAplZdpReplaceDeviceRequest().
Parent topic:ZDP response structures