MCUXpresso SDK Documentation

IMX943EVK#

Note:

IMX943EVK includes IMX943-19X19-LPDDR5-EVK, IMX943-19X19-LPDDR4-EVK, IMX943-15X15-LPDDR4-EVK

IMX943 19x19 LPDDR5 EVK(IMX943LP5EVK-19) = IMX943LP5CPU-19 SOM + X-IMX943BB

IMX943 19x19 LPDDR4 EVK(IMX943LP4EVK-19) = IMX943LP4CPU-19 SOM + X-IMX943BB

IMX943 15x15 LPDDR4 EVK(IMX943LP4EVK-15) = IMX943LP4CPU-15 SOM + X-IMX943BB

Overview#

IMX943EVK

MCU device and part on board is shown below:

  • Device: MIMX94398

  • PartNumber: MIMX94398AVKM, MIMX94398AVMM

  • Note: - IMX943LP5CPU-19 SOM and IMX943LP4CPU-19 SOM boards are using the PartNumber MIMX94398AVKM - IMX943LP4CPU-15 SOM board is using the PartNumber MIMX94398AVMM

SDK Introduction#

For an introduction to the MCUXpresso SDK, see MCUXpresso Software Development Kit (SDK).

Getting Started with MCUXpresso SDK Package#

Getting Started with MCUXpresso SDK GitHub#

Release Notes#

ChangeLog#

Driver API Reference Manual#

This section provides a link to the Driver API RM, detailing available drivers and their usage to help you integrate hardware efficiently.

MIMX94398_drivers

Middleware Documentation#

Find links to detailed middleware documentation for key components. While not all onboard middleware is covered, this serves as a useful reference for configuration and development.

Multicore#

Multicore SDK

FreeMASTER#

freemaster

FreeRTOS#

FreeRTOS

lwIP#

lwIP