sram_controller#
Overview#
The sram_controller example shows how to use SRAMC driver to initialize the SRAMC module.
Supported Boards#
FRDM-IMXRT1186
Hardware requirements
Type-C USB cable
FRDM-IMXRT1186 board
Personal Computer
Board settings
Rework the board to change the connection of the 3 PIN 0402 JUMPER:
R100: Connect to SRAMC_DAT00
R373: Connect to SRAMC_DAT01
R112: Connect to SRAMC_DAT02
R334: Connect to SRAMC_DAT03
R321: Connect to SRAMC_DAT04
R138: Connect to SRAMC_DAT05
R318: Connect to SRAMC_DAT06
R303: Connect to SRAMC_DAT07
R322: Connect to SRAMC_WE
R328: Connect to SRAMC_OEB
R391: Connect to SRAMC_ADV
R178: Connect to SRAMC_CS0
Connect FRDM-IMXRT1186 board 1(SRAM controller) to FRDM-IMXRT1186 board 2(SRAM emulator) as the list:
Pad (board 1)
SRAMC Signal (board 1)
Header (board 1)
EVK Header (board 2)
Pad (board 2)
FlexIO Pin (board 2)
GPIO_EMC_B1_00
SRAMC_D0
J61.pin3
J61.pin3
GPIO_EMC_B1_00
FLEXIO1_FLEXIO00
GPIO_EMC_B1_01
SRAMC_D1
J61.pin4
J61.pin4
GPIO_EMC_B1_01
FLEXIO1_FLEXIO01
GPIO_EMC_B1_02
SRAMC_D2
J61.pin5
J61.pin5
GPIO_EMC_B1_02
FLEXIO1_FLEXIO02
GPIO_EMC_B1_03
SRAMC_D3
J61.pin6
J61.pin6
GPIO_EMC_B1_03
FLEXIO1_FLEXIO03
GPIO_EMC_B1_04
SRAMC_D4
J61.pin7
J61.pin7
GPIO_EMC_B1_04
FLEXIO1_FLEXIO04
GPIO_EMC_B1_05
SRAMC_D5
J61.pin8
J61.pin8
GPIO_EMC_B1_05
FLEXIO1_FLEXIO05
GPIO_EMC_B1_06
SRAMC_D6
J61.pin9
J61.pin9
GPIO_EMC_B1_06
FLEXIO1_FLEXIO06
GPIO_EMC_B1_07
SRAMC_D7
J61.pin10
J61.pin10
GPIO_EMC_B1_07
FLEXIO1_FLEXIO07
GPIO_EMC_B1_26
SRAMC_WE
J61.pin42
J61.pin30
GPIO_EMC_B1_16
FLEXIO1_FLEXIO16
GPIO_EMC_B1_27
SRAMC_OE_B
J61.pin44
J61.pin31
GPIO_EMC_B1_17
FLEXIO1_FLEXIO17
GPIO_EMC_B1_28
SRAMC_ADV
J61.pin41
J61.pin32
GPIO_EMC_B1_18
FLEXIO1_FLEXIO18
GPIO_EMC_B1_29
SRAMC_CS0
J61.pin43
J61.pin34
GPIO_EMC_B1_19
FLEXIO1_FLEXIO19
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
SRAMC Example Start!
Preparing write data...
Writing 256 bytes (8-bit access) to SRAM at 0x43880000...
Write complete.
Reading 256 bytes (8-bit access) from SRAM at 0x43880000...
Read complete.
Comparing written and read data...
SRAMC De-initialized.
--- SRAM Read/Write Test Passed ---