prince#
Overview#
This driver example demonstrates how to setup PRINCE driver for the on-the-fly encryption/decryption of data stored in the internal flash memory. It shows how to enable encryption/decryption for specified flash memory address range, how to generate new IV code and how to load the IV code into the PRINCE bus encryption engine. The example also shows how to correctly perform PRINCE region erase and write operations with dummy data.