MCUXpresso SDK Documentation

MCUXpresso SDK Release Notes#

Overview#

The MCUXpresso SDK is a comprehensive software enablement package designed to simplify and accelerate application development with Arm Cortex-M-based devices from NXP, including its general purpose, crossover and Bluetooth-enabled MCUs. MCUXpresso SW and Tools for DSC further extends the SDK support to current 32-bit Digital Signal Controllers. The MCUXpresso SDK includes production-grade software with integrated RTOS (optional), integrated enabling software technologies (stacks and middleware), reference software, and more.

In addition to working seamlessly with the MCUXpresso IDE, the MCUXpresso SDK also supports and provides example projects for various toolchains. The Development tools chapter in the associated Release Notes provides details about toolchain support for your board. Support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.

Underscoring our commitment to high quality, the MCUXpresso SDK is MISRA compliant and checked with Coverity static analysis tools. For details on MCUXpresso SDK, see MCUXpresso-SDK: Software Development Kit for MCUXpresso.

MCUXpresso SDK#

As part of the MCUXpresso software and tools, MCUXpresso SDK is the evolution of Kinetis SDK, includes support for LPC, DSC,PN76, and i.MX System-on-Chip (SoC). The same drivers, APIs, and middleware are still available with support for Kinetis, LPC, DSC, and i.MX silicon. The MCUXpresso SDK adds support for the MCUXpresso IDE, an Eclipse-based toolchain that works with all MCUXpresso SDKs. Easily import your SDK into the new toolchain to access to all of the available components, examples, and demos for your target silicon. In addition to the MCUXpresso IDE, support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.

In order to maintain compatibility with legacy Freescale code, the filenames and source code in MCUXpresso SDK containing the legacy Freescale prefix FSL has been left as is. The FSL prefix has been redefined as the NXP Foundation Software Library.

Development tools#

The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.

SDK 25.12.00 is the final release that includes MCUXpresso IDE support for KW4x devices. Beginning with SDK 26.x.x, MCUXpresso IDE will no longer be supported for KW4x development, and MCUXpresso for Visual Studio Code will become the recommended integrated development environment.

  • IAR Embedded Workbench for Arm, version is 9.70.2

  • MCUXpresso IDE, Rev. 25.06.xx

  • MCUXpresso for VS Code v26.03

  • GCC Arm Embedded Toolchain 14.2.x

Supported development systems#

This release supports board and devices listed in following table. The board and devices in bold were tested in this release.

Development boards

MCU devices

KW47-EVK

KW47B42Z83AFTA, KW47B42Z96AFTA, KW47B42Z97AFTA,
KW47B42ZB2AFTA, KW47B42ZB3AFTA, KW47B42ZB6AFTA,
KW47B42ZB7AFTA, KW47Z42082AFTA, KW47Z42092AFTA,
KW47Z420B2AFTA, KW47Z420B3AFTA

MCUXpresso SDK release package#

The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.

Device support#

The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.

Board support#

The boards folder provides the board-specific demo applications, driver examples, and middleware examples.

Demo application and other examples#

The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.

RTOS#

FreeRTOS#

Real-time operating system for microcontrollers from Amazon

Middleware#

Wireless XCVR#

The XCVR component provides a base Transceiver Driver for the 2.4 GHz narrowband radio.

Bluetooth LE Controller#

  • Main features supported:

    • Peripheral Role

    • Central Role

    • Multiple PHYs (1 Mbps, 2 Mbps, Coded PHY)

    • Asymmetric Connections

    • Public/Random/Static Addresses

    • Network/Device Privacy Modes

    • Extended Advertising

    • Extended Scanning

    • Passive/Active Scanning

    • LE Encryption

    • LE Ping Procedure

    • HCI Test Interface

    • UART Test Interface

    • Randomized Advertising Channel Indexing

    • Sleep Clock Accuracy Update - Mechanism

    • ADI Field in Scan Response Data

    • HCI Support for Debug Keys in LE - Secure Connections

  • Main capabilities supported:

    • Simultaneous scanning 1 Mbps and Long Range

    • Scanning and advertising in parallel

    • 24 connections as a central role

    • 24 connections as a peripheral role

    • Any combination of central and peripheral roles (24 connections maximum)

    • 8 connections with a 7.5 ms connection interval

    • Two advertising sets in parallel (\Five adv set as Early Access Release).

    • 26 Accept List entries

    • 36 Resolvable Private Address (RPA) entries

    • Up to two Chain Packets per Extended Advertising set

    • Enhanced Notification on end of - Scanning/Advertising/Connection events

    • Connection event counters associated to Bluetooth LE packet reception

    • Timestamp associated to Bluetooth LE packet reception

    • RF channel info associated to Bluetooth LE packet reception

    • NXP proprietary Bluetooth LE Handover feature

    • Decision Based Advertising Filtering (DBAF)

    • Advertising Coding Selection (ACS)

    • Periodic Advertising with Responses (PAwR) Additional features supported for KW47 and MCX W72 devices:

    • Channel Sounding Additional features supported as EAR (\Early Access Release) in the KW47 experimental build:

    • Inline PCT return

    • Channel Sounding Enhancement 1

    • Channel Sounding TX/SNR (18dB, 21 dB, 24 dB and 27dB)

    • Channel Sounding PHY 2Mbps BT2.0

    • Channel Sounding additional supported timings:

      • T_PM=10us

      • T_IP1/T_IP2=60, 50, 30

      • T_FCS=120, 100, 60 Additional features supported as EAR (\Early Access Release) in the KW45/KW47 experimental builds:

    • LE Test Mode Enhancement (\UTP/OTA).

    • LL Extended Feature Set

    • Monitoring Advertisers

    • Randomized Resolvable Private Address (\RPA)

    • LE Enhanced Connection Update

      Note: Project configuration enabling Experimental features on KW45 and MCX W71 requires the Radio Subsystem (NBU) Firmware to be reprogrammed with the firmware provided in the SDK under \middleware\wireless\ble_controller\bin\experimental\. For NBU programming steps, see the EVK Quick Start Guide and Secure Provisioning SDK (SPSDK) documentation.

      Project configurations that require usage of the Bluetooth LE controller including all Bluetooth LE examples require the Radio Subsystem (NBU) Firmware to be re-programmed with the firmware provided in the SDK under middleware\wireless\ble_controller\bin.

Bluetooth LE Host Stack and Applications#

The Bluetooth LE Host Stack component provides an implementation for a Bluetooth 6.0 mandatory and some optional, proprietary, and experimental features. The Bluetooth LE Host Stack component provides application examples, services, and profiles.

Main features supported:

  • Automotive Compliance

  • MISRA Compliance

  • HIS CCM <= 20

  • Advanced Secure Mode

  • Enhanced ATT

  • GATT Caching

  • GCC Libraries

  • IAR Libraries

  • Bluetooth LE Peripheral Libraries

  • Bluetooth LE Central Libraries

  • Bluetooth LE Full Host Features Libraries

  • Bluetooth LE Host Optional Features Libraries

  • Bluetooth LE Host Mandatory Features Libraries

  • BareMetal and FreeRTOS Support

  • Full Privacy Support

  • NCP Mode - FSCI Application

  • Enhanced Notifications

  • Dynamic Database

  • OTA Support - Sample Applications

  • Decision based Advertising Filtering (DBAF)

  • Advertising Coding Selection (ACS)

  • Periodic Advertising with Responses (PAwR)

  • Encrypted Advertising Data (EAD)

  • Monitoring Advertisers - Experimental feature

  • Randomized RPA - Experimental feature

  • Intrusion Detection System (IDS) - Experimental feature

    Note: The CDE(Complex-domain Distance Estimation) algorithm is an experimental feature intended only for testing purposes. It is not maintained and must not be included in production environments.

    Parent topic:Wireless connectivity middleware overview

Wireless Localization#

Localization

Connectivity framework#

The Connectivity Framework is a software component that provides hardware abstraction modules to the upper layer connectivity stacks and components. It also provides a list of services and APIs (see Supported services). The Connectivity Framework modules are located in the middleware\wireless\framework SDK folder.

Supported services#

  • FSCI - Framework Serial Communication Interface

  • FunctionLib - Common function library utilities

  • HWParameter - Hardware parameter management

  • LowPower - Low power mode management

  • ModuleInfo - Module information and versioning

  • NVS - Non-Volatile Storage

  • NVM - Non-Volatile Memory management

  • OtaSupport - Over-The-Air update support

  • SecLib_RNG - Security library and Random Number Generator

  • Sensors - Sensor abstraction layer

  • SFC - Smart Frequency Calibration

  • WorkQ - Work queue management

Supported platform#

  • KW45_MCXW71

  • KW47_MCXW72

  • MCXW23

  • RW61X

  • RT1060 and RT1170

  • i.MX RT595s

Advanced features supported on platforms#

KW45_MCXW71#
  • FRO32K with smart frequency calibration (see SFC)

  • Power down mode support (for evaluation only)

KW47_MCXW72#
  • FRO32K with smart frequency calibration (see SFC)

  • Power down mode support (for evaluation only)

  • Crystal 32M trimming with temperature

  • Debug module for NBU

  • Extended NBU support with SecLib and pseudo RNG support

CMSIS DSP Library#

The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.

TF-M#

Trusted Firmware - M Library

PSA Test Suite#

Arm Platform Security Architecture Test Suite

NXP PSA CRYPTO DRIVER#

PSA crypto driver for crypto library integration via driver wrappers

secure_storage#

secure_storage

EdgeLock SE050 Plug and Trust Middleware#

Secure subsystem library - SSS APIs

Multicore#

Multicore Software Development Kit

NXP IoT Agent#

NXP IoT Agent

mbedTLS#

mbedtls SSL/TLS library v3.x

mbedTLS#

mbedtls SSL/TLS library v2.x

LittleFS#

LittleFS filesystem stack

LIN Stack#

LIN Stack middleware

FreeMASTER#

FreeMASTER communication driver for 32-bit platforms.

Release contents#

Provides an overview of the MCUXpresso SDK release package contents and locations.

Deliverable

Location

Boards

INSTALL_DIR/boards

Demo Applications

INSTALL_DIR/boards/<board_name>/demo_apps

Driver Examples

INSTALL_DIR/boards/<board_name>/driver_examples

eIQ examples

INSTALL_DIR/boards/<board_name>/eiq_examples

Board Project Template for MCUXpresso IDE NPW

INSTALL_DIR/boards/<board_name>/project_template

Driver, SoC header files, extension header files and feature header files, utilities

INSTALL_DIR/devices/<device_name>

CMSIS drivers

INSTALL_DIR/devices/<device_name>/cmsis_drivers

Peripheral drivers

INSTALL_DIR/devices/<device_name>/drivers

Toolchain linker files and startup code

INSTALL_DIR/devices/<device_name>/<toolchain_name>

Utilities such as debug console

INSTALL_DIR/devices/<device_name>/utilities

Device Project Template for MCUXpresso IDE NPW

INSTALL_DIR/devices/<device_name>/project_template

CMSIS Arm Cortex-M header files, DSP library source

INSTALL_DIR/CMSIS

Components and board device drivers

INSTALL_DIR/components

RTOS

INSTALL_DIR/rtos

Release Notes, Getting Started Document and other documents

INSTALL_DIR/docs

Tools such as shared cmake files

INSTALL_DIR/tools

Middleware

INSTALL_DIR/middleware

What is new#

The following updates were implemented with respect to the previous SDK release version (26.06.00-pvw1).

  • Bluetooth LE Host Stack and Applications

    Added

    • Support for LE Read All Remote Features after connection is established.

    • Experimental Inline PCT Transfer support for localization sample applications.

    • Support for configurable limits for concurrent Channel Sounding connections/procedures.

    Improved

    • Optimized memory allocation in isp_mciq_ranging_compute function for localization applications.

    • Updated RAS loc_reader application for multiple CS connections.

    • Updated handover documentation with broadcast time synchronization details.

    • Documentation updates.

    Fixed

    • Fixed double free issue in L2ca_SendAclDataWithSegmentation function.

    • Fixed consecutive CS procedures sustainability issue.

    • Miscellaneous minor application bug fixes.

    Changed

    • CS procedure state management: do not allow a new procedure to start before the previous one completes.

    • Details can be found in github repository nxp-mcuxpresso/mcuxsdk-middleware-bluetooth-host/CHANGELOG.md.

  • Bluetooth LE Controller No update.

  • Transceiver drivers (XCVR)

    • Added support for Bluetooth LE Channel Sounding.

    • Added API to control PA ramp type and duration.

  • Connectivity framework

    • Major Changes

      • [SecLib] Refactored SecLib functions with improved error handling and naming conventions. Added return status codes for better testing, added the SecLib_ prefix for all functions with backward compatibility maintained via #define stubs. Added parameter checks on all functions and improved test coverage for all SecLib flavors.

      • [SecLib] Updated CryptoLibSW APIs by removing unused pMultiplicationBuffer argument from Ecdh_ComputeDhKeyUltraFast(), ECP256_GeneratePublicKeyUltraFast(), and ECP256_GenerateKeyPairUltraFast(). Renamed ECP256_GeneratePublicKey() to ECP256_GeneratePublicKeySeg() in legacy implementation. Added new ECP256_GeneratePublicKey() API for SPAKE2+ ComputeL procedure.

    • Minor Changes

      • [FunctionLib] Enhanced FLib_StrLen() to return an error value when the string size exceeds maximum limit (4096 bytes), adopting strnlen behavior.

      • [Common] Cleaned deprecated mbedtls2x Kconfig configurations.

      • [wireless_mcu][lcl] Updated FEM API to send configuration to NBU for proper XCVR timing adaptation during Channel Sounding activity. XCVR register backup and restore uses current mechanism with config sent through PLATFORM_NbuApiReq().

      • [SecLib_RNG] Removed support for deprecated devices including FSL_FEATURE_SOC_SIM_COUNT for RNG and QN908x platforms.

      • [FactoryDataProvider] Removed deprecated FactoryDataProvider service as it is no longer used following mbedtls2.x deprecation.

    • Bug Fixes

      • [wireless_mcu] Fixed FRO6M calibration failure in OEM closed lifecycle by replacing inaccessible DWT cycle counter with SysTick timer. The implementation saves/restores SysTick state to maintain FreeRTOS compatibility.

      • [wireless_mcu][ble] Removed redundant assert in PLATFORM_SendHciVendorEvent() as invalid parameters are already sanitized with the error returned to the caller.

      • [SecLib] Fixed CMakeLists.txt lib_crypto variant dependency.

      • [MISRA] Various MISRA compliance fixes in OTA, flash related files, FSCI, NVM, platform files, and ICS modules. Fixed potential flash blank check issue with unaligned pointers and split OTA_PostWriteToFlash() to match the HIS_LEVEL constraint. Also prevented infinite loop in FLib_StrLen() and ensured that unions have a consistent non-zero size across compilers.

Known issues#

This section lists the known issues, limitations, and/or workarounds.

FRO6M Clock Stability Issue#

According to ERRATA ERR052742, the FRO6M clock is not stable on some parts. FRO6M outputs lower frequency signal instead of 6MHz when device is reset or wakes up from low power. It can impact peripherals using it as a clock source.

Impact on TSTMR Module#

The TSTMR (Time Stamp Timer) module exclusively uses the FRO6M clock source. Due to the aforementioned stability issues, avoid using TSTMR-related APIs if your application requires high-precision timing.

Recommendation#

For applications requiring precise timing, consider using alternative timer modules that support more stable clock sources.

New project wizard compile failure#

The following components request the user to manually select other components that they depend upon in order to compile. These components depend on several other components and the New Project Wizard (NPW) is not able to decide which one is needed by the user.

Note: xxx means core variants, such as, cm0plus, cm33, cm4, cm33_nodsp.

Also for low-level adapter components, currently the different types of the same adapter cannot be selected at the same time. For example, if there are two types of timer adapters, gpt_adapter and pit_adapter, only one can be selected as timer adapter in one project at a time. Duplicate implementation of the function results in an error.

Only FreeRTOS is tested for RTOS support#

This release only supports the FreeRTOS kernel and a bare-metal non-preemptive task scheduler.

Disabled pairing and bonding for most sensor applications#

Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h header file.

Bluetooth LE#

Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h header file.

Bluetooth LE controller:#

  • The maximum Advertising data length is limited to 800 bytes.

  • The scanner may sporadically miss some chained packets.

Periodic Advertising with Responses (PAwR):

  • Periodic Advertising with Response (PAwR) is not supported with the configuration “Subevent Interval = Number of Response Slots x Response Slot Spacing with Response Slot Spacing = 0x2”.

  • The feature is not functional with the Free-Running Oscillator (FRO32K); it requires a 32 KHz Crystal Oscillator with accuracy less than 50 ppm.

KW45/MCXW71: No specific issues.

KW47/MCXW72: Channel Sounding (CS): Information:

  • RF Bandwidth Occupancy and Connections/Channel Sounding Activities: The RF bandwidth occupancy is tightly coupled with configured activities, including the number of connections, connection event durations, the number of Channel Sounding (CS) procedures, and related CS parameters (e.g., subevent length, repeat mode). The Link Layer Scheduler is responsible for allocating RF bandwidth to these activities, optimizing bandwidth utilization. However, because each activity operates on its own timing constraints, some RF collisions are expected. This is inherent to the Bluetooth LE protocol, particularly when peripheral roles are configured, as anchor placement is controlled by the central peer devices. The application controls several timing parameters, such as connection interval and subevent length. To optimize user experience, the Link Layer expects the application to adjust these parameters to achieve the best RF bandwidth occupancy with the lowest occurrence of RF collisions.

Limitations:

  • RTT with Sounding Sequence is not supported.

  • Maximum 6 Channel Sounding procedures are supported in parallel.

  • Phase measurement bias is within certification range (<1.7x2πns) with KW47 EVK board. However, if different PCB or antenna matching is used, some bias may appear due to increased delay.

Known issues:

  • NADM RTT payload 96bits BT2.0 raises false positives.

  • When CS Subevents are configured very close from each other (<700us), some Subevents may be aborted with reason 0x3.

  • When CS offset is configured too close from ACL anchor point, the anchor point may not be served (TX on central or RX on peripheral will not happen). Ideally, CS Offset should be configured greater than 1ms.

  • RTT bias compensation:

    • For parts not properly configured at production (IFR blank), RTT bias may not be compensated properly. Consequently, an inaccuracy of +/-2m may be observed.

Other limitations#

  • The following Connectivity Framework configurations are Experimental and not recommended for mass production:

    • Power down on application power domain.

  • GenFSK Connectivity_test application is not operational with Low Power enabled.

  • Serial manager is only supported on UART (not I2C nor SPI).

  • If the FRO32K is configured as the clock source of the CM33 Core then the debug session will block in IAR CMSIS-DAP while debugging. Use a lower debug wire speed, for example 1 MHz instead of the default one.

    In IAR, the option is in Runtime Checking -> Debugger -> CMSIS DAP -> Interface -> Interface speed.

Examples hello_world_ns, secure_faults_ns, and secure_faults_trdc_ns have incorrect library path in GUI projects#

When the affected examples are generated as GUI projects, the library linking the secure and non-secure worlds has an incorrect path set. This causes linking errors during project compilation.

Examples: hello_world_ns, hello_world_s, secure_faults_ns, secure_faults_s, secure_faults_trdc_ns, secure_faults_trdc_s

Affected toolchains: mdk, iar

Workaround: In the IDE project settings for the non-secure (_ns) project, find the linked library (named hello_world_s_CMSE_lib.o, or similar, depending on the example project) and replace the path to the library with <build_directory>/<secure_world_project_folder>/<IDE>/, replacing the subdirectory names with the build directory, the secure world project name, and IDE name.