flexcan_legacy_fifo_edma_transfer#
Overview#
The flexcan_legacy_fifo_edma_transfer example shows how to use the EDMA version transactional driver to receive CAN Message from Legacy Rx FIFO.
In this example, when set ENABLE_LOOPBACK macro, only one board is needed. The example will config one FlexCAN Message Buffer as Tx Message Buffer and setup Legacy Rx FIFO. After that, example will send 6 CAN Messages from Tx Message Buffer to Legacy Rx FIFO through internal loopback interconnect and read them out using EDMA version FlexCAN transactional driver. The send and received message will be print out to terminal.
When not define ENABLE_LOOPBACK, need 2 boards are connected through CAN bus. Endpoint A (board A) send a CAN Message to Endpoint B(board B) when user press space key in terminal. Endpoint B receive the message by Legacy Rx FIFO and read them out using EDMA version FlexCAN transactional driver. The send and received message will be print out to terminal.
Supported Boards#
MIMXRT1060-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKB board
Personal Computer
Board settings
The example requires 2 sets of boards, each of them are mounted with the base board. Using a male to male CAN cable to connect the CAN3 instance (J42) between the 2 base boards.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
After connecting the two boards, these instructions display on each terminal window. One board must be chosen as node A and the other board as node B. (Note: Node B should start first) Data is sent continuously between the node A and the node B.
This message displays on the node A terminal:
FlexCAN Legacy Rx FIFO edma example.
Board to board mode.
Node B Legacy Rx FIFO used for Rx.
Node A Message buffer 9 used for Tx.
Please select local node as A or B:
Note: Node B should start first.
Node:a
Press any key to trigger 6 transmission.
Send Msg0: word0 = 0x0, word1 = 0x55, id = 0x123.
Send Msg1: word0 = 0x1, word1 = 0x55, id = 0x124.
Send Msg2: word0 = 0x2, word1 = 0x55, id = 0x125.
Send Msg3: word0 = 0x3, word1 = 0x55, id = 0x126.
Send Msg4: word0 = 0x4, word1 = 0x55, id = 0x127.
Send Msg5: word0 = 0x5, word1 = 0x55, id = 0x128.
Press any key to trigger 6 transmission.
This message displays on the node B terminal:
FlexCAN Legacy Rx FIFO edma example. Board to board mode. Node B Legacy Rx FIFO used for Rx. Node A Message buffer 9 used for Tx. Please select local node as A or B: Note: Node B should start first. Node:b Start to Wait data from Node A
Receive Msg0: word0 = 0x0, word1 = 0x55, ID Filter Hit: 0, Time stamp: 14162. Receive Msg1: word0 = 0x1, word1 = 0x55, ID Filter Hit: 1, Time stamp: 16719. Receive Msg2: word0 = 0x2, word1 = 0x55, ID Filter Hit: 2, Time stamp: 19277. Receive Msg3: word0 = 0x3, word1 = 0x55, ID Filter Hit: 3, Time stamp: 21831. Receive Msg4: word0 = 0x4, word1 = 0x55, ID Filter Hit: 4, Time stamp: 24385. Receive Msg5: word0 = 0x5, word1 = 0x55, ID Filter Hit: 5, Time stamp: 26944.
Wait for the next 6 messages!
Note:
This case will be blocked when transferring data on armgcc debug/sdram_debug target. This issue has been fixed in later release by open ERR005829 feature.