Changelog eRPC#
All notable changes to this project will be documented in this file.
The format is based on Keep a Changelog, and this project adheres to Semantic Versioning.
Unreleased#
Added#
Fixed#
Python code of the eRPC infrastructure was updated to match the proper python code style, add type annotations and improve readability.
1.14.0#
Added#
Added Cmake/Kconfig support.
Made java code jdk11 compliant, GitHub PR #432.
Added imxrt1186 support into mu transport layer.
erpcgen: Added assert for listType before usage, GitHub PR #406.
Fixed#
eRPC: Sources reformatted.
erpc: Fixed typo in semaphore get (mutex -> semaphore), and write it can fail in case of timeout, GitHub PR #446.
erpc: Free the arbitrated client token from client manager, GitHub PR #444.
erpc: Fixed Makefile, install the erpc_simple_server header, GitHub PR #447.
erpc_python: Fixed possible AttributeError and OSError on calling TCPTransport.close(), GitHub PR #438.
Examples and tests consolidated.
1.13.0#
Added#
erpc: Add BSD-3 license to endianness agnostic files, GitHub PR #417.
eRPC: Add new Zephyr-related transports (zephyr_uart, zephyr_mbox).
eRPC: Add new Zephyr-related examples.
Fixed#
eRPC,erpcgen: Fixing/improving markdown files, GitHub PR #395.
eRPC: Fix Python client TCPTransports not being able to close, GitHub PR #390.
eRPC,erpcgen: Align switch brackets, GitHub PR #396.
erpc: Fix zephyr uart transport, GitHub PR #410.
erpc: UART ZEPHYR Transport stop to work after a few transactions when using USB-CDC resolved, GitHub PR #420.
Removed#
eRPC,erpcgen: Remove cstbool library, GitHub PR #403.
1.12.0#
Added#
eRPC: Add dynamic/static option for transport init, GitHub PR #361.
eRPC,erpcgen: Winsock2 support, GitHub PR #365.
eRPC,erpcgen: Feature/support multiple clients, GitHub PR #271.
eRPC,erpcgen: Feature/buffer head - Framed transport header data stored in MessageBuffer, GitHub PR #378.
eRPC,erpcgen: Add experimental Java support.
Fixed#
eRPC: Fix receive error value for spidev, GitHub PR #363.
eRPC: UartTransport::init adaptation to changed driver.
eRPC: Fix typo in assert, GitHub PR #371.
eRPC,erpcgen: Move enums to enum classes, GitHub PR #379.
eRPC: Fixed rpmsg tty transport to work with serial transport, GitHub PR #373.
1.11.0#
Fixed#
eRPC: Makefiles update, GitHub PR #301.
eRPC: Resolving warnings in Python, GitHub PR #325.
eRPC: Python3.8 is not ready for usage of typing.Any type, GitHub PR #325.
eRPC: Improved codec function to use reference instead of address, GitHub PR #324.
eRPC: Fix NULL check for pending client creation, GitHub PR #341.
eRPC: Replace sprintf with snprintf, GitHub PR #343.
eRPC: Use MU_SendMsg blocking call in MU transport.
eRPC: New LPSPI and LPI2C transport layers.
eRPC: Freeing static objects, GitHub PR #353.
eRPC: Fixed casting in deinit functions, GitHub PR #354.
eRPC: Align LIBUSBSIO.GetNumPorts API use with libusbsio python module v. 2.1.11.
erpcgen: Renamed temp variable to more generic one, GitHub PR #321.
erpcgen: Add check that string read is not more than max length, GitHub PR #328.
erpcgen: Move to g++ in pytest, GitHub PR #335.
erpcgen: Use build=release for make, GitHub PR #334.
erpcgen: Removed boost dependency, GitHub PR #346.
erpcgen: Mingw support, GitHub PR #344.
erpcgen: VS build update, GitHub PR #347.
erpcgen: Modified name for common types macro scope, GitHub PR #337.
erpcgen: Fixed memcpy for template, GitHub PR #352.
eRPC,erpcgen: Change default build target to release + adding artefacts, GitHub PR #334.
eRPC,erpcgen: Remove redundant includes, GitHub PR #338.
eRPC,erpcgen: Many minor code improvements, GitHub PR #323.
1.10.0#
Fixed#
eRPC: MU transport layer switched to blocking MU_SendMsg() API use.
1.10.0#
Added#
eRPC: Add TCP_NODELAY option to python, GitHub PR #298.
Fixed#
eRPC: MUTransport adaptation to new supported SoCs.
eRPC: Simplifying CI with installing dependencies using shell script, GitHub PR #267.
eRPC: Using event for waiting for sock connection in TCP python server, formatting python code, C specific includes, GitHub PR #269.
eRPC: Endianness agnostic update, GitHub PR #276.
eRPC: Assertion added for functions which are returning status on freeing memory, GitHub PR #277.
eRPC: Fixed closing arbitrator server in unit tests, GitHub PR #293.
eRPC: Makefile updated to reflect the correct header names, GitHub PR #295.
eRPC: Compare value length to used length() in reading data from message buffer, GitHub PR #297.
eRPC: Replace EXPECT_TRUE with EXPECT_EQ in unit tests, GitHub PR #318.
eRPC: Adapt rpmsg_lite based transports to changed rpmsg_lite_wait_for_link_up() API parameters.
eRPC, erpcgen: Better distuingish which file can and cannot by linked by C linker, GitHub PR #266.
eRPC, erpcgen: Stop checking if pointer is NULL before sending it to the erpc_free function, GitHub PR #275.
eRPC, erpcgen: Changed api to count with more interfaces, GitHub PR #304.
erpcgen: Check before reading from heap the buffer boundaries, GitHub PR #287.
erpcgen: Several fixes for tests and CI, GitHub PR #289.
erpcgen: Refactoring erpcgen code, GitHub PR #302.
erpcgen: Fixed assigning const value to enum, GitHub PR #309.
erpcgen: Enable runTesttest_enumErrorCode_allDirection, serialize enums as int32 instead of uint32.
1.9.1#
Fixed#
eRPC: Construct the USB CDC transport, rather than a client, GitHub PR #220.
eRPC: Fix premature import of package, causing failure when attempting installation of Python library in a clean environment, GitHub PR #38, #226.
eRPC: Improve python detection in make, GitHub PR #225.
eRPC: Fix several warnings with deprecated call in pytest, GitHub PR #227.
eRPC: Fix freeing union members when only default need be freed, GitHub PR #228.
eRPC: Fix making test under Linux, GitHub PR #229.
eRPC: Assert costumizing, GitHub PR #148.
eRPC: Fix corrupt clientList bug in TransportArbitrator, GitHub PR #199.
eRPC: Fix build issue when invoking g++ with -Wno-error=free-nonheap-object, GitHub PR #233.
eRPC: Fix inout cases, GitHub PR #237.
eRPC: Remove ERPC_PRE_POST_ACTION dependency on return type, GitHub PR #238.
eRPC: Adding NULL to ptr when codec function failed, fixing memcpy when fail is present during deserialization, GitHub PR #253.
eRPC: MessageBuffer usage improvement, GitHub PR #258.
eRPC: Get rid for serial and enum34 dependency (enum34 is in python3 since 3.4 (from 2014)), GitHub PR #247.
eRPC: Several MISRA violations addressed.
eRPC: Fix timeout for Freertos semaphore, GitHub PR #251.
eRPC: Use of rpmsg_lite_wait_for_link_up() in rpmsg_lite based transports, GitHub PR #223.
eRPC: Fix codec nullptr dereferencing, GitHub PR #264.
erpcgen: Fix two syntax errors in erpcgen Python output related to non-encapsulated unions, improved test for union, GitHub PR #206, #224.
erpcgen: Fix serialization of list/binary types, GitHub PR #240.
erpcgen: Fix empty list parsing, GitHub PR #72.
erpcgen: Fix templates for malloc errors, GitHub PR #110.
erpcgen: Get rid of encapsulated union declarations in global scale, improve enum usage in unions, GitHub PR #249, #250.
erpcgen: Fix compile error:UniqueIdChecker.cpp:156:104:’sort’ was not declared, GitHub PR #265.
1.9.0#
Added#
eRPC: Allow used LIBUSBSIO device index being specified from the Python command line argument.
Fixed#
eRPC: Improving template usage, GitHub PR #153.
eRPC: run_clang_format.py cleanup, GitHub PR #177.
eRPC: Build TCP transport setup code into liberpc, GitHub PR #179.
eRPC: Fix multiple definitions of g_client error, GitHub PR #180.
eRPC: Fix memset past end of buffer in erpc_setup_mbf_static.cpp, GitHub PR #184.
eRPC: Fix deprecated error with newer pytest version, GitHub PR #203.
eRPC, erpcgen: Static allocation support and usage of rpmsg static FreeRTOSs related APi, GitHub PR #168, #169.
erpcgen: Remove redundant module imports in erpcgen, GitHub PR #196.
1.8.1#
Added#
eRPC: New i2c_slave_transport trasnport introduced.
Fixed#
eRPC: Fix misra erpc c, GitHub PR #158.
eRPC: Allow conditional compilation of message_loggers and pre_post_action.
eRPC: (D)SPI slave transports updated to avoid busy loops in rtos environments.
erpcgen: Re-implement EnumMember::hasValue(), GitHub PR #159.
erpcgen: Fixing several misra issues in shim code, erpcgen and unit tests updated, GitHub PR #156.
erpcgen: Fix bison file, GitHub PR #156.
1.8.0#
Added#
eRPC: Support win32 thread, GitHub PR #108.
eRPC: Add mbed support for malloc() and free(), GitHub PR #92.
eRPC: Introduced pre and post callbacks for eRPC call, GitHub PR #131.
eRPC: Introduced new USB CDC transport.
eRPC: Introduced new Linux spidev-based transport.
eRPC: Added formatting extension for VSC, GitHub PR #134.
erpcgen: Introduce ustring type for unsigned char and force cast to char*, GitHub PR #125.
Fixed#
eRPC: Update makefile.
eRPC: Fixed warnings and error with using MessageLoggers, GitHub PR #127.
eRPC: Extend error msg for python server service handle function, GitHub PR #132.
eRPC: Update CMSIS UART transport layer to avoid busy loops in rtos environments, introduce semaphores.
eRPC: SPI transport update to allow usage without handshaking GPIO.
eRPC: Native _WIN32 erpc serial transport and threading.
eRPC: Arbitrator deadlock fix, TCP transport updated, TCP setup functions introduced, GitHub PR #121.
eRPC: Update of matrix_multiply.py example: Add –serial and –baud argument, GitHub PR #137.
eRPC: Update of .clang-format, GitHub PR #140.
eRPC: Update of erpc_framed_transport.cpp: return error if received message has zero length, GitHub PR #141.
eRPC, erpcgen: Fixed error messages produced by -Wall -Wextra -Wshadow -pedantic-errors compiler flags, GitHub PR #136, #139.
eRPC, erpcgen: Core re-formatted using Clang version 10.
erpcgen: Enable deallocation in server shim code when callback/function pointer used as out parameter in IDL.
erpcgen: Removed ‘$’ character from generated symbol name in ‘_$union’ suffix, GitHub PR #103.
erpcgen: Resolved mismatch between C++ and Python for callback index type, GitHub PR #111.
erpcgen: Python generator improvements, GitHub PR #100, #118.
erpcgen: Fixed error messages produced by -Wall -Wextra -Wshadow -pedantic-errors compiler flags, GitHub PR #136.
1.7.4#
Added#
eRPC: Support MU transport unit testing.
eRPC: Adding mbed os support.
Fixed#
eRPC: Unit test code updated to handle service add and remove operations.
eRPC: Several MISRA issues in rpmsg-based transports addressed.
eRPC: Fixed Linux/TCP acceptance tests in release target.
eRPC: Minor documentation updates, code formatting.
erpcgen: Whitespace removed from C common header template.
1.7.3#
Fixed#
eRPC: Improved the test_callbacks logic to be more understandable and to allow requested callback execution on the server side.
eRPC: TransportArbitrator::prepareClientReceive modified to avoid incorrect return value type.
eRPC: The ClientManager and the ArbitratedClientManager updated to avoid performing client requests when the previous serialization phase fails.
erpcgen: Generate the shim code for destroy of statically allocated services.
1.7.2#
Added#
eRPC: Add missing doxygen comments for transports.
Fixed#
eRPC: Improved support of const types.
eRPC: Fixed Mac build.
eRPC: Fixed serializing python list.
eRPC: Documentation update.
1.7.1#
Fixed#
eRPC: Fixed semaphore in static message buffer factory.
erpcgen: Fixed MU received error flag.
erpcgen: Fixed tcp transport.
1.7.0#
Added#
eRPC: List names are based on their types. Names are more deterministic.
eRPC: Service objects are as a default created as global static objects.
eRPC: Added missing doxygen comments.
eRPC: Added support for 64bit numbers.
eRPC: Added support of program language specific annotations.
Fixed#
eRPC: Improved code size of generated code.
eRPC: Generating crc value is optional.
eRPC: Fixed CMSIS Uart driver. Removed dependency on KSDK.
eRPC: Forbid users use reserved words.
eRPC: Removed outByref for function parameters.
eRPC: Optimized code style of callback functions.
1.6.0#
Added#
eRPC: Added @nullable support for scalar types.
Fixed#
eRPC: Improved code size of generated code.
eRPC: Improved eRPC nested calls.
eRPC: Improved eRPC list length variable serialization.
1.5.0#
Added#
eRPC: Added support for unions type non-wrapped by structure.
eRPC: Added callbacks support.
eRPC: Added support @external annotation for functions.
eRPC: Added support @name annotation.
eRPC: Added Messaging Unit transport layer.
eRPC: Added RPMSG Lite RTOS TTY transport layer.
eRPC: Added version verification and IDL version verification between eRPC code and eRPC generated shim code.
eRPC: Added support of shared memory pointer.
eRPC: Added annotation to forbid generating const keyword for function parameters.
eRPC: Added python matrix multiply example.
eRPC: Added nested call support.
eRPC: Added struct member “byref” option support.
eRPC: Added support of forward declarations of structures
eRPC: Added Python RPMsg Multiendpoint kernel module support
eRPC: Added eRPC sniffer tool
1.4.0#
Added#
eRPC: New RPMsg-Lite Zero Copy (RPMsgZC) transport layer.
Fixed#
eRPC: win_flex_bison.zip for windows updated.
eRPC: Use one codec (instead of inCodec outCodec).
[1.3.0]#
Added#
eRPC: New annotation types introduced (@length, @max_length, …).
eRPC: Support for running both erpc client and erpc server on one side.
eRPC: New transport layers for (LP)UART, (D)SPI.
eRPC: Error handling support.
[1.2.0]#
Added#
eRPC source directory organization changed.
Many eRPC improvements.
[1.1.0]#
Added#
Multicore SDK 1.1.0 ported to KSDK 2.0.0.
[1.0.0]#
Added#
Initial Release