iap3_otp#
Overview#
The IAP OTP project is a simple demonstration program of the SDK IAP driver. It reads fuse word with input index. A message a printed on the UART terminal as fuse read iap operations are performed.
Supported Boards#
EVK-MIMXRT595
Hardware requirements
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
IAP OTP example
Please input the OTP word index to read(0~511):4
Fuse[4] value: 0x1B
Please input the OTP word index to read(0~511):
EVK-MIMXRT685
Hardware requirements
Micro USB cable
EVK-MIMXRT685 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the iap otp example in the terminal window:
IAP OTP example
Please input the OTP word index to read(0~511):4
Fuse[4] value: 0x403B
Please input the OTP word index to read(0~511):
MIMXRT685-AUD-EVK
Hardware requirements
Micro USB cable
MIMXRT685-AUD-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the iap otp example in the terminal window:
IAP OTP example
Please input the OTP word index to read(0~511):4
Fuse[4] value: 0x403B
Please input the OTP word index to read(0~511):