MCUXpresso SDK Documentation

adc_etc_edma

adc_etc_edma#

Overview#

The adc_etc_edma example shows how to use the edma to transfer ADC convert result.

In this example, PIT is used as the hardware trigger source and is triggered once per second. Once ADC gets the trigger from the ADC_ETC, the conversion goes. When the conversion is done, the dma request will be sent, and the dma will transfers the conversion result to a global variable. The user presses the keyboard according to the prompt in the serial terminal to see the ADC conversion result.

Supported Boards#

EVKB-IMXRT1050
Hardware requirements
  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

Board settings

ADC0_IN15 is settings to ADC input, please sample voltage by J23-1 pin.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the adc etc edma demo in the terminal window:

 Adc AutoCalibration Succeed.
 Adc Edma Transfer Example Start.
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2016, voltage = 1.624
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2023, voltage = 1.630
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2017, voltage = 1.625
MIMXRT1060-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKB board

  • Personal Computer

Board settings

ADC0_IN15 is settings to ADC input, please sample voltage by J33-1 pin.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the adc etc edma demo in the terminal window:

 Adc AutoCalibration Succeed.
 Adc Edma Transfer Example Start.
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2016, voltage = 1.624
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2023, voltage = 1.630
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2017, voltage = 1.625
MIMXRT1060-EVKC
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

Board settings

ADC0_IN15 is settings to ADC input, please sample voltage by J33-1 pin.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the adc etc edma demo in the terminal window:

 Adc AutoCalibration Succeed.
 Adc Edma Transfer Example Start.
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2016, voltage = 1.624
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2023, voltage = 1.630
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2017, voltage = 1.625
EVK-MIMXRT1064
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1064 board

  • Personal Computer

Board settings

ADC0_IN15 is settings to ADC input, please sample voltage by J23-1 pin.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the adc etc edma demo in the terminal window:

 Adc AutoCalibration Succeed.
 Adc Edma Transfer Example Start.
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2016, voltage = 1.624
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2023, voltage = 1.630
 Press any key to print output adc current convert value and voltage.
 ADC current convert value = 2017, voltage = 1.625