secure_faults_trdc_s#
Overview#
The Secure Faults demo application demonstrates handling of different secure faults. This application is based on application Hello World. In addition, user can invoke different secure faults by setting testCaseNumber variable (see source code). The following faults can be invoked:
TEST 0: No any secure fault TEST 1: Invalid transition from secure to normal world TEST 2: Invalid entry point from normal to secure world TEST 3: Invalid data access from normal world, example 1 TEST 4: Invalid input parameters in entry function TEST 5: Invalid data access from normal world, example 2