tpm_input_capture#
Overview#
The TPM project is a demonstration program of the SDK TPM driver’s input capture feature. The example sets up a TPM channel for dual-edge capture. Once the input signal is received, this example will print the capture value.
Supported Boards#
EVK9-MIMX8ULP
Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
CM33: Connect input signal to J11-3 and J11-5(GND).
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
IMX952LPD5EVK-19
Hardware requirements
Micro USB cable
IMX952-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
CM7: Connect input signal to TP86 and (GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
EVK-MCIMX7ULP
Hardware requirements
Micro USB cable
MCIMX7ULP-EVK board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
Connect input signal to TP86(PTB0).
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
Connect a micro USB cable between the host PC and the J6 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see information from the terminal as below.
TPM input capture example
Once the input signal is received the input capture value is printed
EVK-MIMX8ULP
Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
CM33: Connect input signal to J11-3 and J11-5(GND).
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
FRDM-K32L2A4S
Hardware requirements
Mini/micro USB cable
FRDM-K32L2A4S board
Personal Computer
Board settings
Connect input signal to J3-3
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see information from the terminal as below.
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=e648
FRDM-K32L2B
Hardware requirements
Mini/micro USB cable
FRDMK32L2B board
Personal Computer
Board settings
Connect input to J4-2
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see information from the terminal as below:
TPM input capture example
Once the input signal is received the input capture value is printed
FRDM-K32L3A6
Hardware requirements
Mini/micro USB cable
FRDM-K32L3A6 board
Personal Computer
Board settings
M0 core: Connect input signal to PTB13(J1-8). M4 core: Connect input signal to PTB2(J2-2).
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see information from the terminal as below.
TPM input capture example
Once the input signal is received the input capture value is printed
FRDM-KE02Z40M
Hardware requirements
Mini/micro USB cable
FRDM-KE02Z40M board
Personal Computer
Board settings
Connect input signal to PTA0(J2-2).
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see information from the terminal as below.
TPM input capture example
Once the input signal is received the input capture value is printed
FRDM-MCXC041
Hardware requirements
Type-C USB cable
FRDM-MCXC041 board
Personal Computer
Oscilloscope
Board settings
Connect input to J2-4
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=XXXX
FRDM-MCXC242
Hardware requirements
USB-C cable
FRDM-MCXC242 board
Personal Computer
Board settings
Connect input to J2-4. This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see information from the terminal as below.
TPM input capture example
Once the input signal is received the input capture value is printed
FRDM-MCXC444
Hardware requirements
Type-C USB cable
FRDM-MCXC444 board
Personal Computer
Board settings
Connect input to J4-2
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see information from the terminal as below:
TPM input capture example
Once the input signal is received the input capture value is printed
FRDM-MCXW71
Hardware requirements
Type-C USB cable
FRDM-MCXW71 Board
Personal Computer
Board settings
connect input signal to J1-8
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b
MCX-W71-EVK
Hardware requirements
Type-C USB cable
MCX-W71-EVK Board
Personal Computer
Board settings
connect input signal to J1-15
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b
IMX95LPD5EVK-19
Hardware requirements
Micro USB cable
IMX95LPD5-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
CM7: Connect input signal to R881 and (GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
FRDM-IMX95
Hardware requirements
Micro USB cable
FRDM-IMX95 board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
CM7: Connect input signal to J19-32 and (GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
FRDM-IMX952
Hardware requirements
Micro USB cable
IMX952-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
CM7: Connect input signal to GPIO_IO13(J18-33) and (GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
FRDM-IMX937
Hardware requirements
Micro USB cable
FRDM-IMX937 board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
CM7: Connect input signal to J19-32 and (GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
KW45B41Z-EVK
Hardware requirements
Mini/micro USB cable
KW45B41Z-EVK Board
Personal Computer
Board settings
connect input signal to J1-8
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b
KW47-EVK
Hardware requirements
Type-C USB cable
KW47-EVK Board
Personal Computer
Board settings
connect input signal to J1-15
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b
MCIMX93AUTO-EVK
Hardware requirements
USB Type-C cable
MCIMX93AUTO-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
CM33: Connect input signal to J17-16 and J17-29(GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.
Connect a USB Type-C cable between the host PC and the J26 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
MCIMX93-EVK
Hardware requirements
USB Type-C cable
MCIMX93-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
CM33: Connect input signal to J1005-3 and J1005-7(GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
MCIMX93W-EVK
Hardware requirements
USB Type-C cable
MCIMX93W-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
CM33: Connect input signal to J1005-3 and J1005-7(GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
MCIMX93-QSB
Hardware requirements
USB Type-C cable
MCIMX93-QSB board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
CM33: Connect input signal to J1406-3 and J1406-7(GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1708 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
IMX943-EVK
Hardware requirements
Micro USB cable
IMX943-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connect input signal to J47-6 and J47-14(GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.
Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61
MCX-W72-EVK
Hardware requirements
Type-C USB cable
MCX-W72-EVK Board
Personal Computer
Board settings
connect input signal to J1-15
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b
KW47-LOC
Hardware requirements
Type-C USB cable
KW47-LOC Board
Personal Computer
Board settings
connect input signal to J1-1
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b
MCXW72-LOC
Hardware requirements
Type-C USB cable
MCXW72-LOC Board
Personal Computer
Board settings
connect input signal to J1-1
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b
FRDM-MCXW72
Hardware requirements
Type-C USB cable
FRDM-MCXW72 Board
Personal Computer
Board settings
Connect input signal to J1-8.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b
FRDM-KW43
Hardware requirements
Type-C USB cable
FRDM-KW43 Board
Personal Computer
Board settings
Connect input to J19-3. This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b
FRDM-MCXW70
Hardware requirements
Type-C USB cable
FRDM-MCXW70 Board
Personal Computer
Board settings
Connect input to J19-3. This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b