ota_rom_server_enet#
Overview#
This application example demonstrates an OTA update using the ROM API and SB image format. File transfer is done using a simple HTTP server running on the board.
Supported Boards#
Prepare the Demo#
Connect a USB cable between the PC and the board, make sure the power is on.
Open a serial terminal on PC for OpenSDA serial(or USB to Serial) device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert the Ethernet Cable into the target board’s RJ45 port and connect it to your PC network adapter.
Configure the PC’s IP to be in the network 192.168.0.0, so for example 192.168.0.100
Running the demo#
Once the example is executed, you should see the following output in the console:
Initializing PHY... ************************************************ ROM OTA HTTP Server Example Built Jan 26 2024 15:15:52 ************************************************ IPv4 Address : 192.168.0.102 IPv4 Subnet mask : 255.255.255.0 IPv4 Gateway : 192.168.0.100 ************************************************
Open web browser and type
http://192.168.0.102(IP address of the board) on the browser address bar. The browser should show the main web page of the example. Note: Make sure to include “http” protocol specifier in the address bar, so that your browser uses port 80Go to OTA page; Here you can upload SB file with update and see current image state
Select SB file with image update and upload it
If the update was successful you should instantly see change in the image state, otherwise see console log for more details
You can now reset the board to let ROM boot the newly installed image
Known issue: Browser may not display progress of the upload. This is an issue of the browser rather than OTA demo. It is possible to watch upload progress in the attached serial console.
Modifying content of static web pages#
To modify content available through the web server you must complete following steps:
Modify, add or delete files in folder
boards\<board_name>\lwip_examples\lwip_httpsrv_ota\webpage.Run the script file
middleware\lwip\src\apps\httpsrv\mkfs\mkfs.pl <directory name>to generate newhttpsrv_fs_data.c. Make sure to execute it from a folder where the filehttpsrv_fs_data.cis. For example:C:\sdk\boards\<board_name>\lwip_examples\lwip_httpssrv_ota> C:\sdk\middleware\lwip\src\apps\httpsrv\mkfs\mkfs.pl webpage
Make sure the
httpsrv_fs_data.cfile has been overwritten with the newly generated content.Re-compile the HTTP server application example and download it to your board.