MCUXpresso SDK Documentation

host_cdc_ecm#

Overview#

The host CDC-ECM project is a simple demonstration program based on the MCUXpresso SDK . It demonstrates Ping and UDP echo server, it also join into a multicast group. The application periodically sends the ICMP echo request to a PC and processes the PC reply and always forwarding UDP message on echo port.

System Requirement#

Hardware requirements#

  • Mini/micro USB cable

  • USB A to micro AB cable

  • Hardware (Tower module/base board, and so on) for a specific device

  • Personal Computer (PC)

Software requirements#

  • The project path is:
    <MCUXpresso_SDK_Install>/boards//usb_examples/usb_host_cdc_ecm//.

The is Bare Metal or FreeRTOS OS.

Getting Started#

Hardware Settings#

For detailed instructions, see the appropriate board User’s Guide.

Set the hardware jumpers (Tower system/base module) to default settings.

Prepare the example#

  1. Connect a USB cable between the PC host and the USB port on the target board with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  2. Make sure to use a USB HUB or an adapter with OTG functionality firstly. Connect the target board to the external power source (the example is self-powered).

  3. Download the program to the target board.

  4. Power off the target board, then power on again.

For detailed instructions, see the appropriate board User’s Guide.

Run the example#

  1. Connect serial port to board and run the example host_cdc_ecm , then plug in USB CDC-ECM device to the board. The log will printed like below:
    Host enumerates CDC-ECM device

  2. If network link of CDC-ECM device is up, the example host_cdc_ecm will start DHCP service and join into a multicast group using IGMP. The example host_cdc_ecm will always listening on UDP port 7 and echo message to sender, then start Ping. The log will printed like below:
    Host running

Supported Boards#

  • MCX-N5XX-EVK

  • MCX-N9XX-EVK

  • FRDM-MCXN947

  • FRDM-MCXN947T

  • RD-RW612-BGA

  • FRDM-RW612

  • FRDM-MCXA577