Sysbuild#
Sysbuild is a higher-level build system that can be used to combine multiple other build systems together. It’s ported from Sysbuild (System build) — Zephyr Project. In MCUXpresso SDK build system, it’s mainly used for multi-project example build.
Sysbuild files#
To include sub projects into building system, you must prepare sysbuild.cmake into main project folder. Sub projects can be located anywhere which are imported by ExternalMCUXProject_Add command inside sysbuild.cmake.
Take multicore hello_world for example:
# examples/multicore_examples/hello_world/primary/sysbuild.cmake
ExternalMCUXProject_Add(
APPLICATION hello_world_secondary_core
SOURCE_DIR ${APP_DIR}/../secondary
board ${SB_CONFIG_secondary_board}
core_id ${SB_CONFIG_secondary_core_id}
config ${SB_CONFIG_secondary_config}
toolchain ${SB_CONFIG_secondary_toolchain}
)
# Let's build the secondary application first
add_dependencies(${DEFAULT_IMAGE} hello_world_secondary_core)
The ${APP_DIR} means the build directory of primary project and ${DEFAULT_IMAGE} indicates the primary project target. The build sequence can be determined by add_dependencies function in sysbuild.cmake.
The variables with SB_ prefix in sysbuild.cmake can be defined before adding sub projects. Or you can pass them with west command -D.
In practice it is more common to set these variables automatically via kconfig to support multiple platforms in a more flexible way. For example, you can prepare a Kconfig.sysbuild in main project folder:
# examples/middleware/multicore/multicore_examples/hello_world/primary/Kconfig.sysbuild
config secondary_board
string
default "$(board)"
config secondary_core_id
string
default "cm4" if $(board) = "evkbmimxrt1170" && $(core_id) = "cm7"
default "cm33_core1" if $(board) = "lpcxpresso55s69" && $(core_id) = "cm33_core0"
config secondary_config
string
default "debug" if $(config) = "debug"
default "debug" if $(config) = "flexspi_nor_debug"
config secondary_toolchain
string
default "$(toolchain)"
Sysbuild is used to organize project build sequence, about how images are linked together is set by the project’s own CMakeLists.txt. For example, you must import the secondary core binary in the CMakeLists.txt of primary project:
# examples/multicore_examples/hello_world/secondary/CMakeLists.txt
mcux_convert_binary(
TOOLCHAINS armgcc mdk iar
BINARY ${APPLICATION_BINARY_DIR}/${CONFIG_TOOLCHAIN}/core1_image.bin
)
# examples/multicore_examples/hello_world/primary/CMakeLists.txt
mcux_add_iar_configuration(
LD "--image_input=${APPLICATION_BINARY_DIR}/../hello_world_secondary_core/iar/core1_image.bin,_core1_image, __core1_image,4 "
)
Application configuration files#
Within the main application’s directory, create a subdirectory named sysbuild. This directory serves as the configuration directory for the application. Based on the naming convention, configuration files placed in this directory are automatically loaded by Sysbuild for each project it manages.
For the main application, the configuration file name should correspond to the folder name the application resides in. For other applications, the configuration file name should match the identifier specified in the project() declaration within the respective CMakeLists.txt file.
For Example, the main application is located in the primary folder:
multicore_examples
├── hello_world
├── primary
| ├── CMakeLists.txt
| ├── prj.conf
| ├── sysbuild.cmake
| └── sysbuild
| ├── primary.conf
| ├── primary_v2.conf
| ├── hello_world_secondary_core.conf
| ├── hello_world_secondary_core_v2.conf
|
├── secondary
├── CMakeLists.txt
├── prj.conf
In this case:
The file
primary.conflocated in thehello_world/primary/sysbuilddirectory is used for the primary application.The file
hello_world_secondary_core.confis used for the hello_world_secondary_core project located in thehello_world/secondarydirectory.
These configuration files take precedence over the default configuration file ${APPLICATION_SOURCE_DIR}/prj.conf.
Sysbuild also supports selecting configuration files based on specific file suffixes. For example, within the previously described project structure, when the west build command is executed with the ‘-DFILE_SUFFIX=v2’ option, Sysbuild automatically loads configuration files that include the specified suffix.
Specifically:
The file
primary_v2.conflocated in thehello_world/primary/sysbuilddirectory is used for the primary application.The file
hello_world_secondary_core_v2.confis used for the hello_world_secondary_core project located in thehello_world/secondarydirectory.
This mechanism enables flexible configuration management across different build variants or versions.
The configuration files can be checked from console log:
west build -b evkmimxrt1180 --sysbuild ./examples/multicore_examples/hello_world/primary --config flexspi_nor_debug --toolchain armgcc -Dcore_id=cm33 -p always -DFILE_SUFFIX=v2
*****************************
* Running CMake for primary *
*****************************
.......
Parsing /home/dev/mcuxsdk/Kconfig
Loaded configuration '/home/dev/mcuxsdk/devices/prj.conf'
Merged configuration '/home/dev/mcuxsdk/devices/RT/RT1180/MIMXRT1189/prj.conf'
Merged configuration '/home/dev/mcuxsdk/devices/RT/RT1180/MIMXRT1189/cm33/prj.conf'
Merged configuration '/home/dev/mcuxsdk/examples/prj.conf'
Merged configuration '/home/dev/mcuxsdk/examples/_boards/evkmimxrt1180/prj.conf'
Merged configuration '/home/dev/mcuxsdk/examples/_boards/evkmimxrt1180/cm33/prj.conf'
Merged configuration '/home/dev/mcuxsdk/examples/multicore_examples/prj.conf'
Merged configuration '/home/dev/mcuxsdk/examples/multicore_examples/hello_world/prj.conf'
Merged configuration '/home/dev/mcuxsdk/examples/multicore_examples/hello_world/primary/prj.conf'
Merged configuration '/home/dev/mcuxsdk/examples/multicore_examples/hello_world/primary/sysbuild/primary_v2.conf'
Merged configuration '/home/dev/mcuxsdk/examples/_boards/evkmimxrt1180/multicore_examples/prj.conf'
Merged configuration '/home/dev/mcuxsdk/examples/_boards/evkmimxrt1180/multicore_examples/hello_world/cm33/prj.conf'
Merged configuration '/home/dev/mcuxsdk/build/primary/zephyr/.config.sysbuild'
Configuration saved to '/home/dev/mcuxsdk/build/primary/.config'
Build command#
To enable sysbuild, only --sysbuild is needed when you build the main project:
west build -b evkbmimxrt1170 --sysbuild ./examples/multicore_examples/hello_world/primary -Dcore_id=cm7 --config flexspi_nor_debug --toolchain=armgcc -p always
You can set Kconfig options via command as -DCONFIG_<var>=<value> for main project or -D<namespace>_CONFIG_<var>=<value> for other projects.
The namespace is the project name declared in project() from CMakeLists.txt file, to imply the config option is for which project. For example:
west build -b evkmimxrt1160 --sysbuild examples/multicore_examples/hello_world/primary -d build -Dcore_id=cm7 --toolchain iar -DCONFIG_MCUX_COMPONENT_driver.lpi2c=y -Dhello_world_secondary_core_CONFIG_MCUX_COMPONENT_driver.lpi2c=y -p always
You can set up a separate config file for each projects via command as -DCONF_FILE=<path/to/config_file> for main project or -D<namespace>_CONF_FILE=<path/to/config_file> for other projects. The namespace is the project name declared in project() from CMakeLists.txt file, to imply the config file is for which project. The config file path can be either an absolute path or a relative path to the current command invocation path. For example:
west build -b evkmimxrt1160 --sysbuild examples/multicore_examples/hello_world/primary -d build -Dcore_id=cm7 --toolchain iar -DCONF_FILE="./examples/multicore_examples/hello_world/prj-static.conf" -Dhello_world_secondary_core_CONF_FILE="./examples/multicore_examples/hello_world/prj-static.conf" -p always
This config file has the highest priority over all.
Kconfig GUI#
The sysbuild projects can be configured with Kconfig GUI just like a normal project in the build system. The only difference is the target name, for main project, they’re menuconfig or guiconfig, for sub project, you must add project name prefix to differ each target.
For example:
west build -t guiconfig
west build -t hello_world_secondary_core_guiconfig
Standalone project#
When using sysbuild command, if you want to generate Standalone project for sharing, you can add “-t standalone_project”. Then the standalone projects will be generated in the <build directory>/<toolchain> folder. The default build directory is “build”, and can be set to other path by adding “-d” parameter.
For example:
west build -b evkmimxrt1160 --sysbuild ./examples/multicore_examples/rpmsg_lite_pingpong/primary -Dcore_id=cm7 --toolchain iar -p always -t standalone_project -d build_rpmsg_lite_pingpong