MCUXpresso SDK Documentation

usart_polling_example

usart_polling_example#

Overview#

The uart_polling example shows how to use uart driver in polling way: In this example, one uart instance connect to PC, the board will send back all characters that PC send to the board.

Supported Boards#

LPC845BREAKOUT
Hardware requirements
  • Micro USB cable

  • LPC845 Breakout board

  • Personal Computer

Board settings

No special settings are required.

Prepare the demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board.

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the USART polling driver example in the terminal window:

Usart polling example.
Board will send back received characters.
Now, please input any character:

LPCXpresso802
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso802 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

Usart polling example.
Board will send back received characters.
Now, please input any character:

LPCXpresso804
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso804 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

Usart polling example.
Board will send back received characters.
Now, please input any character:

LPCXpresso824MAX
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso824MAX board

  • Personal Computer

Board settings

Connect SJ9: 2-3

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

Usart polling example.
Board will send back received characters.
Now, please input any character:

LPCXpresso845MAX
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso845MAX board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

Usart polling example.
Board will send back received characters.
Now, please input any character:

LPCXpresso860MAX
Hardware requirements
  • Micro USB cable

  • LPCXpresso860MAX board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

Usart polling example.
Board will send back received characters.
Now, please input any character: