MCUXpresso SDK Documentation

lpc_gpio_input_interrupt

lpc_gpio_input_interrupt#

Overview#

The GPIO input interrupt example is a demonstration program that uses the KSDK software to manipulate the general-purpose GPIO input interrupt. The example is supported to set with selection of polarity and edge vs level triggering and all GPIO pins can optionally contribute to one of two GPIO interrupts.

Supported Boards#