ZPS_tsAplZdpUserDescConf
This structure is used to store User_Desc_conf message data - a response to a call to the function ZPS_eAplZdpUserDescSetRequest(). This response contains a confirmation of the requested configuration of the User descriptor on a given network node.
The ZPS_tsAplZdpUserDescConfstructure is detailed below.
typedef struct {
uint8 u8Status;
uint16 u16NwkAddrOfInterest;
} ZPS_tsAplZdpUserDescConf;
where:
u8Statusis the return status for ZPS_eAplZdpUserDescSetRequest().u16NwkAddrOfInterestis the network address of the remote node that sent the response (this is the network address that was specified in the request).
Parent topic:ZDP response structures