MCUXpresso SDK Documentation

qsci_interrupt_rb_transfer

qsci_interrupt_rb_transfer#

Overview#

The qsci_interrupt_rb_transfer example shows how to use qsci driver in interrupt way with RX ring buffer enabled:

In this example, one qsci instance is connected to PC, the board will send back all characters that PC sends to the board.

Note: The example echoes every 8 characters, so input 8 characters every time.

Supported Boards#