MCUXpresso SDK Documentation

MCUXpresso SDK Changelog

Contents

MCUXpresso SDK Changelog#

Board Support Files#

board#

[25.06.00]#

  • Initial version

clock_config#

[25.06.00]#

  • Initial version

pin_mux#

[25.06.00]#

  • Initial version


LPC_ADC#

[2.6.0]#

  • New Features

    • Added new feature macro to distinguish whether the GPADC_CTRL0_GPADC_TSAMP control bit is on the device.

    • Added new variable extendSampleTimeNumber to indicate the ADC extend sample time.

  • Bugfix

    • Fixed the bug that incorrectly sets the PASS_ENABLE bit based on the sample time setting.

[2.5.3]#

  • Improvements

    • Release peripheral from reset if necessary in init function.

[2.5.2]#

  • Improvements

    • Integrated different sequence’s sample time numbers into one variable.

  • Bug Fixes

    • Fixed violation of MISRA C-2012 rule 20.9 .

[2.5.1]#

  • Bug Fixes

    • Fixed ADC conversion sequence priority misconfiguration issue in the ADC_SetConvSeqAHighPriority() and ADC_SetConvSeqBHighPriority() APIs.

  • Improvements

    • Supported configuration ADC conversion sequence sampling time.

[2.5.0]#

  • Improvements

    • Add missing parameter tag of ADC_DoOffsetCalibration().

  • Bug Fixes

    • Removed a duplicated API with typo in name: ADC_EnableShresholdCompareInterrupt().

[2.4.1]#

  • Bug Fixes

    • Enabled self-calibration after clock divider be changed to make sure the frequency update be taken.

[2.4.0]#

  • New Features

    • Added new API ADC_DoOffsetCalibration() which supports a specific operation frequency.

  • Other Changes

    • Marked the ADC_DoSelfCalibration(ADC_Type *base) as deprecated.

  • Bug Fixes

    • Fixed the violations of MISRA C-2012 rules:

      • Rule 10.1 10.3 10.4 10.7 10.8 17.7.

[2.3.2]#

  • Improvements

    • Added delay after enabling using the ADC GPADC_CTRL0 LDO_POWER_EN bit for JN5189/QN9090.

  • New Features

    • Added support for platforms which have only one ADC sequence control/result register.

[2.3.1]#

  • Bug Fixes

    • Avoided writing ADC STARTUP register in ADC_Init().

    • Fixed Coverity zero divider error in ADC_DoSelfCalibration().

[2.3.0]#

  • Improvements

    • Updated “ADC_Init()””ADC_GetChannelConversionResult()” API and “adc_resolution_t” structure to match QN9090.

    • Added “ADC_EnableTemperatureSensor” API.

[2.2.1]#

  • Improvements

    • Added a brief delay in uSec after ADC calibration start.

[2.2.0]#

  • Improvements

    • Updated “ADC_DoSelfCalibration” API and “adc_config_t” structure to match LPC845.

[2.1.0]#

  • Improvements

    • Renamed “ADC_EnableShresholdCompareInterrupt” to “ADC_EnableThresholdCompareInterrupt”.

[2.0.0]#

  • Initial version.


AES#

[2.0.3]#

  • Edit aes_one_block() function to be interrupt safe.

[2.0.2]#

  • Fix MISRA-2012 issues.

[2.0.1]#

  • Improvements

    • GCM constant time tag comparison.

[2.0.0]#

  • Initial version.


CLOCK#

[2.3.3]#

  • Improvements

    • Added lost comments for some enumerations.

[2.3.2]#

  • Bug Fixes

    • Fixed violation of MISRA C-2012 rule 5.7.

[2.3.1]#

  • Bug Fixes

    • Fixed MISRA C-2012 rule 10.1, rule 10.4, rule 10.8, rule 15.5 and so on.

    • Fixed IAR warning Pa082 for the clock driver.

[2.3.0]#

  • New feature:

    • Moved SDK_DelayAtLeastUs function from clock driver to common driver.

[2.2.0]#

  • New Feature:

    • add new APIs including CLOCK_GetEmcClkFreq and CLOCK_GetMCanClkFreq due to removing some variables in enum clock_name_t

[2.1.0]#

  • Bug Fix:

    • Fix flexcomm0-9 clock calculation.

    • Correct the return frequency of CLOCK_GetFrgClkFreq.

    • Fix the bug in function CLOCK_GetPllConfig() to refine the cache feature.

    • Update the code to suppress the incorrect configuration in CLOCK_GetUsbPLLOutFromSetup().

    • Fix C++ build errors in CLOCK_GetClockAttachId() and CLOCK_AttachClk().

  • New feature

    • Adding new API CLOCK_DelayAtLeastUs() implemented by DWT to allow users set delay in unit of microsecond.

[2.0.4]#

  • Bug Fix:

    • Fix attach incorrect attach_id.

[2.0.3]#

  • New Feature:

    • add get actual clock attach id api to allow users to obtain the actual clock source in target register.

  • Bug Fix:

    • The attach clock and get actual clock attach id apis should check combination of two clock source.

  • Optimization:

    • Make the judgement statments more clear.

    • Strengthen the compatibility of clock attatch id.

    • Remove some unmeaningful definitions and add some useful ones to enhance readability.

[2.0.2]#

  • Change CLOCK_SetupFROClocking from a macro to a function for different FRO setting address per different ROM version.

[2.0.1]#

  • some minor fixes.

[2.0.0]#

  • initial version.


COMMON#

[2.6.5]#

  • Bug Fixes

    • Fixed the issue that the function SDK_DelayAtLeastUs may underflow and cause a long delay when the input parameter is small and the system clock is low.

[2.6.4]#

  • New Features

    • Add macros to tag deprecated features and experimental features.

[2.6.3]#

  • New Features

    • Added bit mask inversion macros to avoid type promotion.

    • Added register operation macros.

  • Improvements

    • Make function MSDK_EnableCpuCycleCounter compatible with CMSIS-5 and CMSIS-6.

  • Bug Fixes

    • Fixed build issue of CMSIS PACK BSP example caused by CMSIS 6.1 issue.

[2.6.2]#

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rule for implicit conversions in boolean contexts

[2.6.1]#

  • Improvements

    • Support Cortex M23.

[2.6.0]#

  • Bug Fixes

    • Fix CERT-C violations.

[2.5.0]#

  • New Features

    • Added new APIs InitCriticalSectionMeasurementContext, DisableGlobalIRQEx and EnableGlobalIRQEx so that user can measure the execution time of the protected sections.

[2.4.3]#

  • Improvements

    • Enable irqs that mount under irqsteer interrupt extender.

[2.4.2]#

  • Improvements

    • Add the macros to convert peripheral address to secure address or non-secure address.

[2.4.1]#

  • Improvements

    • Improve for the macro redefinition error when integrated with zephyr.

[2.4.0]#

  • New Features

    • Added EnableIRQWithPriority, IRQ_SetPriority, and IRQ_ClearPendingIRQ for ARM.

    • Added MSDK_EnableCpuCycleCounter, MSDK_GetCpuCycleCount for ARM.

[2.3.3]#

  • New Features

    • Added NETC into status group.

[2.3.2]#

  • Improvements

    • Make driver aarch64 compatible

[2.3.1]#

  • Bug Fixes

    • Fixed MAKE_VERSION overflow on 16-bit platforms.

[2.3.0]#

  • Improvements

    • Split the driver to common part and CPU architecture related part.

[2.2.10]#

  • Bug Fixes

    • Fixed the ATOMIC macros build error in cpp files.

[2.2.9]#

  • Bug Fixes

    • Fixed MISRA C-2012 issue, 5.6, 5.8, 8.4, 8.5, 8.6, 10.1, 10.4, 17.7, 21.3.

    • Fixed SDK_Malloc issue that not allocate memory with required size.

[2.2.8]#

  • Improvements

    • Included stddef.h header file for MDK tool chain.

  • New Features:

    • Added atomic modification macros.

[2.2.7]#

  • Other Change

    • Added MECC status group definition.

[2.2.6]#

  • Other Change

    • Added more status group definition.

  • Bug Fixes

    • Undef __VECTOR_TABLE to avoid duplicate definition in cmsis_clang.h

[2.2.5]#

  • Bug Fixes

    • Fixed MISRA C-2012 rule-15.5.

[2.2.4]#

  • Bug Fixes

    • Fixed MISRA C-2012 rule-10.4.

[2.2.3]#

  • New Features

    • Provided better accuracy of SDK_DelayAtLeastUs with DWT, use macro SDK_DELAY_USE_DWT to enable this feature.

    • Modified the Cortex-M7 delay count divisor based on latest tests on RT series boards, this setting lets result be closer to actual delay time.

[2.2.2]#

  • New Features

    • Added include RTE_Components.h for CMSIS pack RTE.

[2.2.1]#

  • Bug Fixes

    • Fixed violation of MISRA C-2012 Rule 3.1, 10.1, 10.3, 10.4, 11.6, 11.9.

[2.2.0]#

  • New Features

    • Moved SDK_DelayAtLeastUs function from clock driver to common driver.

[2.1.4]#

  • New Features

    • Added OTFAD into status group.

[2.1.3]#

  • Bug Fixes

    • MISRA C-2012 issue fixed.

      • Fixed the rule: rule-10.3.

[2.1.2]#

  • Improvements

    • Add SUPPRESS_FALL_THROUGH_WARNING() macro for the usage of suppressing fallthrough warning.

[2.1.1]#

  • Bug Fixes

    • Deleted and optimized repeated macro.

[2.1.0]#

  • New Features

    • Added IRQ operation for XCC toolchain.

    • Added group IDs for newly supported drivers.

[2.0.2]#

  • Bug Fixes

    • MISRA C-2012 issue fixed.

      • Fixed the rule: rule-10.4.

[2.0.1]#

  • Improvements

    • Removed the implementation of LPC8XX Enable/DisableDeepSleepIRQ() function.

    • Added new feature macro switch “FSL_FEATURE_HAS_NO_NONCACHEABLE_SECTION” for specific SoCs which have no noncacheable sections, that helps avoid an unnecessary complex in link file and the startup file.

    • Updated the align(x) to attribute(aligned(x)) to support MDK v6 armclang compiler.

[2.0.0]#

  • Initial version.


CRC#

[2.1.1]#

  • Fix MISRA issue.

[2.1.0]#

  • Add CRC_WriteSeed function.

[2.0.2]#

  • Fix MISRA issue.

[2.0.1]#

  • Fixed KPSDK-13362. MDK compiler issue when writing to WR_DATA with -O3 optimize for time.

[2.0.0]#

  • Initial version.


CTIMER#

[2.3.5]#

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 10.7

[2.3.4]#

  • Bug Fixes

    • Fixed ERRATA ERR053024 CTIMER will enter interrupt twice when function clock much slower than bus clock.

[2.3.3]#

  • Bug Fixes

    • Fix CERT INT30-C INT31-C issue.

    • Make API CTIMER_SetupPwm and CTIMER_UpdatePwmDutycycle return fail if pulse width register overflow.

[2.3.2]#

  • Bug Fixes

    • Clear unexpected DMA request generated by RESET_PeripheralReset in API CTIMER_Init to avoid trigger DMA by mistake.

[2.3.1]#

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 10.7 and 12.2.

[2.3.0]#

  • Improvements

    • Added the CTIMER_SetPrescale(), CTIMER_GetCaptureValue(), CTIMER_EnableResetMatchChannel(), CTIMER_EnableStopMatchChannel(), CTIMER_EnableRisingEdgeCapture(), CTIMER_EnableFallingEdgeCapture(), CTIMER_SetShadowValue(),APIs Interface to reduce code complexity.

[2.2.2]#

  • Bug Fixes

    • Fixed SetupPwm() API only can use match 3 as period channel issue.

[2.2.1]#

  • Bug Fixes

    • Fixed use specified channel to setting the PWM period in SetupPwmPeriod() API.

    • Fixed Coverity Out-of-bounds issue.

[2.2.0]#

  • Improvements

    • Updated three API Interface to support Users to flexibly configure the PWM period and PWM output.

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 8.4.

[2.1.0]#

  • Improvements

    • Added the CTIMER_GetOutputMatchStatus() API Interface.

    • Added feature macro for FSL_FEATURE_CTIMER_HAS_NO_CCR_CAP2 and FSL_FEATURE_CTIMER_HAS_NO_IR_CR2INT.

[2.0.3]#

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 10.3, 10.4, 10.6, 10.7 and 11.9.

[2.0.2]#

  • New Features

    • Added new API “CTIMER_GetTimerCountValue” to get the current timer count value.

    • Added a control macro to enable/disable the RESET and CLOCK code in current driver.

    • Added a new feature macro to update the API of CTimer driver for lpc8n04.

[2.0.1]#

  • Improvements

    • API Interface Change

      • Changed API interface by adding CTIMER_SetupPwmPeriod API and CTIMER_UpdatePwmPulsePeriod API, which both can set up the right PWM with high resolution.

[2.0.0]#

  • Initial version.


LPC_DMA#

[2.5.5]#

  • New Features

    • Added common IRQ handler entry DMA_DriverIRQHandler.

[2.5.4]#

  • Bug Fixes

    • Fixed coverity issues with CERT INT30-C, CERT INT31-C compliance.

[2.5.3]#

  • Improvements

    • Add assert in DMA_SetChannelXferConfig to prevent XFERCOUNT value overflow.

[2.5.2]#

  • Bug Fixes

    • Use separate “SET” and “CLR” registers to modify shared registers for all channels, in case of thread-safe issue.

[2.5.1]#

  • Bug Fixes

    • Fixed violation of the MISRA C-2012 rule 11.6.

[2.5.0]#

  • Improvements

    • Added a new api DMA_SetChannelXferConfig to set DMA xfer config.

[2.4.4]#

  • Bug Fixes

    • Fixed the issue that DMA_IRQHandle might generate redundant callbacks.

    • Fixed the issue that DMA driver cannot support channel bigger then 32.

    • Fixed violation of the MISRA C-2012 rule 13.5.

[2.4.3]#

  • Improvements

    • Added features FSL_FEATURE_DMA_DESCRIPTOR_ALIGN_SIZEn/FSL_FEATURE_DMA0_DESCRIPTOR_ALIGN_SIZE/FSL_FEATURE_DMA1_DESCRIPTOR_ALIGN_SIZE to support the descriptor align size not constant in the two instances.

[2.4.2]#

  • Bug Fixes

    • Fixed violation of the MISRA C-2012 rule 8.4.

[2.4.1]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 5.7, 8.3.

[2.4.0]#

  • Improvements

    • Added new APIs DMA_LoadChannelDescriptor/DMA_ChannelIsBusy to support polling transfer case.

  • Bug Fixes

    • Added address alignment check for descriptor source and destination address.

    • Added DMA_ALLOCATE_DATA_TRANSFER_BUFFER for application buffer allocation.

    • Fixed the sign-compare warning.

    • Fixed violations of the MISRA C-2012 rules 18.1, 10.4, 11.6, 10.7, 14.4, 16.3, 20.7, 10.8, 16.1, 17.7, 10.3, 3.1, 18.1.

[2.3.0]#

  • Bug Fixes

    • Removed DMA_HandleIRQ prototype definition from header file.

    • Added DMA_IRQHandle prototype definition in header file.

[2.2.5]#

  • Improvements

    • Added new API DMA_SetupChannelDescriptor to support configuring wrap descriptor.

    • Added wrap support in function DMA_SubmitChannelTransfer.

[2.2.4]#

  • Bug Fixes

    • Fixed the issue that macro DMA_CHANNEL_CFER used wrong parameter to calculate DSTINC.

[2.2.3]#

  • Bug Fixes

    • Improved DMA driver Deinit function for correct logic order.

  • Improvements

    • Added API DMA_SubmitChannelTransferParameter to support creating head descriptor directly.

    • Added API DMA_SubmitChannelDescriptor to support ping pong transfer.

    • Added macro DMA_ALLOCATE_HEAD_DESCRIPTOR/DMA_ALLOCATE_LINK_DESCRIPTOR to simplify DMA descriptor allocation.

[2.2.2]#

  • Bug Fixes

    • Do not use software trigger when hardware trigger is enabled.

[2.2.1]#

  • Bug Fixes

    • Fixed Coverity issue.

[2.2.0]#

  • Improvements

    • Changed API DMA_SetupDMADescriptor to non-static.

    • Marked APIs below as deprecated.

      • DMA_PrepareTransfer.

      • DMA_Submit transfer.

    • Added new APIs as below:

      • DMA_SetChannelConfig.

      • DMA_PrepareChannelTransfer.

      • DMA_InstallDescriptorMemory.

      • DMA_SubmitChannelTransfer.

      • DMA_SetChannelConfigValid.

      • DMA_DoChannelSoftwareTrigger.

      • DMA_LoadChannelTransferConfig.

[2.0.1]#

  • Improvements

    • Added volatile for DMA descriptor member xfercfg to avoid optimization.

[2.0.0]#

  • Initial version.


DMIC#

[2.3.4]#

  • New Features

    • Added common IRQ handler entry DMIC_CommonDriverIRQHandler.

[2.3.3]#

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rule 10.1, 10.3, 10.4, 10.5, 10.6, 10.7, 10.8.

[2.3.2]#

  • New Features

    • Supported 4 channels in driver.

[2.3.1]#

  • Bug Fixes

    • Fixed the issue that DMIC_EnableChannelDma and DMIC_EnableChannelFifo did not clean relevant bits.

[2.3.0]#

  • Improvements

    • Added new apis DMIC_ResetChannelDecimator/DMIC_EnableChannelGlobalSync/DMIC_DisableChannelGlobalSync.

[2.2.1]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 14.4, 17.7, 10.4, 10.3, 10.8, 14.3.

[2.2.0]#

  • Bug Fixes

    • Corrected the usage of feature FSL_FEATURE_DMIC_IO_HAS_NO_BYPASS.

[2.1.1]#

  • Improvements

    • Added feature FSL_FEATURE_DMIC_HAS_NO_IOCFG for IOCFG register.

[2.1.0]#

  • New Features

    • Added API DMIC_EnbleChannelInterrupt/DMIC_EnbleChannelDma to replace API DMIC_SetOperationMode.

    • Added API DMIC_SetIOCFG and marked DMIC_ConfigIO as deprecated.

    • Added API DMIC_EnableChannelSignExtend to support sign extend feature.

[2.0.5]#

  • Improvements

    • Changed some parameters’ value of DMIC_FifoChannel API, such as enable, resetn, and trig_level. This is not possible for the current code logic, so it improves the DMIC_FifoChannel logic and fixes incorrect math logic.

[2.0.4]#

  • Bug Fixes

    • Fixed the issue that DMIC DMA driver(ver2.0.3) did not support calling DMIC_TransferReceiveDMA in DMA callback as it did before version 2.0.3. But calling DMIC_TransferReceiveDMA in callback is not recommended.

[2.0.3]#

  • New Features

  • Supported linked transfer in DMIC DMA driver.

  • Added new API DMIC_EnableChannelFifo/DMIC_DoFifoReset/DMIC_InstallDMADescriptor.

[2.0.2]#

  • New Features

    • Supported more channels in driver.

[2.0.1]#

  • New Features

    • Added a control macro to enable/disable the RESET and CLOCK code in current driver.

[2.0.0]#

  • Initial version.


DMIC_DMA#

[2.4.2]#

  • Bug Fixes

    • Fixed coverity High Impact finding

[2.4.1]#

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rule 10.1, 10.3, 10.4, 10.5, 10.6, 10.7, 10.8.

[2.4.0]#

  • Bug Fixes

    • Fixed the issue that DMIC_TransferAbortReceiveDMA can not disable dmic and dma request issue.

[2.3.1]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.3.

[2.3.0]#

  • Refer DMIC driver change log 2.0.1 to 2.3.0


EMC#

[2.0.4]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.1, 10.3, 10.4, 10.8, 11.9, 14.2, 14.3, 14.4.

[2.0.3]#

  • Improvements

    • Used SDK_DelayAtLeastUs instead of for loop during the dynamic memory initialization.

[2.0.3]#

  • Improvements

    • Replaced deprecated enumerator CLOCK_GetFreq(kCLOCK_EMC) with CLOCK_GetEmcClkFreq().

[2.0.2]#

  • New Features

    • Added control macro to enable/disable the CLOCK code in current driver.

[2.0.1]#

  • Improvements

    • Added const for two BASE values.

[2.0.0]#

  • Initial version.


LPC_ENET#

[2.3.8]#

  • New Features

    • Added common IRQ handler entry ENET_DriverIRQHandler.

[2.3.7]#

  • Bug Fixes

    • Preserve CSR clock range for MDC clock across software reset.

[2.3.6]#

  • Bug Fixes

    • Fixed ENET_EnableInterrupts to preserve already enabled interrupts.

    • Fixed ENET_DisableInterrupts to correctly manage interrupt summary bits.

    • Fixed IRQ handler to check interrupt enable status before processing events.

[2.3.5]#

  • Bug Fixes

    • Fixed ENET_GetMacAddr address byte order not matching ENET_SetMacAddr.

[2.3.4]#

  • Bug Fixes

    • Fixed the issue that free wrong buffer address when one frame stores in multiple buffers and memory pool is not enough to allocate these buffers to receive one complete frame.

    • Fixed the issue that ENET_DropFrame checks the buffer descriptor flag after it has been re-initialized.

    • Fixed the ENET_GetRxFrame FCS calculation issue.

    • Fixed the issue that there’s no valid error type in the return structure when Rx error bit is set.

[2.3.3]#

  • Bug Fixes

    • Fixed the issue that ENET_SetSMI uses wrong clock source to calculate the divisor.

[2.3.2]#

  • New features

    • Added hardware checksum acceleration support.

  • Bug Fixes

    • Fixed the issue that enable/disable interrupt APIs miss part of configuration.

[2.3.1]#

  • Improvements

    • update ENET_SetSYSControl to support mcx family.

[2.3.0]#

  • Improvements

    • Added MDIO access wrapper APIs for ease of use.

[2.2.0]#

  • Bug Fixes

    • Corrected the timestamp retrieving code in ReadFrame.

  • New Features

    • Supported zero copy Rx with new APIs.

  • Improvements

    • Removed 4 bytes CRC data in ReadFrame function, not give them to user.

    • Deleted previous timestamp rings which store Tx/Rx timestamp temporarily for further retrieving. Now get Rx timestamp directly with receiving frame API, and get Tx timestamp in Tx over interrupt handler callback.

    • Added channel parameter for the SendFrame function, let user to decide which kind of frame can be sent from specified channel.

    • Supported scattered Tx buffers and more Tx configurations in SendFrame which aren’t integrated.

    • Adjusted the callback location in Tx reclaim function. When use multiple BDs for Tx, only last BD transmit over interrupt event calls the callback. It simplifies the usage of Tx reclaiming.

    • Added interrupt configuration in config parameter for ENET_Init() to simplify the interrupt enable.

    • Changed the Tx/Rx descriptor name to common name rather than previous read format name which make user confused when driver uses it as write-back format.

[2.1.5]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 3.1,5.8,8.4,8.6,10.1,10.3,10.4,10.6,10.8,11.6,11.9,12.2,14.4,15.6,17.7,21.15.

[2.1.4]#

  • Bug Fixes

    • Fixed the MDC clock divider setting issue occurring when core clock range exceeds 150M.

[2.1.3]#

  • In ENET_StartRxTx, updated to enable TX and RX at the same time to avoid issue where ENET module could not work under 10 M.

  • Changed to use CLOCK_GetCoreSysClkFreq() instead of SystemCoreClock to get accurate core clock.

[2.1.2]#

  • Bug Fixes

    • Fixed ENET receive issue where it sometimes lost some unicast packets. The issue is caused by the program timing issue for writing MAC_ADDR_LOW and MAC_ADDR_HIGH.

[2.1.1]#

  • New Features

    • Added a control macro to enable/disable the CLOCK code in current driver.

[2.1.0]#

  • New Features

    • Added two APIs to set the ENET to ACCPET or reject the multicast frames.

[2.0.0]#

  • Initial version.


FLEXCOMM#

[2.0.3]#

  • New Features

    • Added common IRQ handler entry FLEXCOMM_DriverIRQHandler.

[2.0.2]#

  • Bug Fixes

    • Fixed typos in FLEXCOMM15_DriverIRQHandler().

    • Fixed MISRA issues.

      • Fixed rules 10.1, 10.3, 10.4, 10.7, 10.8, 11.3, 11.6, 11.8, 11.9, 13.5.

  • Improvements

    • Added instance calculation in FLEXCOMM16_DriverIRQHandler() to align with Flexcomm 14 and 15.

[2.0.1]#

  • Improvements

    • Added more IRQHandler code in drivers to adapt new devices.

[2.0.0]#

  • Initial version.


FMEAS#

[2.1.2]#

  • Improvements

    • Replace macros with inline functions for clock count retrieval.

  • Bug Fixes

    • Fixed violations of the CERT INT30-C INT31-C.

[2.1.1]#

  • Bug Fixes

    • MISRA C-2012 issues fixed: rule 10.4, rule 10.8.

[2.1.0]#

  • Updated “FMEAS_GetFrequency”,”FMEAS_StartMeasure”,”FMEAS_IsMeasureComplete” API and add definition to match ASYNC_SYSCON.

[2.0.0]#

  • Initial version ported from LPCOpen.


GINT#

[2.1.2]#

  • New Features

    • Added common IRQ handler entry GINT_DriverIRQHandler.

[2.1.1]#

  • Improvements

    • Added support for platforms with PORT_POL and PORT_ENA registers without arrays.

[2.1.0]#

  • Improvements

    • Updated for platforms which only has one port.

[2.0.3]#

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 10.8.

[2.0.2]#

  • Bug Fixes

    • Fixed issue for MISRA-2012 check.

      • Fixed rule 17.7.

[2.0.1]#

  • Added control macro to enable/disable the RESET and CLOCK code in current driver.

[2.0.0]#

  • Initial version.


GPIO#

[2.1.7]#

  • Improvements

    • Enhanced GPIO_PinInit to enable clock internally.

[2.1.6]#

  • Bug Fixes

    • Clear bit before set it within GPIO_SetPinInterruptConfig() API.

[2.1.5]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 3.1, 10.6, 10.7, 17.7.

[2.1.4]#

  • Improvements

    • Added API GPIO_PortGetInterruptStatus to retrieve interrupt status for whole port.

    • Corrected typos in header file.

[2.1.3]#

  • Improvements

    • Updated “GPIO_PinInit” API. If it has DIRCLR and DIRSET registers, use them at set 1 or clean 0.

[2.1.2]#

  • Improvements

    • Removed deprecated APIs.

[2.1.1]#

  • Improvements

    • API interface changes:

      • Refined naming of APIs while keeping all original APIs, marking them as deprecated. Original APIs will be removed in next release. The mainin change is updating APIs with prefix of _PinXXX() and _PorortXXX

[2.1.0]#

  • New Features

    • Added GPIO initialize API.

[2.0.0]#

  • Initial version.


I2C#

[2.3.4]#

  • Bug Fixes

    • Added internal reset of master function after arbitration lost in I2C_MasterTransferHandleIRQ(), otherwise the STAT[MSTARBLOSS] is not set in next transfer.

[2.3.3]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.1.

    • Fixed issue that if master only sends address without data during I2C interrupt transfer, address nack cannot be detected.

[2.3.2]#

  • Improvement

    • Enable or disable timeout option according to enableTimeout.

  • Bug Fixes

    • Fixed timeout value calculation error.

    • Fixed bug that the interrupt transfer cannot recover from the timeout error.

[2.3.1]#

  • Improvement

    • Before master transfer with transactional APIs, enable master function while disable slave function and vise versa for slave transfer to avoid the one affecting the other.

  • Bug Fixes

    • Fixed bug in I2C_SlaveEnable that the slave enable/disable should not affect the other register bits.

[2.3.0]#

  • Improvement

    • Added new return codes kStatus_I2C_EventTimeout and kStatus_I2C_SclLowTimeout, and added the check for event timeout and SCL timeout in I2C master transfer.

    • Fixed bug in slave transfer that the address match event should be invoked before not after slave transmit/receive event.

[2.2.0]#

  • New Features

    • Added enumeration _i2c_status_flags to include all previous master and slave status flags, and added missing status flags.

    • Modified I2C_GetStatusFlags to get all I2C flags.

    • Added API I2C_ClearStatusFlags to clear all clearable flags not just master flags.

    • Modified master transactional APIs to enable bus event timeout interrupt during transfer, to avoid glitch on bus causing transfer hangs indefinitely.

  • Bug Fixes

    • Fixed bug that status flags and interrupt enable masks share the same enumerations by adding enumeration _i2c_interrupt_enable for all master and slave interrupt sources.

[2.1.0]#

  • Bug Fixes

    • Fixed bug that during master transfer, when master is nacked during slave probing or sending subaddress, the return status should be kStatus_I2C_Addr_Nak rather than kStatus_I2C_Nak.

  • Bug Fixes

    • Fixed MISRA issues.

      • Fixed rules 10.1, 10.4, 13.5.

  • New Features

    • Added macro I2C_MASTER_TRANSMIT_IGNORE_LAST_NACK, so that user can configure whether to ignore the last byte being nacked by slave during master transfer.

[2.0.8]#

  • Bug Fixes

    • Fixed I2C_MasterSetBaudRate issue that MSTSCLLOW and MSTSCLHIGH are incorrect when MSTTIME is odd.

[2.0.7]#

  • Bug Fixes

    • Two dividers, CLKDIV and MSTTIME are used to configure baudrate. According to reference manual, in order to generate 400kHz baudrate, the clock frequency after CLKDIV must be less than 2mHz. Fixed the bug that, the clock frequency after CLKDIV may be larger than 2mHz using the previous calculation method.

    • Fixed MISRA 10.1 issues.

    • Fixed wrong baudrate calculation when feature FSL_FEATURE_I2C_PREPCLKFRG_8MHZ is enabled.

[2.0.6]#

  • New Features

    • Added master timeout self-recovery support for feature FSL_FEATURE_I2C_TIMEOUT_RECOVERY.

  • Bug Fixes

    • Eliminated IAR Pa082 warning.

    • Fixed MISRA issues.

      • Fixed rules 10.1, 10.3, 10.4, 10.7, 10.8, 11.3, 11.6, 11.8, 11.9, 13.5.

[2.0.5]#

  • Bug Fixes

    • Fixed wrong assignment for datasize in I2C_InitTransferStateMachineDMA.

    • Fixed wrong working flow in I2C_RunTransferStateMachineDMA to ensure master can work in no start flag and no stop flag mode.

    • Fixed wrong working flow in I2C_RunTransferStateMachine and added kReceiveDataBeginState in _i2c_transfer_states to ensure master can work in no start flag and no stop flag mode.

    • Fixed wrong handle state in I2C_MasterTransferDMAHandleIRQ. After all the data has been transfered or nak is returned, handle state should be changed to idle.

  • Improvements

    • Rounded up the calculated divider value in I2C_MasterSetBaudRate.

[2.0.4]#

  • Improvements

    • Updated the I2C_WATI_TIMEOUT macro to unified name I2C_RETRY_TIMES

    • Updated the “I2C_MasterSetBaudRate” API to support baudrate configuration for feature QN9090.

  • Bug Fixes

    • Fixed build warnning caused by uninitialized variable.

    • Fixed COVERITY issue of unchecked return value in I2C_RTOS_Transfer.

[2.0.3]#

  • Improvements

    • Unified the component full name to FLEXCOMM I2C(DMA/FREERTOS) driver.

[2.0.2]#

  • Improvements

    • In slave IRQ:

      1. Changed slave receive process to first set the I2C_SLVCTL_SLVCONTINUE_MASK to acknowledge the received data, then do data receive.

      2. Improved slave transmit process to set the I2C_SLVCTL_SLVCONTINUE_MASK immediately after writing the data.

[2.0.1]#

  • Improvements

    • Added I2C_WATI_TIMEOUT macro to allow users to specify the timeout times for waiting flags in functional API and blocking transfer API.

[2.0.0]#

  • Initial version.


I2S#

[2.3.2]#

  • Bug Fixes

    • Fixed warning for comparison between pointer and integer.

[2.3.1]#

  • Bug Fixes

    • Updated the value of TX/RX software transfer state machine after transfer contents are submitted to avoid race condition.

[2.3.0]#

  • Improvements

    • Added api I2S_InstallDMADescriptorMemory/I2S_TransferSendLoopDMA/I2S_TransferReceiveLoopDMA to support loop transfer.

    • Added api I2S_EmptyTxFifo to support blocking flush tx fifo.

    • Updated api I2S_TransferAbortDMA by removed the blocking flush tx fifo from this function.

  • Bug Fixes

    • Removed the while loop in abort transfer function to fix the dead loop issue under specific user case.

[2.2.2]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 8.4.

[2.2.1]#

  • Improvements

    • Added feature FSL_FEATURE_FLEXCOMM_INSTANCE_I2S_SUPPORT_SECONDARY_CHANNELn for the SOC has parts of instance support secondary channel.

  • Bug Fixes

    • Added volatile statement for the state variable of i2s_handle and enable the mainline channel pair before enable interrupt to avoid the issue of code excution reordering which may cause the interrupt generated unexpectedly.

[2.2.0]#

  • Improvements

    • Added 8/16/24 bits mono data format transfer support in I2S driver.

    • Added new apis I2S_SetBitClockRate.

  • Bug Fixes

    • Fixed the PA082 build warning.

    • Fixed the sign-compare warning.

    • Fixed violations of the MISRA C-2012 rules 10.4, 10.8, 11.9, 10.1, 11.3, 13.5, 11.8, 10.3, 10.7.

    • Fixed the Operand don’t affect result Coverity issue.

[2.1.0]#

  • Improvements

    • Added a feature for the FLEXCOMM which supports I2S and has interconnection with DMIC.

    • Used a feature to control PDMDATA instead of I2S_CFG1_PDMDATA.

    • Added member bytesPerFrame in i2s_dma_handle_t, used for DMA transfer width configure, instead of using sizeof(uint32_t) hardcode.

    • Used the macro provided by DMA driver to define the I2S DMA descriptor.

  • Bug Fixes

    • Fixed the issue that I2S DMA driver always generated duplicate callback.

[2.0.3]#

  • New Features

    • Added a feature to remove configuration for the second channel on LPC51U68.

[2.0.2]#

  • New Features

    • Added ENABLE_IRQ handle after register I2S interrupt handle.

[2.0.1]#

  • Improvements

    • Unified the component full name to FLEXCOMM I2S (DMA) driver.

[2.0.0]#

  • Initial version.


I2S_DMA#

[2.3.3]#

  • Bug Fixes

    • Fixed data size limit does not match the macro DMA_MAX_TRANSFER_BYTES issue.

[2.3.2]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.3.

[2.3.1]#

  • Refer I2S driver change log 2.0.1 to 2.3.1


IAP#

[2.0.7]#

  • Bug Fixes

    • Fixed IAP_ReinvokeISP bug that can’t support UART ISP auto baud detection.

[2.0.6]#

  • Bug Fixes

    • Fixed IAP_ReinvokeISP wrong parameter setting.

[2.0.5]#

  • New Feature

    • Added support config flash memory access time.

[2.0.4]#

  • Bug Fixes

    • Fixed the violations of MISRA 2012 rules 9.1

[2.0.3]#

  • New Features

    • Added support for LPC 845’s FAIM operation.

    • Added support for LPC 80x’s fixed reference clock for flash controller.

    • Added support for LPC 5411x’s Read UID command useless situation.

  • Improvements

    • Improved the document and code structure.

  • Bug Fixes

    • Fixed the violations of MISRA 2012 rules:

      • Rule 10.1 10.3 10.4 17.7

[2.0.2]#

  • New Features

    • Added an API to read generated signature.

  • Bug Fixes

    • Fixed the incorrect board support of IAP_ExtendedFlashSignatureRead().

[2.0.1]#

  • New Features

    • Added an API to read factory settings for some calibration registers.

  • Improvements

    • Updated the size of result array in part APIs.

[2.0.0]#

  • Initial version.


INPUTMUX#

[2.0.10]#

  • Bug Fixes

    • Fixed CERT-C violations.

[2.0.9]#

  • Improvements

    • Use INPUTMUX_CLOCKS to initialize the inputmux module clock to adapt to multiple inputmux instances.

    • Modify the API base type from INPUTMUX_Type to void.

[2.0.8]#

  • Improvements

    • Updated a feature macro usage for function INPUTMUX_EnableSignal.

[2.0.7]#

  • Improvements

    • Release peripheral from reset if necessary in init function.

[2.0.6]#

  • Bug Fixes

    • Fixed the documentation wrong in API INPUTMUX_AttachSignal.

[2.0.5]#

  • Bug Fixes

    • Fixed build error because some devices has no sct.

[2.0.4]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rule 10.4, 12.2 in INPUTMUX_EnableSignal() function.

[2.0.3]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.4, 10.7, 12.2.

[2.0.2]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.4, 12.2.

[2.0.1]#

  • Support channel mux setting in INPUTMUX_EnableSignal().

[2.0.0]#

  • Initial version.


IOCON#

[2.2.1]#

  • Improvements

    • Added macros IOCON_INV_DI and IOCON_OPENDRAIN_DI

[2.2.0]#

  • Improvements

    • Removed duplicate macro defintions.

    • Renamed ‘IOCON_I2C_SLEW’ macro to ‘IOCON_I2C_MODE’ to match its companion ‘IOCON_GPIO_MODE’. The original is kept as a deprecated symbol.

[2.1.2]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.3.

[2.1.1]#

  • Updated left shift format with mask value instead of a constant value to automatically adapt to all platforms.

[2.1.0]#

  • Added a new IOCON_PinMuxSet() function with a feature IOCON_ONE_DIMENSION for LPC845MAX board.

[2.0.0]#

  • Initial version.


LPC_LCDC#

[2.0.2]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 3.1, 10.3, 10.4, 10.6, 10.7, 10.8, 14.4, 17.7.

[2.0.1]#

  • New Features

    • Added a control macro to enable/disable the RESET and CLOCK code in current driver.

[2.0.0]#

  • Initial version.


MCAN#

[2.4.4]#

  • New Features

    • Added common IRQ handler entry MCAN_DriverIRQHandler.

[2.4.3]#

  • Bug Fixes

    • Fixed violations of the CERT INT30-C INT31-C.

  • Improvements

    • Simplified MCAN_SetMessageRamConfig code implementation.

[2.4.2]#

  • Bug Fixes

    • Fixed MISRA issue rule-10.3, rule-10.6, rule-10.7 and rule-15.7.

[2.4.1]#

  • Bug Fixes

    • Fixed incorrect fifo1 status on message lost.

[2.4.0]#

  • Improvements

    • Add MCAN_CalculateSpecifiedTimingValues() API to get CAN bit timing parameter with user-defined settings.

    • Add MCAN_FDCalculateSpecifiedTimingValues() API to get CANFD bit timing parameter with user-defined settings.

[2.3.2]#

  • Bug Fixes

    • Fix MISRA C-2012 issue 10.1 and 10.4.

[2.3.1]#

  • Bug Fixes

    • Fixed the issue that MCAN_TransferSendNonBlocking() API can’t send remote frame.

[2.3.0]#

  • Improvements

    • Add MCAN_SetMessageRamConfig() API to perform global message RAM configure.

    • Add MCAN_EnterInitialMode() API.

[2.2.0]#

  • Improvements

    • Add MCAN_SetBaudRate/MCAN_SetBaudRateFD APIs to make users easy to set CAN baud rate.

[2.1.8]#

  • Bug Fixes

    • Add check FIFO status code in MCAN_ReadRxFifo() to avoid read back empty frame and wrong trigger the FIFO index increase.

[2.1.7]#

  • Bug Fixes

    • Fixed the clear error flags issue in MCAN_TransferHandleIRQ() API.

    • Fixed the Solve Tx interrupt issue in MCAN_TransferHandleIRQ() API which may abort the unhandled transfers.

    • Remove disable global tx interrupt from MCAN_TransferAbortSend API.

[2.1.6]#

  • Bug Fixes

    • Fixed the issue of writing 1 in the following functions.

    • MCAN_TransmitAddRequest

    • MCAN_TransmitCancelRequest

    • MCAN_ClearRxBufferStatusFlag

[2.1.5]#

  • Bug Fixes

    • Fix MISRA C-2012 issue.

[2.1.4]#

  • Improvements

    • Updated improve timing APIs to make it can calculate the CiA recommended timing configuration.

    • Implement Transmitter Delay Compensation feature.

    • Modify the default baudRateFD value to 2M.

  • Bug Fixes

    • Fixed the code error issue in MCAN_ClearStatusFlag() to avoid clear all flags.

[2.1.3]#

  • Bug Fixes

    • Fixed the code error issue and simplified the algorithm in improved timing APIs.

      • MCAN_CalculateImprovedTimingValues

      • MCAN_FDCalculateImprovedTimingValues

[2.1.2]#

  • Bug Fixes

    • Fixed the non-divisible case in improved timing APIs.

      • MCAN_CalculateImprovedTimingValues

      • MCAN_FDCalculateImprovedTimingValues

[2.1.1]#

  • Bug Fixes

    • MISRA C-2012 issue check.

      • Fixed rules, containing: rule-10.1, rule-10.3, rule-10.4, rule-10.6, rule-10.7, rule-10.8, rule-11.9, rule-14.4, rule-15.5, rule-15.6, rule-15.7, rule-17.7, rule-18.4, rule-2.2, rule-21.15, rule-5.8, rule-8.3.

      • Fixed the Coverity issue of BAD_SHIFT in MCAN.

      • Fixed the issue of Pa082 warning.

      • Fixed the issue of dropping interrupt flags in handler function.

[2.1.0]#

  • Bug Fixes

    • Fixed Coverity issue FORWARD_NULL.

    • Fixed Clang issue.

    • Fixed legacy issue in the driver and changed default bus data baud rate for CANFD.

  • Improvements

    • Implemented feature for improved timing configuration.

[2.0.3]#

  • Improvements

    • Used memset to initialize the structure before using.

    • Added function definition comment in c file.

    • Updated source file license to SPDX BSD_3.

    • Corrected capital mistake of Fifo and fifo.

    • Reset the MCAN module in LPC drivers after clock enable.

[2.0.2]#

  • Bug Fixes

    • Picked MISRA fixed in release 8 branch.

    • MISRA C 2012 fixed regarding FlexCAN and MCAN address update.

  • Improvements

    • Implemented for delay/retry in MCAN driver.

[2.0.1]#

  • Improvements

    • LPC54608 chip did not support the FD feature, so added a feature macro for it.

[2.0.0]#

  • Initial version.


MRT#

[2.0.5]#

  • Bug Fixes

    • Fixed CERT INT31-C violations.

[2.0.4]#

  • Improvements

    • Don’t reset MRT when there is not system level MRT reset functions.

[2.0.3]#

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rule 10.1 and 10.4.

    • Fixed the wrong count value assertion in MRT_StartTimer API.

[2.0.2]#

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rule 10.4.

[2.0.1]#

  • Added control macro to enable/disable the RESET and CLOCK code in current driver.

[2.0.0]#

  • Initial version.


OTP#

[2.0.1]#

  • Bug Fixes

    • Fixed MISRA-C 2012 violations.

[2.0.0]#

  • Initial version.


PINT#

[2.3.1]#

  • New Features

    • Added common IRQ handler entry PINT_DriverIRQHandler.

[2.3.0]#

  • Improvements

    • Add API PINT_EnableInterruptByIndex and PINT_DisableInterruptByIndex to provide more granular interrupt control.

[2.2.0]#

  • Fixed

    • Fixed the issue that clear interrupt flag when it’s not handled. This causes events to be lost.

  • Changed

    • Used one callback for one PINT instance. It’s unnecessary to provide different callbacks for all PINT events.

[2.1.13]#

  • Improvements

    • Added instance array for PINT to adapt more devices.

    • Used release reset instead of reset PINT which may clear other related registers out of PINT.

[2.1.12]#

  • Bug Fixes

    • Fixed coverity issue.

[2.1.11]#

  • Bug Fixes

    • Fixed MISRA C-2012 rule 10.7 violation.

[2.1.10]#

  • New Features

    • Added the driver support for MCXN10 platform with combined interrupt handler.

[2.1.9]#

  • Bug Fixes

    • Fixed MISRA-2012 rule 8.4.

[2.1.8]#

  • Bug Fixes

    • Fixed MISRA-2012 rule 10.1 rule 10.4 rule 10.8 rule 18.1 rule 20.9.

[2.1.7]#

  • Improvements

    • Added fully support for the SECPINT, making it can be used just like PINT.

[2.1.6]#

  • Bug Fixes

    • Fixed the bug of not enabling common pint clock when enabling security pint clock.

[2.1.5]#

  • Bug Fixes

    • Fixed issue for MISRA-2012 check.

      • Fixed rule 10.1 rule 10.3 rule 10.4 rule 10.8 rule 14.4.

    • Changed interrupt init order to make pin interrupt configuration more reasonable.

[2.1.4]#

  • Improvements

    • Added feature to control distinguish PINT/SECPINT relevant interrupt/clock configurations for PINT_Init and PINT_Deinit API.

    • Swapped the order of clearing PIN interrupt status flag and clearing pending NVIC interrupt in PINT_EnableCallback and PINT_EnableCallbackByIndex function.

    • Bug Fixes

      • Fixed build issue caused by incorrect macro definitions.

[2.1.3]#

  • Bug fix:

    • Updated PINT_PinInterruptClrStatus to clear PINT interrupt status when the bit is asserted and check whether was triggered by edge-sensitive mode.

    • Write 1 to IST corresponding bit will clear interrupt status only in edge-sensitive mode and will switch the active level for this pin in level-sensitive mode.

    • Fixed MISRA c-2012 rule 10.1, rule 10.6, rule 10.7.

    • Added FSL_FEATURE_SECPINT_NUMBER_OF_CONNECTED_OUTPUTS to distinguish IRQ relevant array definitions for SECPINT/PINT on lpc55s69 board.

    • Fixed PINT driver c++ build error and remove index offset operation.

[2.1.2]#

  • Improvement:

    • Improved way of initialization for SECPINT/PINT in PINT_Init API.

[2.1.1]#

  • Improvement:

    • Enabled secure pint interrupt and add secure interrupt handle.

[2.1.0]#

  • Added PINT_EnableCallbackByIndex/PINT_DisableCallbackByIndex APIs to enable/disable callback by index.

[2.0.2]#

  • Added control macro to enable/disable the RESET and CLOCK code in current driver.

[2.0.1]#

  • Bug fix:

    • Updated PINT driver to clear interrupt only in Edge sensitive.

[2.0.0]#

  • Initial version.


POWER#

[2.1.0]#

  • New features

    • Added BOD control APIs.

[2.0.0]#

  • initial version.


PUF#

[2.2.0]#

  • Add support for kPUF_KeySlot4.

  • Add new PUF_ClearKey() function, that clears a desired PUF internal HW key register.

[2.1.6]#

  • Changed wait time in PUF_Init(), when initialization fails it will try PUF_Powercycle() with shorter time. If this shorter time will also fail, initialization will be tried with worst case time as before.

[2.1.5]#

  • Use common SDK delay in puf_wait_usec().

[2.1.4]#

  • Replace register uint32_t ticksCount with volatile uint32_t ticksCount in puf_wait_usec() to prevent optimization out delay loop.

[2.1.3]#

  • Fix MISRA C-2012 issue.

[2.1.2]#

  • Update: Add automatic big to little endian swap for user (pre-shared) keys destinated to secret hardware bus (PUF key index 0).

[2.1.1]#

  • Fix ARMGCC build warning .

[2.1.0]#

  • Align driver with PUF SRAM controller registers on LPCXpresso55s16.

  • Update initizalition logic .

[2.0.3]#

  • Fix MISRA C-2012 issue.

[2.0.2]#

  • New feature:

    • Add PUF configuration structure and support for PUF SRAM controller.

  • Improvements:

    • Remove magic constants.

[2.0.1]#

  • Bug Fixes:

    • Fixed puf_wait_usec function optimization issue.

[2.0.0]#

  • Initial version.


RESET#

[2.4.0]#

  • Improvements

    • Add RESET_ReleasePeripheralReset API.

[2.0.1]#

  • Update component full_name to “Reset Driver”.

[2.0.0]#

  • initial version.


RIT#

[2.1.2]#

  • Bug Fixes

    • Fixed CERT INT31-C violations.

[2.1.1]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.3, 11.9, 17.7.

[2.1.0]#

  • Bug Fixes

    • Fixed issue for wrong implementation of clearing counter API in RIT driver.

[2.0.2]#

  • New Features

    • Added control macro to enable/disable the CLOCK code in current driver.

[2.0.1]#

  • Bug Fixes

    • Fixed incorrect comments of some APIs.

[2.0.0]#

  • Initial version.


RNG#

[2.1.0]#

  • Renamed function RNG_GetRandomData() to RNG_GetRandomDataWord(). Added function RNG_GetRandomData() which discarding next 32 words after reading RNG register which results into better entropy, as is recommended in UM.

  • API is aligned with other RNG driver, having similar functionality as other RNG/TRNG drivers.

[2.0.0]#

  • Initial version.


RTC#

[2.2.0]#

  • New Features

    • Created new APIs for the RTC driver.

      • RTC_EnableSubsecCounter

      • RTC_GetSubsecValue

[2.1.3]#

  • Bug Fixes

    • Fixed issue that RTC_GetWakeupCount may return wrong value.

[2.1.2]#

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 10.1, 10.4 and 10.7.

[2.1.1]#

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 10.3 and 11.9.

[2.1.0]#

  • Bug Fixes

    • Created new APIs for the RTC driver.

      • RTC_EnableTimer

      • RTC_EnableWakeUpTimerInterruptFromDPD

      • RTC_EnableAlarmTimerInterruptFromDPD

      • RTC_EnableWakeupTimer

      • RTC_GetEnabledWakeupTimer

      • RTC_SetSecondsTimerMatch

      • RTC_GetSecondsTimerMatch

      • RTC_SetSecondsTimerCount

      • RTC_GetSecondsTimerCount

    • deprecated legacy APIs for the RTC driver.

      • RTC_StartTimer

      • RTC_StopTimer

      • RTC_EnableInterrupts

      • RTC_DisableInterrupts

      • RTC_GetEnabledInterrupts

[2.0.0]#

  • Initial version.


SCTIMER#

[2.5.4]#

  • New Features

    • Added common IRQ handler entry SCTIMER_DriverIRQHandler.

[2.5.3]#

  • Bug Fixes

    • Fixed overflow error in SCT_EV_STATE_STATEMSKn macro definition.

[2.5.2]#

  • Bug Fixes

    • Fixed CERT INT31-C violation issues.

[2.5.1]#

  • Bug Fixes

    • Fixed bug in SCTIMER_SetupCaptureAction: When kSCTIMER_Counter_H is selected, events 12-15 and capture registers 12-15 CAPn_H field can’t be used.

[2.5.0]#

  • Improvements

    • Add SCTIMER_GetCaptureValue API to get capture value in capture registers.

[2.4.9]#

  • Improvements

    • Supported platforms which don’t have system level SCTIMER reset.

[2.4.8]#

  • Bug Fixes

    • Fixed the issue that the SCTIMER_UpdatePwmDutycycle() can’t writes MATCH_H bit and RELOADn_H.

[2.4.7]#

  • Bug Fixes

    • Fixed the issue that the SCTIMER_UpdatePwmDutycycle() can’t configure 100% duty cycle PWM.

[2.4.6]#

  • Bug Fixes

    • Fixed the issue where the H register was not written as a word along with the L register.

    • Fixed the issue that the SCTIMER_SetCOUNTValue() is not configured with high 16 bits in unify mode.

[2.4.5]#

  • Bug Fixes

    • Fix SCT_EV_STATE_STATEMSKn macro build error.

[2.4.4]#

  • Bug Fixes

    • Fix MISRA C-2012 issue 10.8.

[2.4.3]#

  • Bug Fixes

    • Fixed the wrong way of writing CAPCTRL and REGMODE registers in SCTIMER_SetupCaptureAction.

[2.4.2]#

  • Bug Fixes

    • Fixed SCTIMER_SetupPwm 100% duty cycle issue.

[2.4.1]#

  • Bug Fixes

    • Fixed the issue that MATCHn_H bit and RELOADn_H bit could not be written.

[2.4.0]#

[2.3.0]#

  • Bug Fixes

    • Fixed the potential overflow issue of pulseperiod variable in SCTIMER_SetupPwm/SCTIMER_UpdatePwmDutycycle API.

    • Fixed the issue of SCTIMER_CreateAndScheduleEvent API does not correctly work with 32 bit unified counter.

    • Fixed the issue of position of clear counter operation in SCTIMER_Init API.

  • Improvements

    • Update SCTIMER_SetupPwm/SCTIMER_UpdatePwmDutycycle to support generate 0% and 100% PWM signal.

    • Add SCTIMER_SetupEventActiveDirection API to configure event activity direction.

    • Update SCTIMER_StartTimer/SCTIMER_StopTimer API to support start/stop low counter and high counter at the same time.

    • Add SCTIMER_SetCounterState/SCTIMER_GetCounterState API to write/read counter current state value.

    • Update APIs to make it meaningful.

      • SCTIMER_SetEventInState

      • SCTIMER_ClearEventInState

      • SCTIMER_GetEventInState

[2.2.0]#

  • Improvements

    • Updated for 16-bit register access.

[2.1.3]#

  • Bug Fixes

    • Fixed the issue of uninitialized variables in SCTIMER_SetupPwm.

    • Fixed the issue that the Low 16-bit and high 16-bit work independently in SCTIMER driver.

  • Improvements

    • Added an enumerable macro of unify counter for user.

      • kSCTIMER_Counter_U

    • Created new APIs for the RTC driver.

      • SCTIMER_SetupStateLdMethodAction

      • SCTIMER_SetupNextStateActionwithLdMethod

      • SCTIMER_SetCOUNTValue

      • SCTIMER_GetCOUNTValue

      • SCTIMER_SetEventInState

      • SCTIMER_ClearEventInState

      • SCTIMER_GetEventInState

    • Deprecated legacy APIs for the RTC driver.

      • SCTIMER_SetupNextStateAction

[2.1.2]#

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 10.3, 10.4, 10.6, 10.7, 11.9, 14.2 and 15.5.

[2.1.1]#

  • Improvements

    • Updated the register and macro names to align with the header of devices.

[2.1.0]#

  • Bug Fixes

    • Fixed issue where SCT application level Interrupt handler function is occupied by SCT driver.

    • Fixed issue where wrong value for INSYNC field inside SCTIMER_Init function.

    • Fixed issue to change Default value for INSYNC field inside SCTIMER_GetDefaultConfig.

[2.0.1]#

  • New Features

    • Added control macro to enable/disable the RESET and CLOCK code in current driver.

[2.0.0]#

  • Initial version.


SDIF#

[2.1.1]#

  • Bug Fixes

    • Fixed some code quality issues.

  • New Features

    • Added common IRQ handler entry SDIF_CommonDriverIRQHandler.

[2.1.0]#

  • Improvements

    • Removed reduntant member endianMode in sdif_config_t.

    • Added error status check in function SDIF_WaitCommandDone.

    • Fixed the read fifo data incomplete issue in interrupt non-dma mode.

[2.0.15]#

  • Bug Fixes

    • Cleared the interrupt status before enable the interrupt to avoid interrupt generate unexpectedly.

    • Fixed the SDIF_ReadDataPortBlocking blocking at wrong condition issue.

  • Improvements

    • Enabled the functionality of timeout parameter in SDIF_SendCommand.

    • Added the error recovery while sending sync clock command timeout.

[2.0.14]#

  • Improvements

    • Used different status code for command and data interrupt callback.

  • Bug Fixes

    • Fixed the DMA descriptor attribute field unreset when configuing the current transfer DMA descriptor issue which may cause the transfer terminate unexpected.

[2.0.13]#

  • Improvements

    • Disabled redundant interrupt per different transfer request.

    • Disabled interrupt and reset command/data pointer in handle when transfer completes.

  • Bug Fixes

    • Fixed the PA082 build warning.

    • Fixed violations of the MISRA C-2012 rules 14.4, 17.7, 10.4, 10.3, 10.8, 14.3, 10.1, 16.4, 15.7, 12.2, 11.3, 11.9.

[2.0.12]#

  • Bug Fixes

    • Fixed the issue that SDIF_ConfigClockDelay didn’t reset the delay field before write.

    • Removed useless fifo reset code in transfer function.

    • Fixed the divider overflow issue in function SDIF_SetCardClock.

[2.0.11]#

  • Improvements

    • Added API SDIF_GetEnabledInterruptStatus/SDIF_GetEnabledDMAInterruptStatus and used in SDIF_TransferHandleIRQ.

    • Removed useless members interruptFlags/dmaInterruptFlags in the sdif_handle_t.

    • Improved SDIF_SendCommand with return success directly when timeout is 0.

    • Added timeout error check when sending update clock command in SDIF_SetCardClock.

    • Removed START_CMD status polling for normal command sending in SDIF_TransferBloking/SDIF_TransferNonBlocking.

    • Disabled timeout parameter in function SDIF_SendCommand.

  • Bug Fixes

    • Added delay cycle for the default speed mode(400 K and 25 M) to fix the timing issue when different AHB clocks are configured.

[2.0.10]#

  • Bug Fixes

    • Fixed the issue that API SDIF_EnableCardClock could not clear the clock enable bit.

[2.0.9]#

  • Bug Fixes

    • Fixed MDK 66-D warning.

[2.0.8]#

  • New Features

    • Added control macro to enable/disable the RESET and CLOCK code in current driver.

    • Disabled useless interrupt while DMA is used.

    • Updated SDIF driver for one instance support two cards.

[2.0.7]#

  • Bug Fixes

    • Enlarged the timeout value to avoid a command conflict issue.

[2.0.6]#

  • Bug Fixes

    • Removed assert(srcClock_Hz <= FSL_FEATURE_SDIF_MAX_SOURCE_CLOCK).

    • Used hardware reset instead of software reset during initialization.

[2.0.5]#

  • New Features

    • Added non-word aligned data address and DMA descriptor address transfer support. Once one of the above addresses is not aligned, switch to host transfer mode.

  • Bug Fixes

    • Fixed the issue that DMA suspended during initialization.

    • Removed useless memset function call.

[2.0.4]#

  • Improvements

    • Added cardInserted/cardRemoved callback function.

    • Added host base address/user data parameter for all call back functions.

[2.0.3]#

  • Improvements

    • Improved Clock Delay macro to allow the user to redefine and remove useless delay for clock below 25 MHz.

[2.0.2]#

  • Bug Fixes

    • Fixed the issue that the status flag could not be cleared entirely after transfer complete.

[2.0.1]#

  • New Features

    • Improved interrupt transfer callback.

  • Bug Fixes

    • Added assert to limit the SDIF source clock below 52 MHz.

[2.0.0]#

  • Initial version.


SHA#

[2.3.2]#

  • Add -O2 optimization for GCC to sha_process_message_data_master(), because without it the function hangs under some conditions.

[2.3.1]#

  • Modified sha_process_message_data_master() to ensure that MEMCTRL will be written within 64 cycles of writing last word to INDATA as is mentioned in errata, even with different optimization levels.

[2.3.0]#

  • Modified SHA_Update to use blocking version of AHB Master mode when its available on chip. Added SHA_UpdateNonBlocking() function which uses nonblocking AHB Master mode.

  • Fixed incorrect calculation of SHA when calling SHA_Update multiple times when is CPU used to load data.

  • Added Reset into SHA_ClkInit and SHA_ClkDeinit function.

[2.2.2]#

  • Modified SHA_Finish function. While using pseudo DMA with maximum optimization, compiler optimize out condition. Which caused block in this function and did not check flag, which has been set in interrupt.

[2.2.1]#

  • MISRA C-2012 issue fix.

[2.2.0]#

  • Support MEMADDR pseudo DMA for loading input data in SHA_Update function (LPCXpresso54018 and LPCXpresso54628).

[2.1.1]#

  • MISRA C-2012 issue fixed: rule 10.3, 10.4, 11.9, 14.4, 16.4 and 17.7.

[2.1.0]#

  • Updated “sha_ldm_stm_16_words” “sha_one_block” API to match QN9090. QN9090 has no ALIAS register.

  • Added “SHA_ClkInit” “SHA_ClkInit”

[2.0.0]#

  • Initial version.


SPI#

[2.3.2]#

  • Bug Fixes

    • Fixed the txData from void * to const void * in transmit API

[2.3.1]#

  • Improvements

    • Changed SPI_DUMMYDATA to 0x00.

[2.3.0]#

  • Update version.

[2.2.2]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules.

[2.2.1]#

  • Bug Fixes

    • Fixed MISRA 2012 10.4 issue.

    • Added code to clear FIFOs before transfer using DMA.

[2.2.0]#

  • Bug Fixes

    • Fixed bug that slave gets stuck during interrupt transfer.

[2.1.1]#

  • Improvements

    • Added timeout mechanism when waiting certain states in transfer driver.

  • Bug Fixes

    • Fixed MISRA 10.1, 5.7 issues.

[2.1.0]#

  • Bug Fixes

    • Fixed Coverity issue of incrementing null pointer in SPI_TransferHandleIRQInternal.

    • Eliminated IAR Pa082 warnings.

    • Fixed MISRA issues.

      • Fixed rules 10.1, 10.3, 10.4, 10.7, 10.8, 11.3, 11.6, 11.8, 11.9, 13.5.

  • New Features

    • Modified the definition of SPI_SSELPOL_MASK to support the socs that have only 3 SSEL pins.

[2.0.4]#

  • Bug Fixes

    • Fixed the bug of using read only mode in DMA transfer. In DMA transfer mode, if transfer->txData is NULL, code attempts to read data from the address of 0x0 for configuring the last frame.

    • Fixed wrong assignment of handle->state. During transfer handle->state should be kSPI_Busy rather than kStatus_SPI_Busy.

  • Improvements

    • Rounded up the calculated divider value in SPI_MasterSetBaud.

[2.0.3]#

  • Improvements

    • Added “SPI_FIFO_DEPTH(base)” with more definition.

[2.0.2]#

  • Improvements

    • Unified the component full name to FLEXCOMM SPI(DMA/FREERTOS) driver.

[2.0.1]#

  • Changed the data buffer from uint32_t to uint8_t which matches the real applications for SPI DMA driver.

  • Added dummy data setup API to allow users to configure the dummy data to be transferred.

  • Added new APIs for half-duplex transfer function. Users can not only send and receive data by one API in polling/interrupt/DMA way, but choose either to transmit first or to receive first. Besides, the PCS pin can be configured as assert status in transmission (between transmit and receive) by setting the isPcsAssertInTransfer to true.

[2.0.0]#

  • Initial version.


SPI_DMA#

[2.2.3]#

  • Bug Fixes

    • Fixed the bug SPI_MasterTransferGetCountDMA and SPI_SlaveTransferGetCountDMA returns wrong count.

[2.2.2]#

  • Bug Fixes

    • Fixed the bug half duplex mode can’t be used if data size is larger than 1024 bytes.

[2.2.1]#

  • Bug Fixes

    • Fixed MISRA 2012 11.6 issue..

[2.2.0]#

  • Improvements

    • Supported dataSize larger than 1024 data transmit.


SPI Flash Interface#

[2.0.4]#

  • Bug Fixes

    • Add explicit boolean to integer conversions (? 1U : 0U) for enable flags in SPIFI control register.

    • Add explicit boolean to integer conversions (? 1U : 0U) for poll mode flag in command register.

    • Add safe type conversion with explicit masking for uint16_t to uint8_t narrowing conversion.

    • Follow INT31-C CERT coding standard for safe boolean to unsigned long conversions.

[2.0.3]#

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 10.3, 10.4, and 14.4.

[2.0.2]#

  • Bug Fixes

    • Fixed the command function set issue. After the command being set, there will be no wait for the CMD flag, as it may have been cleared by CS deassert.

[2.0.1]#

  • New Features

    • Added an API to read/write 1/2 Bytes data from/to SPIFI. This interface is useful for flash command, which only needs 1/2 Bytes data. The previous driver needed users to make sure of the minimum length being 4, which might cause issues in some flash commands.

[2.0.0]#

  • Initial version.


USART#

[2.9.0]#

  • New Features

    • Added support for RS-485 (configuration of OESEL, OEPOL, OETA in CFG register).

    • Added handling when a start is detected on the receiver input in USART_TransferHandleIRQ().

[2.8.5]#

  • Bug Fixes

    • Fixed race condition during call of USART_EnableTxDMA and USART_EnableRxDMA.

[2.8.4]#

  • Bug Fixes

    • Fixed exclusive access in USART_TransferReceiveNonBlocking and USART_TransferSendNonBlocking.

[2.8.3]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.3, 11.8.

[2.8.2]#

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 14.2.

[2.8.1]#

  • Bug Fixes

    • Fixed the Baud Rate Generator(BRG) configuration in 32kHz mode.

[2.8.0]#

  • New Features

    • Added the rx timeout interrupts and status flags of bus status.

    • Added new rx timeout configuration item in usart_config_t.

    • Added API USART_SetRxTimeoutConfig for rx timeout configuration.

  • Improvements

    • When the calculated baudrate cannot meet user’s configuration, lower OSR value is allewed to use.

[2.7.0]#

  • New Features

    • Added the missing interrupts and status flags of bus status.

    • Added the check of tx error, noise error framing error and parity error in interrupt handler.

[2.6.0]#

  • Improvements

    • Used separate data for TX and RX in usart_transfer_t.

  • Bug Fixes

    • Fixed bug that when ring buffer is used, if some data is received in ring buffer first before calling USART_TransferReceiveNonBlocking, the received data count returned by USART_TransferGetReceiveCount is wrong.

  • New Features

    • Added missing API USART_TransferGetSendCountDMA get send count using DMA.

[2.5.0]#

  • New Features

    • Added APIs USART_GetRxFifoCount/USART_GetTxFifoCount to get rx/tx FIFO data count.

    • Added APIs USART_SetRxFifoWatermark/USART_SetTxFifoWatermark to set rx/tx FIFO water mark.

  • Bug Fixes

    • Fixed DMA transfer blocking issue by enabling tx idle interrupt after DMA transmission finishes.

[2.4.0]#

  • New Features

    • Modified usart_config_t, USART_Init and USART_GetDefaultConfig APIs so that the hardware flow control can be enabled during module initialization.

  • Bug Fixes

    • Fixed MISRA 10.4 violation.

[2.3.1]#

  • Bug Fixes

    • Fixed bug that operation on INTENSET, INTENCLR, FIFOINTENSET and FIFOINTENCLR should use bitwise operation not ‘or’ operation.

    • Fixed bug that if rx interrupt occurrs before TX interrupt is enabled and after txDataSize is configured, the data will be sent early by mistake, thus TX interrupt will be enabled after data is sent out.

  • Improvements

    • Added check for baud rate’s accuracy that returns kStatus_USART_BaudrateNotSupport when the best achieved baud rate is not within 3% error of configured baud rate.

[2.3.0]#

  • New Features

    • Added APIs to configure 9-bit data mode, set slave address and send address.

    • Modified USART_TransferReceiveNonBlocking and USART_TransferHandleIRQ to use 9-bit mode in multi-slave system.

[2.2.0]#

  • New Features

    • Added the feature of supporting USART working at 32 kHz clocking mode.

  • Improvements

    • Modified USART_TransferHandleIRQ so that txState will be set to idle only when all data has been sent out to bus.

    • Modified USART_TransferGetSendCount so that this API returns the real byte count that USART has sent out rather than the software buffer status.

    • Added timeout mechanism when waiting for certain states in transfer driver.

  • Bug Fixes

    • Fixed MISRA 10.1 issues.

    • Fixed bug that operation on INTENSET, INTENCLR, FIFOINTENSET and FIFOINTENCLR should use bitwise operation not ‘or’ operation.

    • Fixed bug that if rx interrupt occurrs before TX interrupt is enabled and after txDataSize is configured, the data will be sent early by mistake, thus TX interrupt will be enabled after data is sent out.

[2.1.1]#

  • Improvements

    • Added check for transmitter idle in USART_TransferHandleIRQ and USART_TransferSendDMACallback to ensure all the data would be sent out to bus.

    • Modified USART_ReadBlocking so that if more than one receiver errors occur, all status flags will be cleared and the most severe error status will be returned.

  • Bug Fixes

    • Eliminated IAR Pa082 warnings.

    • Fixed MISRA issues.

      • Fixed rules 10.1, 10.3, 10.4, 10.7, 10.8, 11.3, 11.6, 11.8, 11.9, 13.5.

[2.1.0]#

  • New Features

    • Added features to allow users to configure the USART to synchronous transfer(master and slave) mode.

  • Bug Fixes

    • Modified USART_SetBaudRate to get more acurate configuration.

[2.0.3]#

  • New Features

    • Added new APIs to allow users to enable the CTS which determines whether CTS is used for flow control.

[2.0.2]#

  • Bug Fixes

    • Fixed the bug where transfer abort APIs could not disable the interrupts. The FIFOINTENSET register should not be used to disable the interrupts, so use the FIFOINTENCLR register instead.

[2.0.1]#

  • Improvements

    • Unified the component full name to FLEXCOMM USART (DMA/FREERTOS) driver.

[2.0.0]#

  • Initial version.


USART_DMA#

[2.6.0]#

  • Refer USART driver change log 2.0.1 to 2.6.0


UTICK#

[2.0.6]#

  • New Features

    • Added common IRQ handler entry UTICK_CommonDriverIRQHandler.

[2.0.5]#

  • Improvements

    • Improved for SOC RW610.

[2.0.4]#

  • Bug Fixes

    • Fixed compile fail issue of no-supporting PD configuration in utick driver.

[2.0.3]#

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rules: 8.4, 14.4, 17.7

[2.0.2]#

  • Added new feature definition macro to enable/disable power control in drivers for some devices have no power control function.

[2.0.1]#

  • Added control macro to enable/disable the CLOCK code in current driver.

[2.0.0]#

  • Initial version.


WWDT#

[2.1.11]#

  • Bug Fixes

    • Fixed CERT INT31-C static analysis finding by clamping boolean configuration values (WDEN/WDRESET/LOCK) to 0/1 before writing the MOD register in WWDT_Init.

[2.1.10]#

  • Bug Fixes

    • Chek WWDT_RSTS instead of FSL_FEATURE_WWDT_HAS_NO_RESET to determine whether the peripheral can be reset.

[2.1.9]#

  • Bug Fixes

    • Fixed violation of the MISRA C-2012 rule 10.4.

[2.1.8]#

  • Improvements

    • Updated the “WWDT_Init” API to add wait operation. Which can avoid the TV value read by CPU still be 0xFF (reset value) after WWDT_Init function returns.

[2.1.7]#

  • Bug Fixes

    • Fixed the issue that the watchdog reset event affected the system from PMC.

    • Fixed the issue of setting watchdog WDPROTECT field without considering the backwards compatibility.

    • Fixed the issue of clearing bit fields by mistake in the function of WWDT_ClearStatusFlags.

[2.1.5]#

  • Bug Fixes

    • deprecated a unusable API in WWWDT driver.

      • WWDT_Disable

[2.1.4]#

  • Bug Fixes

    • Fixed violation of the MISRA C-2012 rules Rule 10.1, 10.3, 10.4 and 11.9.

    • Fixed the issue of the inseparable process interrupted by other interrupt source.

      • WWDT_Init

[2.1.3]#

  • Bug Fixes

    • Fixed legacy issue when initializing the MOD register.

[2.1.2]#

  • Improvements

    • Updated the “WWDT_ClearStatusFlags” API and “WWDT_GetStatusFlags” API to match QN9090. WDTOF is not set in case of WD reset. Get info from PMC instead.

[2.1.1]#

  • New Features

    • Added new feature definition macro for devices which have no LCOK control bit in MOD register.

    • Implemented delay/retry in WWDT driver.

[2.1.0]#

  • Improvements

    • Added new parameter in configuration when initializing WWDT module. This parameter, which must be set, allows the user to deliver the WWDT clock frequency.

[2.0.0]#

  • Initial version.