ZPS_tsAplZdpFindNodeCacheRsp#
This structure is used to store Find_node_cache_rsp message data - a response to a call to the function ZPS_eAplZdpFindNodeCacheRequest(). This response indicates that the sending node holds ‘discovery information’ about a given network node in its primary discovery cache.
The ZPS_tsAplZdpFindNodeCacheRspstructure is detailed below.
typedef struct {
uint16 u16CacheNwkAddr;
uint16 u16NwkAddr;
uint64 u64IeeeAddr;
} ZPS_tsAplZdpFindNodeCacheRsp;
where:
u16CacheNwkAddris the network address of the remote node that sent the response.u16NwkAddris the network address of the node of interest (this is the network address that was specified in the request).u64IeeeAddris the IEEE address of the node of interest (this is the IEEE address that was specified in the request).
Parent topic:ZDP response structures