MCUXpresso SDK Documentation

csi_mipi_yuv

csi_mipi_yuv#

Overview#

This project shows how to use the CSI with MIPI_CSI. In this example, the camera device output pixel format is YUYV, the MIPI_CSI converts it to YUV internally and sends to CSI. In other words, the CSI input data bus width is 24-bit. The CSI saves the frame as 32-bit format XYUV8888. PXP is used to convert the XYUV to RGB565 and show in the LCD panel.

Supported Boards#

MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

  • RK055AHD091 panel or RK055MHD091 panel

  • OV5640 camera

Board settings

Connect the panel to J48 Connect camera to J2 Connect 5V power to J43, set J38 to 1-2

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build the project, the project uses RK055MHD091 by default, to use other panels, set the coresponding panel DEMO_PANEL_xxx(without ‘_SUPPORT’) to y in prj.conf under board example folder before project generation. The supported panels can be found in examples_boards<board>\project_segments\display_support\Kconfig.prjseg. Or change the macro DEMO_PANEL in mcux_config.h of the project, which number represents which panel can be found in display_support.h and mcux_config.h

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs, the screen shows the camera input frame.

MIMXRT1160-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1160-EVK board

  • Personal Computer

  • RK055AHD091 panel or RK055MHD091 panel

  • OV5640 camera

Board settings

Connect the panel to J48 Connect camera to J2 Connect 5V power to J43, set J38 to 1-2

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build the project, this project uses RK055MHD091 panel by default, to use the RK055AHD091 panel, change #define DEMO_PANEL 2 to #define DEMO_PANEL 0 in mcux_config.h.

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs, the screen shows the camera input frame.