power_manager_test_asymmetric_multiCore_bm_core#
Overview#
This example demonstrates the basic usage of the Power Manager framework for asymmetric multicore platforms. For such platforms, each one should use a copy of the Power Manager framework. Each copy of PM calculates the suitable power state for each core based on its constraints. The primary core is responsible for setting clock roots, configuring system pin mux, getting the target power state and timeout value from terminal, and using the Messaging Unit (MU) module to send the selected power state and timeout value from the primary core to the secondary core. The current consumption of each power state is aligned with the data provided in the DS. The demo shows how the various power mode switch to each other based on power manager framework. However, in actual low power use case, to save energy and reduce the consumption even more, many things can be done including:
Disable the clock for unnecessary module during low power mode. That means, programmer can disable the clocks before entering the low power mode and re-enable them after exiting the low power mode when necessary.
Disable the function for unnecessary part of a module when other part would keep working in low power mode. At the most time, more powerful function means more power consumption. For example, disable the digital function for the unnecessary pin mux, and so on.
Set the proper pin state (direction and logic level) according to the actual application hardware. Otherwise, the pin current would be activated unexpectedly waste some energy.
Other low power consideration based on the actual application hardware.
Debug pins(e.g SWD_DIO) would consume additional power, had better to disable related pins or disconnect them.
Supported Boards#
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
USB to Com Converter
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When running the demo, the debug console shows the menu to provide the desired operation.
Power Manager Multi-Core Bare-metal Demo.
Primary Core Boot. Previous setpoint is 0. Current setpoint is 0. Starting Second Core… Copy Secondary core image to address: 0x20200000, size: 11713 Second Core application has been started.
Please select the desired power mode: Press A to enter: Setpoint0, CM7 domain WAIT, CM4 domain WAIT Press B to enter: Setpoint1, CM7 domain STOP, CM4 domain WAIT Press C to enter: Setpoint10, CM7 domain SUSPEND, CM4 domain SUSPEND Press D to enter: Setpoint15, CM7 domain SUSPEND, CM4 domain SUSPEND
Waiting for power mode select…
Note: To debug in external flash, following steps are needed:
Select the flash target and compile.
Set the SW1: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J11.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to external flash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
Note: Flexspi_nor_debug and Flexspi_nor_release targets on armgcc toolchain need to click SW4(reset button) to run cases after downloading the image.