tmu_3_monitor_report#
Overview#
The TMU example shows how to configure TMU register to monitor and report the temperature from one remote temperature measurement sites located on the chip.
TMU has access to temperature measurement site strategically located on the chip. It monitors the site and can signal an alarm if a programmed threshold is ever exceeded.
Note: Before monitoring the temperature, we must programming the calibration table.
Supported Boards#
MCIMX93AUTO-EVK
Hardware requirements
USB Type-C cable
MCIMX93AUTO-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.
Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
Start TMU monitor report example.
Board immediate temperature is 35.85 celsius degree.
Board immediate temperature is 36.35 celsius degree.
Board immediate temperature is 36.85 celsius degree.
Board immediate temperature is 36.85 celsius degree.
Board immediate temperature is 36.85 celsius degree.
MCIMX93-EVK
Hardware requirements
USB Type-C cable
MCIMX93-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
Start TMU monitor report example.
Board immediate temperature is 35.85 celsius degree.
Board immediate temperature is 36.35 celsius degree.
Board immediate temperature is 36.85 celsius degree.
Board immediate temperature is 36.85 celsius degree.
Board immediate temperature is 36.85 celsius degree.
MCIMX93W-EVK
Hardware requirements
USB Type-C cable
MCIMX93W-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
Start TMU monitor report example.
Board immediate temperature is 35.85 celsius degree.
Board immediate temperature is 36.35 celsius degree.
Board immediate temperature is 36.85 celsius degree.
Board immediate temperature is 36.85 celsius degree.
Board immediate temperature is 36.85 celsius degree.
MCIMX93-QSB
Hardware requirements
USB Type-C cable
MCIMX93-QSB board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
Start TMU monitor report example.
Board immediate temperature is 35.85 celsius degree.
Board immediate temperature is 36.35 celsius degree.
Board immediate temperature is 36.85 celsius degree.
Board immediate temperature is 36.85 celsius degree.
Board immediate temperature is 36.85 celsius degree.