MCUXpresso SDK Documentation

wdt

Contents

wdt#

Overview#

The WDT example is to demonstrate usage of the MSDK WDT driver. In this example, the Watchdog Timer can be used to limit the duration within which a software task must complete. As soon as the timer started to count down, feed watchdog before the timer reaches zero.Otherwise the system reset will be generated. The Watchdog timer includes a non-maskable interrupt,and it will be generated when the counter reaches the WDOG_INT_THRESHOLD.