rtc_1#
Overview#
The RTC project is a simple demonstration program of the SDK RTC driver. It sets up the RTC hardware block to trigger an alarm after a user specified time period. The test will set the current date and time to a predefined value. The alarm will be set with reference to this predefined date and time.
Supported Boards#
FRDM-KE02Z40M
Hardware requirements
Mini/micro USB cable
FRDM-KE02Z40M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
RTC example: set up time to wake up an alarm.
Current datetime: 2014-12-25 19:00:00
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19:01:11
Alarm occurs !!!! Current datetime: 2014-12-25 19:01:11
Please input the number of second to wait for alarm
The second must be positive value
...............................................
...............................................