MCUXpresso SDK Documentation

qtmr_outputpwm

qtmr_outputpwm#

Overview#

The QTMR project is a demonstration program of the SDK QTMR driver’s output variable frequency pwm feature by interrupt. The example also up one QTMR channel to output pwm. The user should probe a 50Khz PWM signal output with 50% dutycycle with a oscilloscope. The user can enter a value to update the Duty cycle.

Supported Boards#

MC56F80000-EVK
Hardware requirements
  • Micro USB cable

  • MC56F80000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2

  2. Reset pin setting:

    Connect J11 pin2 and pin3

  3. Debugger setting:

    Connect J13 pin 1-2, 3-4, 5-6, 7-8

Board settings
  • Use oscilloscope to monitor J1-3.

Prepare the Demo
  1. Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with Multilink debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:


****Output PWM example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
MC56F81000-EVK
Hardware requirements
  • 2 x Micro USB cable

  • MC56F81000-EVK board

  • Personal Computer

  • Oscilloscope

Board hardware common setting
  1. Power setting:

    Connect J8 pin2 and pin3 Connect J5 pin1 and pin2 Connect J6 pin1 and pin2

  2. Onboard PnE U-MultiLink debugger setting:

    Connet J11 pin2 and pin3 Connect J13 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger PnE U-MultiLink. Note: when use external debugger(connected to J10), leave all J13 pins open.

Board settings
  • Use oscilloscope to monitor J1-3.

Prepare the Demo
  1. Connect USB cable between the host PC and the USB(J26) port on the target board to setup USB to UART bridge.

  2. Connect USB cable between the host PC and the USB(J12) port on the target baord to setup mulitlink debugger.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board with PnE U-MultiLink debug configuration.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted default FCF(flash configuration field) makes the MCU boot from flash.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:


****Output PWM example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
MC56F83000-EVK
Hardware requirements
  • Micro USB cable

  • MC56F83000-EVK board

  • Personal Computer

  • Oscilloscope

Board hardware common setting
  1. Power setting:

    Connect J19 pin2 and pin3 Connect J12 pin1 and pin2 Connect J13 pin1 and pin2 Connect J15 pin1 and pin2 Connect J16 pin2 and pin3 Connect J17 pin1 and pin2

  2. Onboard OSJTAG debugger setting:

    Leave J5 open Leave J6 open Note: J6 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J11 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J10), leave all J11 pins open.

Board settings
  • Use oscilloscope to monitor J4-7.

Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J8) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted that default FCF(flash configuration field) setting makes MCU boot from bootloader. So after reset button press, it will wait 5s(wait in bootloader) to run the application code.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:


****Output PWM example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
TWR-MC56F8200
Hardware requirements
  • Mini USB cable

  • TWR-MC56F8200 board

  • Personal Computer

  • Oscilloscope

Board hardware common setting
  1. HW reworkd(workaround):

    Connect J18(the mini USB port) pin4 and pin5. Note: This is due to HW design error, correct setting should be: J18 pin4 left empty and pin5 connected GND.

  2. Power setting:

    Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2

  3. UART setting:

    Connect J8 pin3 and pin4 Connect J9 pin3 and pin4

  4. Onboard OSJTAG debugger setting:

    Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open

Board settings
  • Use oscilloscope to monitor J501-19.

Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:


****Output PWM example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
TWR-MC56F8400
Hardware requirements
  • Mini USB cable

  • TWR-MC56F8400 board

  • Personal Computer

  • Oscilloscope

Board hardware common setting
  1. Power setting:

    Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2

  2. UART setting:

    Connect J8 pin3 and pin4 Connect J9 pin3 and pin4

  3. Onboard OSJTAG debugger setting:

    Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open

Board settings
  • Use oscilloscope to monitor J503-29.

Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:


****Output PWM example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~