flexio_mcu_lcd#
Overview#
The FlexIO MCU LCD demo application demonstrates how to use SDK FlexIO to drive MCU interface LCD.
The example displays one picture and an arrow at the right bottom of the screen. When press the arrow, a new picture is shown.
The project has provide the source code of the pictures (pictures.c), you can modify and re-generate the pictures.bin. For example, the pictures.bin could be generated using armgcc commands:
arm-none-eabi-gcc -c pictures.c -DBUILD_PIC_BIN
arm-none-eabi-objcopy -O binary pictures.o pictures.bin
Running the demo#
This demo could run without debug console. The debug console only shows some instructions and demo status.
At the beginning, the debug console shows:
FLEXIO MCU LCD example:
Touch the arrow to show next picture...
Press the arrow to show the next picture. If touch point is out of arrow, there is error log from the debug console:
Not touch the arrow...