MCUXpresso SDK Documentation

lwip_httpssrv_mbedTLS_freertos#

Overview#

The lwip_httpsrv_mbedTLS demo application demonstrates an HTTP server set up on lwIP TCP/IP and the MbedTLS stack with FreeRTOS. The user uses an internet browser to send an HTTPS request for connection. The board acts as an HTTP server and sends a web page back to the PC.

The example supports both IPv4 and IPv6 protocols. But some combinations of boards or build configurations may have only IPv4 enabled due to memory constraints. If it fits into memory, it is possible for the example to be compiled with both IPv4 and IPv6 (LWIP_IPV4=1 and LWIP_IPV6=1 in lwipopts.h), IPv4 only (LWIP_IPV4=1 and LWIP_IPV6=0 in lwipopts.h) or IPv6 only (LWIP_IPV4=0 and LWIP_IPV6=1 in lwipopts.h). If IPv6 is enabled, the board will assign a link-local IPv6 address to its interface, but this is often not enough as web browsers tend to not support link-local address with zone index in URL (e.g. https://[FE80::5627:8DFF:FE46:29F8%eth0]). So if the board is connected directly to the host PC, the PC should be configured to send ICMPv6 Router Advertisement messages with Prefix option, which the board could use to assign itself a routable address using the Stateless Address Autoconfiguration mechanism. If the board and the host PC are connected through a router, sending of Router Advertisement messages could be configured on that router (if it supports IPv6). Instructions how to set the IPv6 network correctly can be different on each system and it is out of scope of this readme. It can take a couple of seconds until the addresses are validated and assigned to the board’s ethernet interface, so the board will print “IPv6 address update” messages followed by all valid IPv6 addresses anytime there is a change. The assigned unique local or global unique addresses could be typed into the web browser’s address bar in a form like “https://[FD00:AABB:CCDD:EEFF:5627:8DFF:FE46:29F8]” to access the web server over IPv6.

Prepare the Demo#

  1. Connect a USB cable between the PC host and the OpenSDA(or USB to Serial) USB port on the target board.

  2. Open a serial terminal on PC for OpenSDA serial(or USB to Serial) device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert the Ethernet Cable into the target board’s RJ45 port and connect it to your PC network adapter.

  4. Configure the host PC IP address to 192.168.0.100.

  5. Configure the host PC to advertise IPv6 address prefix.

  6. Open a web browser.

  7. Download the program to the target board.

  8. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

  1. When the demo runs successfully, the terminal will display the following: Initializing PHY…

    ***********************************************************
    mbedTLS HTTPS Server example
    ***********************************************************
     IPv4 Address     : 192.168.0.102
     IPv4 Subnet mask : 255.255.255.0
     IPv4 Gateway     : 192.168.0.100
     IPv6 Address0    : -
     IPv6 Address1    : -
     IPv6 Address2    : -
    ***********************************************************
    IPv6 address update, valid addresses:
     IPv6 Address0    : FE80::5627:8DFF:FE46:29F8
     IPv6 Address1    : -
     IPv6 Address2    : -
    
    IPv6 address update, valid addresses:
     IPv6 Address0    : FE80::5627:8DFF:FE46:29F8
     IPv6 Address1    : FD00:AABB:CCDD:EEFF:5627:8DFF:FE46:29F8
     IPv6 Address2    : -
    
  2. If the example has been compiled with IPv4 enabled (LWIP_IPV4=1), type https://192.168.0.102 (IP address of the board) into the browser address bar. The browser should show a web page. Username admin and password admin is required to access “Authorization example” section of the web page.

  3. If the example has been compiled with IPv6 enabled (LWIP_IPV6=1), wait for the unique local or global unique IPv6 address to appear in the list of valid addresses in the console output. Then the server could be reached over IPv6. For the example output above, https://[FD00:AABB:CCDD:EEFF:5627:8DFF:FE46:29F8] could be typed into the browser’s address bar to make it show the web page and communicate with the board over IPv6.

Modifying content of static web pages#

To modify content available through the web server you must complete following steps:

  1. Modify, add or delete files in folder “boards/<board_name>/lwip_examples/lwip_httpssrv_mbedTLS_freertos/webpage”.

  2. Run the script file “middleware/lwip/src/apps/httpsrv/mkfs/mkfs.pl <directory name>” to generate new “httpsrv_fs_data.c”. Make sure to execute it from a folder where the file “httpsrv_fs_data.c” is. For example:

    C:\sdk\boards\<board_name>\lwip_examples\lwip_httpssrv_mbedTLS_freertos> C:\sdk\middleware\lwip\src\apps\httpsrv\mkfs\mkfs.pl webpage
    Processing file webpage/auth.html
    Processing file webpage/cgi.html
    Processing file webpage/favicon.ico
    Processing file webpage/help.html
    Processing file webpage/httpsrv.css
    Processing file webpage/index.html
    Processing file webpage/NXP_logo.png
    Processing file webpage/poll.html
    Processing file webpage/request.js
    Processing file webpage/ssi.shtml
    Processing file webpage/welcome.html
    Done.
    
  3. Make sure the “httpsrv_fs_data.c” file has been overwritten with the newly generated content.

  4. Re-compile the HTTP server application example and download it to your board.

Supported Boards#