MCUXpresso SDK Documentation

sysmpu#

Overview#

The SYSMPU example defines protected/unprotected memory region for the core access.

First, the SYSMPU will capture the hardware information and show it on the terminal. Then, a memory region is configured as the non-writable region. The bus fault interrupt is enabled to report the memory protection interrupt event for this non-writable region. If an operation writes to this region, the bus fault interrupt happens. Then the bus fault interrupt handler provides a prevention alert by outputting a message on terminal, then the write rights will be given to this region for core access. After the write access enabled, the writing to the region becomes successful. When the bus fault happen, the details of the error information will be captured and printed on the terminal.

This example provides the terminal input control to give the example show for several regions access test. Just press any key to the terminal when the terminal show “Press any key to continue”.

Running the demo#

When the demo runs successfully, the following message is displayed in the terminal:

SYSMPU Example Start.

SYSMPU revision level 1, 5 slave ports and 12 region numbers are supported.

Set regionArray0 to un-writeable.

Write 0 to regionArray at No.0.

Core access violation and generate busfault.

RegionArray[0] = 0, not updated.

Core is granted write access permission.

Error access happen on slave port: 2, access master port 0.

Error access attributes: accessSupervisorMode.

Error access type: write.

Error access control: overlappRegion.

Error access address: xxxxxxx.

RegionArray[0] = 0, updated now.

Protected regionArray successfully.

Press any key to continue.

Otherwise, the log will show

ERROR: Cannot protect regionArray.

Supported Boards#

TWR-KM34Z50MV3
Hardware requirements
  • Mini USB cable

  • TWR-KM34Z50MV3 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

TWR-KM34Z75M
Hardware requirements
  • Mini USB cable

  • TWR-KM34Z75M board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

TWR-KM35Z75M
Hardware requirements
  • Micro USB cable

  • TWR-KM35Z75M board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

FRDM-MCXE247
Hardware requirements
  • Micro USB cable

  • FRDM-MCXE247 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.