MCUXpresso SDK Documentation

host_audio_recorder_freertos#

Overview#

The Host Audio example supports the audio microphone device.
The application prints the audio microphone information when the USB microphone device is attached.

System Requirement#

Hardware requirements#

  • Mini/micro USB cable

  • USB A to micro AB cable

  • Hardware (Tower module/base board, and so on) for a specific device

  • Personal Computer

  • Consider the performance requirement, please run this case by high speed.

Software requirements#

  • The project files are in:
    <MCUXpresso_SDK_Install>/boards//usb_examples/usb_host_audio_recorder//.

The is FreeRTOS OS, do not support Bare Metal because writing sdcard is in blocking mode. Even though in freertos, the host can’t totally guarantee getting all of stream data of audio device (some transfers may be lost) on some platforms because some SOCs’ performance may not meet this case’s requirement.

Getting Started#

Hardware Settings#

For detailed instructions, see the appropriate board User’s Guide.

Set the hardware jumpers (Tower system/base module) to default settings.

Prepare the example#

  1. Download the program to the target board.

  2. Power off the target board and power on again.

  3. Prepare a sdcard and format it with FAT32 file system.

For detailed instructions, see the appropriate board User’s Guide.

Run the example#

  1. Connect the board UART to the PC, you can see the Serial port number from “Device Manager”, then open the COM port in a terminal tool such as PuTTy as the following picture, the baud rate is 115200.
    UART port number
    Open UART

  2. Insert the SD card into the slot. “sdcard inserted” and free memory size is printed out in the terminal as the following image.
    SDcard Insert

  3. Make sure to use a USB HUB or an adapter with OTG functionality firstly. Plug in the USB audio microphone(generator) device to the board and the related information is printed in the terminal.

  4. Enter ‘r’ to start recording. The USB application will transfers the audio data from the USB audio microphone device and the sound is written in sd card. Enter ‘s’ to stop recording, then one PCM file is saved. The following image shows how to attach a USB audio microphone device.
    Attach audio 1.0 microphone device
    Attach audio 2.0 microphone device

  5. Every time step 4 is executed, a file will be saved. For the convenience of audio testing, the following python script is provided to convert PCM to be WAV. Please set right parameters for setparams functon, which nchannels is channel count, sampwidth is byte width, framerate is sample rate. In the current test case, we should use setparams((1, 1, 8000, 0, ‘NONE’, ‘NONE’)). Open the WAV file with any media player and verify it by listening on the speaker of Laptop/PC.

                import sys
                import wave

                for arg in sys.argv[1:]:
                    with open(arg, 'rb') as pcmfile:
                        pcmdata = pcmfile.read()
                    with wave.open(arg+'.wav', 'wb') as wavfile:
                        wavfile.setparams((nchannels, sampwidth, framerate, 0, 'NONE', 'NONE'))
                        wavfile.writeframes(pcmdata)


Convert PCM to WAV using python

  1. USB host only supports PCM format. If device has no PCM format, usb host will print necessary log.

Supported Boards#

MIMXRT1040-EVK
Getting Started
Hardware Settings
  • The USB_OTG1_ID shares the same pin with SDIO0_SD1_SEL. Please remove the R461.

EVK-MIMXRT595
Getting Started
Hardware Settings
  • For evkmimxrt595 REV.C1, need to rework it to use sdcard instead of EMMC. Make sure resistors R691~R697 are populated and resistors R611~R620,R660, R661 are removed.