flexio_a-format_sync_transfer#
Overview#
The a-format_sync example shows how to use flexio A-format driver in sync way:
In this example, a flexio simulated A-format connect to the encoder through RS-485, the board will send requests to and receive responses from the board.
Supported Boards#
IMX943-EVK
Hardware requirements
Micro USB cable
IMX943-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
RS-485 adapter board
Board settings
This example requires connecting between FlexIO1 pins and RS-485 adapter board which is connected to the encoder.
FLEXIO_A_FORMAT_DR_PIN(J48-10) -> D/R pin of RS-485
FLEXIO_A_FORMAT_TX_PIN(J48-9) -> RX pin of RS-485
FLEXIO_A_FORMAT_RX_PIN(J48-11) -> TX pin of RS-485
3.3V pin(J49-8) -> 3.3V pin of RS-485
GND pin(J49-12) -> GND pin of RS-485
5.0V pin(J49-10) -> 5.0V pin of encoder
GND pin(J49-14) -> GND pin of encoder
A pin of RS-485 -> SD+ pin of encoder
B pin of RS-485 -> SD- pin of encoder
Please note this application can’t support running with Linux BSP!
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict. Tips: After you insert the USB2COM, a new USBCOM will be found. The function output in new USBCOM.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a micro USB cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
Encoder A-format example
Encoder ID: 5946590
Multi-turn data: 64474, single-turn data: 147617
[0.10s] Encoder ID: 0x5ABCDE
Multi-turn data: 64474, single-turn data: 147617
Temperature: 45.000000
[0.20s] Encoder ID: 0x5ABCDE
Multi-turn data: 64474, single-turn data: 147617
Temperature: 44.000000