jpegdec_single_stream_repeat#
Overview#
The SD JPEG decoder example decodes a series of JPEG pictures stored on SD card then shows them one by one on panel. Only one slot is used with two descriptors linked with each other as ping-pong descriptors. After one descriptor finishes the other will be loaded.