MCUXpresso SDK Documentation

MIMXRT700-EVK#

Overview#

The i.MX RT700 EVK (MIMXRT700-EVK) features NXPs advanced implementation of the Arm Cortex-M33 core, combined with the highly optimized Cadence Tensilica HiFi4 and HiFi1 DSP processor cores. MIMXRT700-EVK supports development for the MIMXRT798, MIMXRT758 and MIMXRT735 products and its features make it ideal for portable HMI applications. The i.MX RT700 EVK can help jump start your next design with the included schematics and layout files.

MIMXRT700-EVK

MCU device and part on board is shown below:

  • Device: MIMXRT798S

  • PartNumber: MIMXRT798SGFOB

SDK Introduction#

For an introduction to the MCUXpresso SDK, see MCUXpresso Software Development Kit (SDK).

Getting Started with MCUXpresso SDK Package#

Getting Started with MCUXpresso SDK GitHub#

Getting Started with MCUXpresso SDK Xplorer#

Release Notes#

ChangeLog#

Driver API Reference Manual#

This section provides a link to the Driver API RM, detailing available drivers and their usage to help you integrate hardware efficiently.

MIMXRT798S

Middleware Documentation#

Find links to detailed middleware documentation for key components. While not all onboard middleware is covered, this serves as a useful reference for configuration and development.

VG-Lite GPU Library#

VGLite Graphics Driver

Multicore#

Multicore SDK

MCU Boot#

mcuboot_opensource

eIQ#

eIQ

FreeMASTER#

freemaster

NXP Wi-Fi#

Wi-Fi, Bluetooth, 802.15.4

FreeRTOS#

FreeRTOS

lwIP#

lwIP

File systemFatfs#

FatFs

DSP Audio Streamer#

Xtensa Audio Framework (XAF)

Trusted-Frimware-M#

Trusted-Firmware-M