MCUXpresso SDK Documentation

lwip_dhcp_freertos#

Overview#

The lwip_dhcp demo application demonstrates a DHCP demo on the lwIP TCP/IP stack. The application acts as a DHCP client and prints the status as it is progressing. Once the interface is being bound to an IP address obtained from DHCP server, address information is printed. It does so continuously - it prints the client’s state even as the link state changes. Those link state changes are also printed.

Prepare the Demo#

  1. Connect a USB cable between the PC host and the OpenSDA(or USB to Serial) USB port on the target board.

  2. Open a serial terminal on PC for OpenSDA serial(or USB to Serial) device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert the Ethernet Cable into the target board’s RJ45 port and connect it to a router (or other DHCP server capable device).

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs, the log would be seen on the terminal like:

Initializing PHY...
[LINK STATE] netif=0, state=up, speed=1000M_full

************************************************
 DHCP example
************************************************
 DHCP state       : SELECTING
 DHCP state       : REQUESTING
 DHCP state       : CHECKING
 DHCP state       : BOUND

 IPv4 Address     : 192.168.0.4
 IPv4 Subnet mask : 255.255.255.0
 IPv4 Gateway     : 192.168.0.1

Supported Boards#

MIMXRT1060-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKB board

  • Personal Computer

Board settings

No special settings are required.

IMX952LPD5EVK-19
Hardware requirements
  • Micro USB cable

  • IMX952-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

This example uses NETC ENETC0 1G port in default. To choose other port, configure in lwip_netc_port.h.

MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • Network cable RJ45 standard

  • MIMXRT1170-EVKB board

  • Personal Computer

Board settings

This example uses 1G port(J4) as default. If want to test 100M port(J3), please set the macro BOARD_NETWORK_USE_100M_ENET_PORT to 1.

MIMXRT1060-EVKC
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

Board settings

No special settings are required.

FRDM-IMXRT1152
Hardware requirements
  • FRDM-IMXRT1152 board

  • USB Type-C cable

  • RJ45 network cable

  • Personal Computer

Board settings
  • Connect the USB Type-C cable to the FRDM-IMXRT1152 USB debug connector.

  • Use the Gigabit Ethernet RJ45 port (J130).

  • Set J134 to position 1-2 for the shared ENET_MDIO / ETH0_RDATA3 routing.

MIMXRT1040-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1040-EVK board

  • Personal Computer

Board settings

No special settings are required.

EVK-MIMXRT1064
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1064 board

  • Personal Computer

Board settings

No special settings are required.

MIMXRT1160-EVK
Hardware requirements
  • Mini/micro USB cable

  • Network cable RJ45 standard

  • MIMXRT1160-EVK board

  • Personal Computer

Board settings

This example uses 1G port(J4) as default. If want to test 100M port(J3), please set the macro BOARD_NETWORK_USE_100M_ENET_PORT to 1.

MIMXRT1180-EVK
Hardware requirements
  • Mini/micro USB cable

  • Network cable RJ45 standard

  • MIMXRT1180-EVK board

  • Personal Computer

Board settings

This example uses Ethernet RJ45 port J32.

FRDM-MCXA577
Hardware requirements
  • Type-C USB cable

  • RJ45 Network cable (for 100BASE-TX mode)

  • 10BASE-T1S network adapter and cable (optional for 10BASE-T1S mode)

  • FRDM-MCXA577 board

  • Personal Computer

Board settings

Short position 2-3 on J29.

Use with 10BASE-T1S Ethernet

The example uses 100BASE-TX Ethernet over RJ45 by default. If you want to use the internal 10BASE-T1S digital PHY, redefine BOARD_NETWORK_USE_TENBASET_PHY from board.h to 1 and rebuild. Connect to a PC with a 10BASE-T1S network adapter instead of RJ45 and enable PLCA on a PC with the following parameters: - node ID: 0 (PLCA coordinator) - node count: 8 - TO timer: 32 BT - burst count: 0 - burst timer: 128 BT

FRDM-MCXE247
Hardware requirements
  • USB-C cable

  • Network cable RJ45 standard

  • FRDM-MCXE247 board

  • Personal Computer

Board settings

No special settings are required.

FRDM-MCXN947
Hardware requirements
  • Type-C USB cable

  • RJ45 Network cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings

Connect JP13 2-3 pin. Populate R274 to sync reference clock.

FRDM-MCXN947T
Hardware requirements
  • Type-C USB cable

  • RJ45 Network cable

  • FRDM-MCXN947T board

  • Personal Computer

Board settings

Connect JP13 2-3 pin. Populate R274 to sync reference clock.

FRDM-RW612
Hardware requirements
  • USB-C cable

  • Network cable RJ45 standard

  • FRDM-RW612 board

  • Personal Computer

Board settings

Make sure SJ21 and SJ22 have positions 1 and 2 soldered (default).

IMX95LPD5EVK-19
Hardware requirements
  • Micro USB cable

  • IMX95LPD5-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

This example uses NETC ENETC0 1G port in default. To choose other port, configure in lwip_netc_port.h.

FRDM-IMX95
Hardware requirements
  • Micro USB cable

  • FRDM-IMX95 board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

This example uses NETC ENETC0 1G port in default. To choose other port, configure in lwip_netc_port.h.

FRDM-IMX952
Hardware requirements
  • Micro USB cable

  • IMX952-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

This example uses NETC ENETC0 1G port in default. To choose other port, configure in lwip_netc_port.h.

FRDM-IMX937
Hardware requirements
  • Micro USB cable

  • FRDM-IMX937 board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

This example uses NETC ENETC0 1G port in default. To choose other port, configure in lwip_netc_port.h.

LPCXpresso54628
Hardware requirements
  • Mini/micro USB cable

  • RJ45 Network cable

  • LPCXpresso54628 board

  • Router or other device with DHCP server capability

  • Personal Computer

Board settings

For LPCXpresso54628 V2.0:JP11 and JP12 1-2 on.

LPCXpresso54S018
Hardware requirements
  • Mini/micro USB cable

  • RJ45 Network cable

  • LPCXpresso54S018 board

  • Router or other device with DHCP server capability

  • Personal Computer

Board settings
LPCXpresso54S018M
Hardware requirements
  • Mini/micro USB cable

  • RJ45 Network cable

  • LPCXpresso54S018M board

  • Router or other device with DHCP server capability

  • Personal Computer

Board settings

For LPCXpresso54S018M V2.0:JP11, JP12, JP14 and JP15 1-2 on.

MCIMX93AUTO-EVK
Hardware requirements
  • USB Type-C cable

  • Network cable RJ45 standard

  • MCIMX93AUTO-EVK board

  • Personal Computer

Board settings

This example uses 1G port(J601) as default.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

MCIMX93-EVK
Hardware requirements
  • USB Type-C cable

  • Network cable RJ45 standard

  • MCIMX93-EVK board

  • Personal Computer

Board settings

This example uses 1G port(J601) as default.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

MCIMX93W-EVK
Hardware requirements
  • USB Type-C cable

  • Network cable RJ45 standard

  • MCIMX93W-EVK board

  • Personal Computer

Board settings

This example uses 1G port(J601) as default.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

MCX-N5XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • RJ45 Network cable

  • MCX-N5XX-EVK board

  • Personal Computer

Board settings

Connect JP13 2-3 pin. Populate R274 to sync reference clock.

MCX-N9XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • RJ45 Network cable

  • MCX-N9XX-EVK board

  • Personal Computer

Board settings

Connect JP13 2-3 pin. Populate R274 to sync reference clock.

RD-RW612-BGA
Hardware requirements
  • Micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings

Connect JP54. Load R520, R508, R505 Remove R518, R507, R506

IMX943-ORANGEBOX
Hardware requirements
  • Micro USB cable

  • IMX943-ORANGEBOX board

  • 12V~20V power supply

  • Personal Computer

Board settings

This example uses NETC ENETC0 1G port in default. To choose other port, configure in lwip_netc_port.h.

FRDM-IMXRT1186
Hardware requirements
  • Type-C USB cable

  • Network cable RJ45 standard

  • FRDM-IMXRT1186 board

  • Personal Computer

Board settings

Short jumpers J12 (1-2) and J13 (2-3) and connect network cable to J56A.

IMX943-EVK
Hardware requirements
  • Micro USB cable

  • IMX943-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

This example uses NETC ENETC0 (ETH2/J25) 1G port in default. To choose other port, configure in lwip_netc_port.h.