MCUXpresso SDK Documentation

mcxromapi_flash_hiding

mcxromapi_flash_hiding#

Overview#

The FLASH_HIDING project is a simple demonstration program showing flash hiding and customer defined proteted area (CDPA). MBC provides read, write, and execute access control per block to internal flash memory. A message a printed on the UART terminal as various operations on flash memory are performed.

Supported Boards#

FRDM-MCXN236
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN236 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a type-c USB cable between the PC host and the MCU-Link USB port (J10) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

Flash Hiding example...
FLASH_Init PASSED
FFR_Init PASSED
Erasing FLASH sectors, address: 10000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 10000, size: 1000
flash_page_program PASSED
FLASH hiding no enabled and read PASSED!
MBCAddr = 0
MBCAddr = 500
FLASH hiding enabled and read limit PASSED
flash hiding test erase and program PASSED

CDPA example...
FLASH_Init PASSED
FFR_Init PASSED
Before enabling the CDPA, call flash_erase API and flash_program API ...
Erasing FLASH sectors, address: 18000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 18000, size: 1000
CDPA no enabled and flash_program PASSED
CDPABlock = 0
CDPABlock = 4000
CDPA enabled and read test PASSED
CDPA test erase and program PASSED
FRDM-MCXN947
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

Flash Hiding example...
FLASH_Init PASSED
FFR_Init PASSED
Erasing FLASH sectors, address: 10000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 10000, size: 1000
flash_page_program PASSED
FLASH hiding no enabled and read PASSED!
MBCAddr = 0
MBCAddr = 500
FLASH hiding enabled and read limit PASSED
flash hiding test erase and program PASSED

CDPA example...
FLASH_Init PASSED
FFR_Init PASSED
Before enabling the CDPA, call flash_erase API and flash_program API ...
Erasing FLASH sectors, address: 18000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 18000, size: 1000
CDPA no enabled and flash_program PASSED
CDPABlock = 0
CDPABlock = 4000
CDPA enabled and read test PASSED
CDPA test erase and program PASSED
FRDM-MCXN947T
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947T board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

Flash Hiding example...
FLASH_Init PASSED
FFR_Init PASSED
Erasing FLASH sectors, address: 10000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 10000, size: 1000
flash_page_program PASSED
FLASH hiding no enabled and read PASSED!
MBCAddr = 0
MBCAddr = 500
FLASH hiding enabled and read limit PASSED
flash hiding test erase and program PASSED

CDPA example...
FLASH_Init PASSED
FFR_Init PASSED
Before enabling the CDPA, call flash_erase API and flash_program API ...
Erasing FLASH sectors, address: 18000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 18000, size: 1000
CDPA no enabled and flash_program PASSED
CDPABlock = 0
CDPABlock = 4000
CDPA enabled and read test PASSED
CDPA test erase and program PASSED
MCX-N5XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N5XX-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

Flash Hiding example...
FLASH_Init PASSED
FFR_Init PASSED
Erasing FLASH sectors, address: 10000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 10000, size: 1000
flash_page_program PASSED
FLASH hiding no enabled and read PASSED!
MBCAddr = 0
MBCAddr = 500
FLASH hiding enabled and read limit PASSED
flash hiding test erase and program PASSED

CDPA example...
FLASH_Init PASSED
FFR_Init PASSED
Before enabling the CDPA, call flash_erase API and flash_program API ...
Erasing FLASH sectors, address: 18000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 18000, size: 1000
CDPA no enabled and flash_program PASSED
CDPABlock = 0
CDPABlock = 4000
CDPA enabled and read test PASSED
CDPA test erase and program PASSED
MCX-N9XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N9XX-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

Flash Hiding example...
FLASH_Init PASSED
FFR_Init PASSED
Erasing FLASH sectors, address: 10000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 10000, size: 1000
flash_page_program PASSED
FLASH hiding no enabled and read PASSED!
MBCAddr = 0
MBCAddr = 500
FLASH hiding enabled and read limit PASSED
flash hiding test erase and program PASSED

CDPA example...
FLASH_Init PASSED
FFR_Init PASSED
Before enabling the CDPA, call flash_erase API and flash_program API ...
Erasing FLASH sectors, address: 18000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 18000, size: 1000
CDPA no enabled and flash_program PASSED
CDPABlock = 0
CDPABlock = 4000
CDPA enabled and read test PASSED
CDPA test erase and program PASSED