MCUXpresso SDK Documentation

ZPS_tsAplZdpRemoveNodeCacheRsp

ZPS_tsAplZdpRemoveNodeCacheRsp#

This structure is used to store Remove_node_cache_rsp message data - a response to a call to the function ZPS_eAplZdpRemoveNodeCacheRequest(). This response indicates whether the sending node has successfully removed from its primary discovery cache all ‘discovery information’ relating to a given End Device node.

The ZPS_tsAplZdpRemoveNodeCacheRspstructure is detailed below.

typedef struct {
     uint8 u8Status;
} ZPS_tsAplZdpRemoveNodeCacheRsp;

where u8Statusis the return status for the function ZPS_eAplZdpRemoveNodeCacheRequest().

Parent topic:ZDP response structures