i2c_master_read_sensor_tmp117#
Overview#
The example shows how to use lpc_i2c driver as master to read temperature data from sensor TMP117.
The example will do dynamic address assignment to the TMP117 sensor, read the temperature data and print it in while loop.
Supported Boards#
MCXW23-EVK
Hardware requirements
Mini/micro USB cable
MCXW23-EVK Board
Personal Computer
Board settings
Apply the jummpers on J13 1-2, 9-10 and 13-14.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J33.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
i2c master read sensor data example.
Temperature:28.4688
Temperature:28.4766
Temperature:28.4766