MCUXpresso SDK Documentation

adc12_lpit_trgmux

adc12_lpit_trgmux#

Overview#

The adc12_lpit_trgmux example shows how to use the LPIT and TRGMUX to generate a ADC trigger.

In this example, user should indicate a channel to provide a voltage signal (can be controlled by user) as the ADC12’s sample input. When run the example, the ADC is triggered by TRGMUX and gets the ADC conversion result in the ADC Conversion Complete (COCO) Interrupt. The LPIT is configured as periodic counter which will output pre-trigger and tigger signal to TRGMUX periodically.

Running the demo#

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

ADC Full Range: 4096

Change the input voltage to check ADC12's conversion result...

ADC12 Interrupt Counter: 1
ADC12 Conversion Completed, result value: 4056

ADC12 Interrupt Counter: 2
ADC12 Conversion Completed, result value: 781

Supported Boards#

FRDM-KE15Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE15Z board

  • Personal Computer

Board settings

This example project uses ADC12 instance 0 to sample and convert the voltage signal input from channel 0(PTA0). So the voltage signal input from PTA0 should be changed to observe the dynamical conversion result.

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

FRDM-KE16Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE16Z board

  • Personal Computer

Board settings

This example project uses ADC12 instance 0 to sample and convert the voltage signal input from channel 0(PTA0). So the voltage signal input from J4-12(PTA0) should be changed to observe the dynamical conversion result.

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

FRDM-KE17Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE17Z board

  • Personal Computer

Board settings

This example project uses ADC12 instance 0 to sample and convert the voltage signal input from channel 0(PTE9). So the voltage signal input from PTE9(J3-3) should be changed to observe the dynamical conversion result.

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

FRDM-KE17Z512
Hardware requirements
  • Micro USB cable

  • FRDM-KE17Z512 board

  • Personal Computer

Board settings

This example project uses ADC12 instance 0 to sample and convert the voltage signal input from channel 0(PTE9). So the voltage signal input from PTE9(J2-19) should be changed to observe the dynamical conversion result.

Prepare the Demo
  1. Connect a USB cable between the PC host and the MCU-LINK USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

FRDM-MCXE247
Hardware requirements
  • USB-C cable

  • FRDM-MCXE247 board

  • Personal Computer

Board settings

This example project uses ADC12 instance 0 to sample and convert the voltage signal input from channel 0 (PTA0). So the voltage signal input on PTA0 (J4-10) should be changed to observe the dynamical conversion result.

Prepare the Demo
  1. Connect a USB cable between the PC host and the MCU-LINK USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.