ele_crypto_generic_rsa#
Overview#
The ELE Crypto Generic Example project is a demonstration program that uses the MCUX SDK software to perform generic crypto operations usign plaintext key with EdgeLock Enclave (ELE).
Running the demo#
Example output on terminal:
EdgeLock Enclave secure Sub-System Driver Example:
*********** Load EdgeLock FW ****************************** EdgeLock FW loaded and authenticated successfully.
****************** Start RNG ****************** EdgeLock RNG Start success. EdgeLock RNG ready to use.
*********** Generic Crypto RSA keygen ********************* RSA Key-Pair generation. RSA Key-pair generated successfully.
*********** Generic Crypto RSA PKCS#1.5 Signature gen ***** RSA signature with input as digest generated successfully. RSA signature with input as message generated successfully.
*********** Generic Crypto RSA PSS Signature gen ********** RSA signature generated successfully.
*********** Generic Crypto RSA 2048 PKCS#1.5 Verify ******* RSA verify success
*********** Generic Crypto RSA 3072 PSS Verify ************ RSA verify success
*********** Generic Crypto RSA PKCS#1.5 encrypt *********** RSA encryption success.
*********** Generic Crypto RSA PKCS#1.5 decrypt *********** RSA decryption success, plaintext match original one.
*********** Generic Crypto RSA OAEP encrypt *************** RSA encryption success.
*********** Generic Crypto RSA OAEP decrypt *************** RSA decryption success, plaintext match original one.
End of Example with SUCCESS!!
Supported Boards#
MIMXRT1180-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Example output on terminal:
EdgeLock Enclave secure Sub-System Driver Example:
*********** Load EdgeLock FW ****************************** EdgeLock FW loaded and authenticated successfully.
****************** Start RNG ****************** EdgeLock RNG Start success. EdgeLock RNG ready to use.
*********** Generic Crypto RSA keygen ********************* RSA Key-Pair generation. RSA Key-pair generated successfully.
*********** Generic Crypto RSA PKCS#1.5 Signature gen ***** RSA signature with input as digest generated successfully. RSA signature with input as message generated successfully.
*********** Generic Crypto RSA PSS Signature gen ********** RSA signature generated successfully.
*********** Generic Crypto RSA 2048 PKCS#1.5 Verify ******* RSA verify success
*********** Generic Crypto RSA 3072 PSS Verify ************ RSA verify success
*********** Generic Crypto RSA PKCS#1.5 encrypt *********** RSA encryption success.
*********** Generic Crypto RSA PKCS#1.5 decrypt *********** RSA decryption success, plaintext match original one.
*********** Generic Crypto RSA OAEP encrypt *************** RSA encryption success.
*********** Generic Crypto RSA OAEP decrypt *************** RSA decryption success, plaintext match original one.
End of Example with SUCCESS!!
FRDM-IMXRT1186
Hardware requirements
Type-C USB cable
FRDM-IMXRT1186 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Example output on terminal:
EdgeLock Enclave secure Sub-System Driver Example:
*********** Load EdgeLock FW ****************************** EdgeLock FW loaded and authenticated successfully.
****************** Start RNG ****************** EdgeLock RNG Start success. EdgeLock RNG ready to use.
*********** Generic Crypto RSA keygen ********************* RSA Key-Pair generation. RSA Key-pair generated successfully.
*********** Generic Crypto RSA PKCS#1.5 Signature gen ***** RSA signature with input as digest generated successfully. RSA signature with input as message generated successfully.
*********** Generic Crypto RSA PSS Signature gen ********** RSA signature generated successfully.
*********** Generic Crypto RSA 2048 PKCS#1.5 Verify ******* RSA verify success
*********** Generic Crypto RSA 3072 PSS Verify ************ RSA verify success
*********** Generic Crypto RSA PKCS#1.5 encrypt *********** RSA encryption success.
*********** Generic Crypto RSA PKCS#1.5 decrypt *********** RSA decryption success, plaintext match original one.
*********** Generic Crypto RSA OAEP encrypt *************** RSA encryption success.
*********** Generic Crypto RSA OAEP decrypt *************** RSA decryption success, plaintext match original one.
End of Example with SUCCESS!!