MCUXpresso SDK Documentation

cadc_sequential_conversion

Contents

cadc_sequential_conversion#

Overview#

The cadc_sequential_conversion example shows how to use a long conversion sequence (can include as many as all the 16 sample slots) with CADC driver.

In this example, the CADC is configured as “kCADC_DualConverterWorkAsTriggeredSequential” work mode. User should indicate 4 channel pairs to provide the differential voltage signal (can be controlled by user) as the inputs for CADC sample slots. These sample slots would be assembled into a long conversion sequence.

In “kCADC_DualConverterWorkAsTriggeredSequential” mode, all the sample slots are organized as a long conversion sequence. The converter A’s control logic would be used to operate this long conversion sequence. It can start and stop the sequence.

When running the project, typing any key into debug console would trigger the conversion. And then, the conversion result data of the four sample slots (Sample 0, 1, 2, 3) would be displayed in the terminal.