MCUXpresso SDK Documentation

igpio_input_interrupt

igpio_input_interrupt#

Overview#

The GPIO Example project is a demonstration program that uses the KSDK software to manipulate the general-purpose outputs. The example is supported by the set, clear registers for each GPIO pin output register.

Supported Boards#

EVKB-IMXRT1050
Hardware requirements
  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW8 , and “SW8 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW8 is turned on.
 ......
MIMXRT1060-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKB board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW2 , and “SW2 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW2 is turned on.
 ......
MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW7 , and “SW7 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW7 is turned on.
 ......
MIMXRT1060-EVKC
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW2 , and “SW2 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW2 is turned on.
 ......
FRDM-IMXRT1152
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1152 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW6 , and “SW6 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW6 is turned on.
 ......
EVK-MIMXRT1010
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1010 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW4 , and “SW4 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW4 is turned on.
 ......

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

EVK-MIMXRT1015
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1015 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW4 , and “SW4 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW4 is turned on.
 ......

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

EVK-MIMXRT1020
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1020 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW4 , and “SW4 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW4 is turned on.
 ......

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1024-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1024-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW4 , and “SW4 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW4 is turned on.
 ......

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1040-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1040-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW8 , and “SW8 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW8 is turned on.
 ......
EVK-MIMXRT1064
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1064 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW8 , and “SW8 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW8 is turned on.
 ......
MIMXRT1160-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1160-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW7 , and “SW7 is turned on” is shown on the terminal window

 GPIO Driver example.

 SW7 is turned on.
 ......