se05x_Minimal#
Overview#
This is a bare minimum example for se050. This gets the amount of free memory.
Supported Boards#
FRDM-MCXA153
Hardware requirements
Mini/micro USB cable
FRDM-MCXN947 board (Rev D or Later)
Personal Computer
Board settings
Jumper settings for OM- SE050ARD & OM- SE051ARD: -J14 3-4 (Default): EdgeLock SE05x_VCC pin routed to SE05X_VOUT pin -J15 3-4 (Default): I2C target SDA connection -J17 3-4 (Default): I2C target SCL connection
For A71CH
Connect OM3710/A71CHARD to the board.
For SE050
Connect OM- SE050ARD to the board.
Please consult SE050 user manual and Plug & Trust middleware documentation which is present in the Plug & Trust MW package for further details.
The Plug & Trust MW package can be downloaded from https://www.nxp.com/products/security-and-authentication/authentication/:SE050?tab=Design_Tools_Tab
Please refer to the RST file in the doc folder for additional details about the example.
For running ex_rsa example enable following options in the fsl_sss_ftr.h file: SSS_HAVE_APPLET_SE05X_C - 1 SSS_HAVE_RSA - 1
FRDM-MCXN947
Hardware requirements
Mini/micro USB cable
FRDM-MCXN947 board (Rev D or Later)
Personal Computer
Board settings
Jumper settings for OM- SE050ARD & OM- SE051ARD: -J14 3-4 (Default): EdgeLock SE05x_VCC pin routed to SE05X_VOUT pin -J15 3-4 (Default): I2C target SDA connection -J17 3-4 (Default): I2C target SCL connection
For A71CH
Connect OM3710/A71CHARD to the board.
For SE050
Connect OM- SE050ARD to the board.
Please consult SE050 user manual and Plug & Trust middleware documentation which is present in the Plug & Trust MW package for further details.
The Plug & Trust MW package can be downloaded from https://www.nxp.com/products/security-and-authentication/authentication/:SE050?tab=Design_Tools_Tab
Please refer to the RST file in the doc folder for additional details about the example.
For running ex_rsa example enable following options in the fsl_sss_ftr.h file: SSS_HAVE_APPLET_SE05X_C - 1 SSS_HAVE_RSA - 1
FRDM-MCXN947T
Hardware requirements
Mini/micro USB cable
FRDM-MCXN947T board (Rev D or Later)
Personal Computer
Board settings
Jumper settings for OM- SE050ARD & OM- SE051ARD: -J14 3-4 (Default): EdgeLock SE05x_VCC pin routed to SE05X_VOUT pin -J15 3-4 (Default): I2C target SDA connection -J17 3-4 (Default): I2C target SCL connection
For A71CH
Connect OM3710/A71CHARD to the board.
For SE050
Connect OM- SE050ARD to the board.
Please consult SE050 user manual and Plug & Trust middleware documentation which is present in the Plug & Trust MW package for further details.
The Plug & Trust MW package can be downloaded from https://www.nxp.com/products/security-and-authentication/authentication/:SE050?tab=Design_Tools_Tab
Please refer to the RST file in the doc folder for additional details about the example.
For running ex_rsa example enable following options in the fsl_sss_ftr.h file: SSS_HAVE_APPLET_SE05X_C - 1 SSS_HAVE_RSA - 1
LPCXpresso55S69
Hardware requirements
Mini/micro USB cable
LPCXpresso55s69 board
Personal Computer
Board settings
Jumper settings for OM- SE050ARD & OM- SE051ARD: -J14 3-4 (Default): EdgeLock SE05x_VCC pin routed to SE05X_VOUT pin -J15 3-4 (Default): I2C target SDA connection -J17 3-4 (Default): I2C target SCL connection
For SE050
Connect OM- SE050ARD to the board.
Please consult SE050 user manual and Plug & Trust middleware documentation which is present in the Plug & Trust MW package for further details.
The Plug & Trust MW package can be downloaded from https://www.nxp.com/products/security-and-authentication/authentication/:SE050?tab=Design_Tools_Tab
Please refer to the RST file in the doc folder for additional details about the example.
For running ex_rsa example enable following options in the fsl_sss_ftr.h file: SSS_HAVE_APPLET_SE05X_C - 1 SSS_HAVE_RSA - 1