iap_eeprom#
Overview#
The IAP EEPROM project is a simple demonstration program of the SDK IAP driver. It writes and reads the EEPROM page. A message a printed on the UART terminal as EEPROM read and write operations are performed.
Supported Boards#
LPCXpresso54628
Hardware requirements
Micro USB cable
LPCXpresso54628 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
IAP EEPROM example
Read EEPROM sector 1
Write EEPROM sector 1
End of IAP EEPROM Example