usb_pd_charger_battery#
Overview#
The PD charger + battery example is a simple demonstration based on the MCUXpresso SDK PD stack.
The application simulate battery product (for example: laptop), it prints the battery percent continually.
The demo works as DRP. When connect, the board can be source or sink.
System Requirement#
Hardware requirements#
One or two Type-C shield board
One or two 9V DC power suppliers
Type-C Cable
One or two hardwares (Tower module/base board, and so on) for a specific device, for example: lpcxpresso54114 board
Personal Computer
Software requirements#
The project files are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_pd_charger_battery/ / .
The
is Bare Metal or FreeRTOS OS.
Terminal tool.
Getting Started#
Hardware Settings#
For detailed instructions, see the appropriate board User’s Guide.
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example#
Download the program to the target board.
Power on Type-C shield board then power on development board.
Run the example#
Connect the board to one charger or another shield board + development board (download this program too) with Type-C cable.
Connect the OpenSDA USB port to the PC and open terminal.
If running as source after connect.
If battery is (30%, 100%]: source caps are high power (5V/9V).
If battery is (0%, 30%]: source caps are low power (only 5V).
If partner request power role swap: accept.
prefer to work as sink.
get partner source cap, and judge whether to swap (if partner is external powered and satisfy self request).
if get partner source cap fail, retry one more time.
if can swap, then start power role swap.
if cannot swap or get source cap fail. still work as source.
do power role swap.
if fail, re-try one more time, if still fail, still work as source.
if success, please reference to sink description.
battery will decrease (if battery decrease to [0%, 20%]):
get partner source cap, and judge whether to swap (source cap satisfy self request).
if get partner source cap fail, retry one more time.
if can swap, then start power role swap.
if cannot swap or get source cap fail, send low power source caps.
do power role swap.
if fail, re-try one more time, if still fail send low power source caps.
if success, please reference to sink description.
if swap fail, after send low power source caps to trigger source capabilities change.
retry swap with interval 10s.
if battery decrease to 5%:
stop provide vbus.
set Try.SNK
Running as sink after connect.
when connect:
if battery is less than 100%: request high power (9V).
if battery is 100%: request low power (5V).
when battery increase to 100%, request low power (5V).
If partner request power role swap
if battery is (30%, 100%]: accept.
if battery is [0%, 30%]: reject.
when battery increase to (30%, 100%]:
update self source caps as high power.
Supported Boards#
MIMXRT1170-EVKB
FRDM-K22F
LPCXpresso55S69
EVK-MIMXRT1064
MIMXRT685-AUD-EVK
LPCXpresso55S16
MIMXRT1060-EVKB
MIMXRT1040-EVK
FRDM-MCXN947
FRDM-MCXN947T
MIMXRT1024-EVK
LPCXpresso55S28
LPCXpresso55S36
MCX-N5XX-EVK
MIMXRT1060-EVKC
MIMXRT1160-EVK
MIMXRT1180-EVK
FRDM-K32L2A4S
EVK-MIMXRT1020
MIMXRT700-EVK
FRDM-IMXRT700
EVK-MIMXRT595
EVK-MIMXRT685
MCX-N9XX-EVK
EVKB-IMXRT1050
EVK-MIMXRT1015
FRDM-MCXN236
FRDM-IMXRT1152