memfault#
Overview#
This example demonstrates how to use Memfault SDK to collect fault data. The dumped data is saved to flash, and can be sent to Memfault cloud for analysis. For more dtails, please refer to: https://memfault.com/
NOTE Only flash targets are supported!
This project only dumps some necessary memory regions, if you want to dump more,
please refer to the memfault document: https://docs.memfault.com/docs/mcu/coredumps#choosing-what-to-store-in-a-coredump,
and create your own function memfault_platform_coredump_get_regions to override
the default one which is a weak function in file memfault_platform_port.c.
Configuration#
A flash region is reserved for memfault dumped data, this flash region position and size can be configured.
When use Kconfig, go to the “Component Configuration -> Debug -> MemFault SDK”,
configure the “Backend flash offset” and “Backend flash size”.
When use the package without Kconfig, modify the macros CONFIG_MEMFAULT_FLASH_BASE_OFFSET
and CONFIG_MEMFAULT_FLASH_SIZE in file “mcux_config.h”.
NOTE When the flash region is reconfigured, the linker script should be updated too, to make sure the flash region match.
Running the project#
Follow the instructions in the terminal, press ‘A’ to trigger a fault. When the fault occurs, MCU will dump the data to flash reset. After reset, press ‘B’ to show the dumped data and send the data to Memfault cloud to check.
After ‘B’ is pressed, the dumped data is cleared from flash, so if ‘B’ is pressed again, no data will be shown.
Option ‘C’ is self test, if run pass, Test successed will be printed.
Note If run ‘A’ then ‘C’, the test will fail, because there is valid dump data
in flash, selftest can’t erase the dump data.
Analyze the dumped result#
There are two methods to analyze the dumped result: Upload dumped data chunk to Memfault server, or debug use GDB.
Upload data chunk to Memfault server#
When ‘B’ is pressed, the data chunks are shown in the terminal, post the data following such guide: https://docs.memfault.com/docs/mcu/export-chunks-over-console
Debug with GDB#
Install the python tool using command
pip install memfault-core-convert. Details of this tool is: https://pypi.org/project/memfault-core-convert/Export the dumped data in flash, for example, using gdb command like,
dump binary memory memfault-core.bin 0x00010000 0x00018000, fill the right flash address according to your settings. An easy way is dump all memfault flash region, the region base address is:CONFIG_FLASH_BASE_ADDRESS+CONFIG_MEMFAULT_FLASH_BASE_OFFSET, the regioni size is:CONFIG_MEMFAULT_FLASH_SIZE. These values can be got from the file “mcux_config.h”.Generate the core elf file use
memfault-core-convert --file memfault-core.bin --out_elf core.elfRun GDB to debug:
arm-none-eabi-gdb -se memfault.elf --core core.elf, herememfault.elfis current project image.
Detailed steps can be found here: https://docs.memfault.com/docs/mcu/coredump-elf-with-gdb.
NOTE Don’t run step 2 after pressing ‘B’, because the flash will be cleaned when press ‘B’.
Supported Boards#
FRDM-RW612
Hardware requirements
Micro USB cable
FRDM-RW612 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
RD-RW612-BGA
Hardware requirements
Micro USB cable
RD-RW612-BGA board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
FRDM-MCXW71
Hardware requirements
Type-C USB cable
FRDM-MCXW71 Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.