MCUXpresso SDK Changelog#
Board Support Files#
board#
[25.06.00]#
Initial version
clock_config#
[25.06.00]#
Initial version
pin_mux#
[25.06.00]#
Initial version
ADC16#
[2.3.0]#
Improvements
Added new API ADC16_EnableAsynchronousClockOutput() to enable/disable ADACK output.
In ADC16_GetDefaultConfig(), set enableAsynchronousClock to false.
[2.2.0]#
Improvements
Added hardware average mode in adc_config_t structure, then the hardware average mode can be set by invoking ADC16_Init() function.
[2.1.0]#
New Features:
Supported KM series’ new ADC reference voltage source, bandgap from PMC.
[2.0.3]#
Bug Fixes
Fixed IAR warning Pa082: the order of volatile access should be defined.
[2.0.2]#
Improvements
Used conversion control feature macro instead of that in IO map.
[2.0.1]#
Bug Fixes
Fixed MISRA-2012 rules.
Rule 16.4, 10.1, 13.2, 14.4 and 17.7.
[2.0.0]#
Initial version
AFE#
[2.0.3]#
Improvements
Fixed CERT-C issues
[2.0.2]#
Bug Fixes
Fixed MISRA C-2012 rule 10.1, rule 10.4 and so on.
[2.0.1]#
Improvements
Changed type modifiers from const xx_Type * s_xxBases to xx_Type *const s_xxBases.
Added static modifier for s_xxx variables defined in drivers.
[2.0.0]#
Initial version.
CLOCK#
[2.0.2]#
Bug Fixes
Fixed MSG issues.
[2.0.1]#
Bug Fixes
Fixed an issue that in CLOCK_SetFbeMode() C4 register not updated.
[2.0.0]#
Initial version.
CMP#
[2.0.3]#
Improvements
Updated to clear CMP settings in DeInit function.
[2.0.2]#
Bug Fixes
Fixed the violations of MISRA 2012 rules:
Rule 10.3
[2.0.1]#
Bug Fixes
Fixed MISRA-2012 rules.
Rule 14.4, rule 10.3, rule 10.1, rule 10.4 and rule 17.7.
[2.0.0]#
Initial version.
COMMON#
[2.6.7]#
Improvements
EnableIRQ/DisableIRQ: Use IRQSTEER_GetInstIdxByIRQ() to determine IRQSTEER instance index instead of simple division. Supports multiple IRQSTEER instances with different interrupt counts.
[2.6.6]#
Improvements
Support Cortex M55.
[2.6.5]#
Bug Fixes
Fixed the issue that the function SDK_DelayAtLeastUs may underflow and cause a long delay when the input parameter is small and the system clock is low.
[2.6.4]#
New Features
Add macros to tag deprecated features and experimental features.
[2.6.3]#
New Features
Added bit mask inversion macros to avoid type promotion.
Added register operation macros.
Improvements
Make function
MSDK_EnableCpuCycleCountercompatible with CMSIS-5 and CMSIS-6.
Bug Fixes
Fixed build issue of CMSIS PACK BSP example caused by CMSIS 6.1 issue.
[2.6.2]#
Bug Fixes
Fixed violations of MISRA C-2012 rule for implicit conversions in boolean contexts
[2.6.1]#
Improvements
Support Cortex M23.
[2.6.0]#
Bug Fixes
Fix CERT-C violations.
[2.5.0]#
New Features
Added new APIs InitCriticalSectionMeasurementContext, DisableGlobalIRQEx and EnableGlobalIRQEx so that user can measure the execution time of the protected sections.
[2.4.3]#
Improvements
Enable irqs that mount under irqsteer interrupt extender.
[2.4.2]#
Improvements
Add the macros to convert peripheral address to secure address or non-secure address.
[2.4.1]#
Improvements
Improve for the macro redefinition error when integrated with zephyr.
[2.4.0]#
New Features
Added EnableIRQWithPriority, IRQ_SetPriority, and IRQ_ClearPendingIRQ for ARM.
Added MSDK_EnableCpuCycleCounter, MSDK_GetCpuCycleCount for ARM.
[2.3.3]#
New Features
Added NETC into status group.
[2.3.2]#
Improvements
Make driver aarch64 compatible
[2.3.1]#
Bug Fixes
Fixed MAKE_VERSION overflow on 16-bit platforms.
[2.3.0]#
Improvements
Split the driver to common part and CPU architecture related part.
[2.2.10]#
Bug Fixes
Fixed the ATOMIC macros build error in cpp files.
[2.2.9]#
Bug Fixes
Fixed MISRA C-2012 issue, 5.6, 5.8, 8.4, 8.5, 8.6, 10.1, 10.4, 17.7, 21.3.
Fixed SDK_Malloc issue that not allocate memory with required size.
[2.2.8]#
Improvements
Included stddef.h header file for MDK tool chain.
New Features:
Added atomic modification macros.
[2.2.7]#
Other Change
Added MECC status group definition.
[2.2.6]#
Other Change
Added more status group definition.
Bug Fixes
Undef __VECTOR_TABLE to avoid duplicate definition in cmsis_clang.h
[2.2.5]#
Bug Fixes
Fixed MISRA C-2012 rule-15.5.
[2.2.4]#
Bug Fixes
Fixed MISRA C-2012 rule-10.4.
[2.2.3]#
New Features
Provided better accuracy of SDK_DelayAtLeastUs with DWT, use macro SDK_DELAY_USE_DWT to enable this feature.
Modified the Cortex-M7 delay count divisor based on latest tests on RT series boards, this setting lets result be closer to actual delay time.
[2.2.2]#
New Features
Added include RTE_Components.h for CMSIS pack RTE.
[2.2.1]#
Bug Fixes
Fixed violation of MISRA C-2012 Rule 3.1, 10.1, 10.3, 10.4, 11.6, 11.9.
[2.2.0]#
New Features
Moved SDK_DelayAtLeastUs function from clock driver to common driver.
[2.1.4]#
New Features
Added OTFAD into status group.
[2.1.3]#
Bug Fixes
MISRA C-2012 issue fixed.
Fixed the rule: rule-10.3.
[2.1.2]#
Improvements
Add SUPPRESS_FALL_THROUGH_WARNING() macro for the usage of suppressing fallthrough warning.
[2.1.1]#
Bug Fixes
Deleted and optimized repeated macro.
[2.1.0]#
New Features
Added IRQ operation for XCC toolchain.
Added group IDs for newly supported drivers.
[2.0.2]#
Bug Fixes
MISRA C-2012 issue fixed.
Fixed the rule: rule-10.4.
[2.0.1]#
Improvements
Removed the implementation of LPC8XX Enable/DisableDeepSleepIRQ() function.
Added new feature macro switch “FSL_FEATURE_HAS_NO_NONCACHEABLE_SECTION” for specific SoCs which have no noncacheable sections, that helps avoid an unnecessary complex in link file and the startup file.
Updated the align(x) to attribute(aligned(x)) to support MDK v6 armclang compiler.
[2.0.0]#
Initial version.
CRC#
[2.1.0]#
Bug fix:
Choosing CRC clocks from CRC clock array according to instance instead of hardcoded value.
[2.0.5]#
Bug fix:
Fix CERT-C issue with boolean-to-unsigned integer conversion.
[2.0.4]#
Improvements
Release peripheral from reset if necessary in init function.
[2.0.3]#
Bug fix:
Fix MISRA issues.
[2.0.2]#
Bug fix:
Fix MISRA issues.
[2.0.1]#
Bug fix:
DATA and DATALL macro definition moved from header file to source file.
[2.0.0]#
Initial version.
DMA#
[2.1.4]#
New Features
Added common IRQ handler entry DMA_DriverIRQHandler.
[2.1.3]#
Bug Fixes
Fixed coverity issues with CERT INT30-C, CERT INT31-C compliance.
[2.1.2]#
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.3.
[2.1.1]#
Improvements
Corrected the dma channel feature macro from FSL_FEATURE_DMAMUX_MODULE_CHANNEL to FSL_FEATURE_DMA_MODULE_CHANNEL.
[2.1.0]#
Improvements
Added api DMA_PrepareTransferConfig to expose option address increment.
Added api DMA_EnableAutoStopRequest to support auto stop request feature.
[2.0.2]#
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.4, 10.3, 14.4, 16.4, 11.6, 10.1.
[2.0.1]#
Bug Fixes
By adding parenthesis, fixed the build fail of DMA driver due to rule 12.5, MISRA C 2004.
[2.0.0]#
Initial version.
DMAMUX#
[2.1.4]#
Bug Fixes
Fixed CERT INT31-C violation in DMAMUX_SetSource by adding non-negative assertion and explicit cast.
[2.1.3]#
Improvements
Wrap DMAMUX_GetInstance into FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL to avoid build issues.
[2.1.2]#
Bug Fixes
Add macro FSL_DMAMUX_CHANNEL_NUM to calculat correct DMAMUX channel number when input EDAM channel number.
[2.1.1]#
Improvements
Add macro FSL_FEATURE_DMAMUX_CHANNEL_NEEDS_ENDIAN_CONVERT and DMAMUX_CHANNEL_ENDIAN_CONVERTn do channel endian convert.
[2.1.0]#
Improvements
Modify the type of parameter source from uint32_t to int32_t in the DMAMUX_SetSource.
[2.0.5]#
Improvements
Added feature FSL_FEATURE_DMAMUX_CHCFG_REGISTER_WIDTH for the difference of CHCFG register width.
[2.0.4]#
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.4.
[2.0.3]#
Bug Fixes
Fixed the issue for MISRA-2012 check.
Fixed rule 10.4 and rule 10.3.
[2.0.2]#
New Features
Added an always-on enable feature to a DMA channel for ULP1 DMAMUX support.
[2.0.1]#
Bug Fixes
Fixed the build warning issue by changing the type of parameter source from uint8_t to uint32_t when setting DMA request source in DMAMUX_SetSourceChange.
[2.0.0]#
Initial version.
EWM#
[2.0.4]#
Bug Fixes
Fixed CERT INT31-C violations.
[2.0.3]#
Bug Fixes
Fixed violation of MISRA C-2012 rules: 10.1, 10.3.
[2.0.2]#
Bug Fixes
Fixed violation of MISRA C-2012 rules: 10.3, 10.4.
[2.0.1]#
Bug Fixes
Fixed the hard fault in EWM_Deinit.
[2.0.0]#
Initial version.
FLASH#
[3.3.0]#
New Feature
Support for EEPROM Quick Write on devices with FTFC
[3.2.0]#
New Feature
Basic support for FTFC
[3.1.3]#
New Feature
Support 512KB flash for Kinetis E serials.
[3.1.2]#
Bug Fixes — Remove redundant comments.
[3.1.1]#
Bug Fixes — MISRA C-2012 issue fixed: rule 10.3
[3.1.0]#
New Feature
Support erase flash asynchronously.
[3.0.2]#
Bug Fixes — MISRA C-2012 issue fixed: rule 8.4, 17.7, 10.4, 16.1, 21.15, 11.3, 10.7 — building warning -Wnull-dereference on arm compiler v6
[3.0.1]#
New Features
Added support FlexNVM alias for (kw37/38/39).
[3.0.0]#
Improvements
Reorganized FTFx flash driver source file.
Extracted flash cache driver from FTFx driver.
Extracted flexnvm flash driver from FTFx driver.
[2.3.1]#
Bug Fixes
Unified Flash IFR design from K3.
New encoding rule for K3 flash size.
[2.3.0]#
New Features
Added support for device with LP flash (K3S/G).
Added flash prefetch speculation APIs.
Improvements
Refined flash_cache_clear function.
Reorganized the member of flash_config_t struct.
[2.2.0]#
New Features
Supported FTFL device in FLASH_Swap API.
Supported various pflash start addresses.
Added support for KV58 in cache clear function.
Added support for device with secondary flash (KW40).
Bug Fixes
Compiled execute-in-ram functions as PIC binary code for driver use.
Added missed flexram properties.
Fixed unaligned variable issue for execute-in-ram function code array.
[2.1.0]#
Improvements
Updated coding style to align with KSDK 2.0.
Different-alignment-size support for pflash and flexnvm.
Improved the implementation of execute-in-ram functions.
[2.0.0]#
Initial version
GPIO#
[2.8.6]#
Bug Fixes
Fixed CERT INT31-C violations in
GPIO_FIT_REGmacro for platforms with 8-bit register width.
[2.8.5]#
Improvements
Add AND logic in GPIO_GpioClearInterruptFlags to support clearing multiple interrupt flags simultaneously.
[2.8.4]#
Improvements
Make function
GPIO_PortGetInterruptFlagsandGPIO_PortClearInterruptFlagsavailable for all variants, they are used for all pins flags in one GPIO port.
[2.8.3]#
Bug Fixes
Fixed violations of the MISRA C-2012 Rule 10.1, 5.7.
[2.8.2]#
Bug Fixes
Fixed COVERITY issue that GPIO_GetInstance could return clock array overflow values due to GPIO base and clock being out of sync.
[2.8.1]#
Bug Fixes
Fixed CERT INT31-C issues.
[2.8.0]#
Improvements
Add API GPIO_PortInit/GPIO_PortDeinit to set GPIO clock enable and releasing GPIO reset.
[2.8.0]#
Improvements
Add API GPIO_PortInit/GPIO_PortDeinit to set GPIO clock enable and releasing GPIO reset.
Remove support for API GPIO_GetPinsDMARequestFlags with GPIO_ISFR_COUNT <= 1.
[2.7.3]#
Improvements
Release peripheral from reset if necessary in init function.
[2.7.2]#
New Features
Support devices without PORT module.
[2.7.1]#
Bug Fixes
Fixed MISRA C-2012 rule 10.4 issues in GPIO_GpioGetInterruptChannelFlags() function and GPIO_GpioClearInterruptChannelFlags() function.
[2.7.0]#
New Features
Added API to support Interrupt select (IRQS) bitfield.
[2.6.0]#
New Features
Added API to get GPIO version information.
Added API to control a pin for general purpose input.
Added some APIs to control pin in secure and previliege status.
[2.5.3]#
Bug Fixes
Correct the feature macro typo: FSL_FEATURE_GPIO_HAS_NO_INDEP_OUTPUT_CONTORL.
[2.5.2]#
Improvements
Improved GPIO_PortSet/GPIO_PortClear/GPIO_PortToggle functions to support devices without Set/Clear/Toggle registers.
[2.5.1]#
Bug Fixes
Fixed wrong macro definition.
Fixed MISRA C-2012 rule issues in the FGPIO_CheckAttributeBytes() function.
Defined the new macro to separate the scene when the width of registers is different.
Removed some redundant macros.
New Features
Added some APIs to get/clear the interrupt status flag when the port doesn’t control pins’ interrupt.
[2.4.1]#
Improvements
Improved GPIO_CheckAttributeBytes() function to support 8 bits width GACR register.
[2.4.0]#
Improvements
API interface added:
New APIs were added to configure the GPIO interrupt clear settings.
[2.3.2]#
Bug Fixes
Fixed the issue for MISRA-2012 check.
Fixed rule 3.1, 10.1, 8.6, 10.6, and 10.3.
[2.3.1]#
Improvements
Removed deprecated APIs.
[2.3.0]#
New Features
Updated the driver code to adapt the case of interrupt configurations in GPIO module. New APIs were added to configure the GPIO interrupt settings if the module has this feature on it.
[2.2.1]#
Improvements
API interface changes:
Refined naming of APIs while keeping all original APIs by marking them as deprecated. The original APIs will be removed in next release. The main change is updating APIs with prefix of _PinXXX() and _PortXXX.
[2.1.1]#
Improvements
API interface changes:
Added an API for the check attribute bytes.
[2.1.0]#
Improvements
API interface changes:
Added “pins” or “pin” to some APIs’ names.
Renamed “_PinConfigure” to “GPIO_PinInit”.
I2C#
[2.0.12]#
Bug Fixes
Set the C1[TXAK] before start of reading last byte to sent NACK in I2C_MasterReadBlocking().
Updated I2C_MasterTransferBlocking() to does not change xfer->subaddressSize.
[2.0.11]#
New Features
Added common IRQ handler entry I2C_DriverIRQHandler.
[2.0.10]#
Bug Fixes
Fixed coverity issues.
[2.0.9]#
Bug Fixes
Fixed the MISRA-2012 violations.
Fixed rule 8.4, 10.1, 10.4, 13.5, 20.8.
[2.0.8]#
Bug Fixes
Fixed the bug that DFEN bit of I2C Status register 2 could not be set in I2C_MasterInit.
MISRA C-2012 issue fixed: rule 14.2, 15.7, and 16.4.
Eliminated IAR Pa082 warnings from I2C_MasterTransferDMA and I2C_MasterTransferCallbackDMA by assigning volatile variables to local variables and using local variables instead.
Fixed MISRA issues.
Fixed rules 10.1, 10.3, 10.4, 11.9, 14.4, 15.7, 17.7.
Improvements
Improved timeout mechanism when waiting certain state in transfer API.
Updated the I2C_WAIT_TIMEOUT macro to unified name I2C_RETRY_TIMES.
Moved the master manually acknowledge byte operation into static function I2C_MasterAckByte.
Fixed control/status clean flow issue inside I2C_MasterReadBlocking to avoid potential issue that pending status is cleaned before it’s proceeded.
[2.0.7]#
Bug Fixes
Fixed the issue for MISRA-2012 check.
Fixed rule 11.9 ,15.7 ,14.4 ,10.4 ,10.8 ,10.3, 10.1, 10.6, 13.5, 11.3, 13.2, 17.7, 5.7, 8.3, 8.5, 11.1, 16.1.
Fixed Coverity issue of unchecked return value in I2C_RTOS_Transfer.
Fixed variable redefine issue by moving i2cBases from fsl_i2c.h to fsl_i2c.c.
Improvements
Added I2C_MASTER_FACK_CONTROL macro to enable FACK control for master transfer receive flow with IP supporting double buffer, then master could hold the SCL by manually setting TX AK/NAK during data transfer.
[2.0.6]#
Bug Fixes
Fixed the issue that I2C Master transfer APIs(blocking/non-blocking) did not support the situation of master transfer with subaddress and transfer data size being zero, which means no data followed by the subaddress.
[2.0.5]#
Improvements
Added I2C_WATI_TIMEOUT macro to allow the user to specify the timeout times for waiting flags in functional API and blocking transfer API.
[2.0.4]#
Bug Fixes
Added a proper handle for transfer config flag kI2C_TransferNoStartFlag to support transmit with kI2C_TransferNoStartFlag flag. Support write only or write+read with no start flag; does not support read only with no start flag.
[2.0.3]#
Bug Fixes
Removed enableHighDrive member in the master/slave configuration structure because the operation to HDRS bit is useless, the user need to use DSE bit in port register to configure the high drive capability.
Added register reset operation in I2C_MasterInit and I2C_SlaveInit APIs. Fixed issue where I2C could not switch between master and slave mode.
Improved slave IRQ handler to handle the corner case that stop flag and address match flag come synchronously.
[2.0.2]#
Bug Fixes
Fixed issue in master receive and slave transmit mode with no stop flag. The master could not succeed to start next transfer because the master could not send out re-start signal.
Fixed the out-of-order issue of data transfer due to memory barrier.
Added hold time configuration for slave. By leaving the SCL divider and MULT reset values when configured to slave mode, the setup and hold time of the slave is then reduced outside of spec for lower baudrates. This can cause intermittent arbitration loss on the master side.
New Features
Added address nak event for master.
Added general call event for slave.
[2.0.1]#
New Features
Added double buffer enable configuration for SoCs which have the DFEN bit in S2 register.
Added flexible transmit/receive buffer size support in I2C_SlaveHandleIRQ.
Added start flag clear, address match, and release bus operation in I2C_SlaveWrite/ReadBlocking API.
Bug Fixes
Changed the kI2C_SlaveRepeatedStartEvent to kI2C_SlaveStartEvent.
[2.0.0]#
Initial version.
IRTC#
[2.3.4]#
Bug Fixes
Fixed CERT INT31-C violations to ensure safe integer conversions.
[2.3.3]#
Bug Fixes
Fix CERT INT31-C issue.
[2.3.2]#
Bug Fixes
Fixed API IRTC_GetDatetime read YEARMON, DAYS, HOURMIN, SECONDS registers issue.
[2.3.1]#
Bug Fixes
Fixed MISRA C-2012 issue 10.4.
[2.3.0]#
New Feature
Supported platforms with multiple IRTC instances.
[2.2.4]#
Bug Fixes
Fixed MISRA C-2012 issue 10.1, 10.3, 10.4, 10.7, 12.2.
[2.2.3]#
Bug Fixes
Updated undefined macro names by available ones.
[2.2.2]#
Bug Fixes
Fixed MISRA C-2012 issue 10.3.
[2.2.1]#
Bug Fixes
Fixed MISRA issues.
[2.2.0]#
New Feature
Add new APIs for CLK_SEL and CLKO to select RTC clock and enable/disable output to peripherals.
Supported platforms without tamper feature.
[2.1.3]#
Bug Fixes
Fixed MISRA C-2012 issue 10.1 and 10.4.
[2.1.2]#
Bug Fixes
Fixed kIRTC_TamperFlag flag can’t be cleared issue.
[2.1.1]#
Bug Fixes
MISRA C-2012 issue check.
Fixed rules, containing: rule-10.1, rule-10.3, rule-10.4.
[2.1.0]#
Bug Fixes
Fixed incorrect leap year check in IRTC_CheckDatetimeFormat.
New Feature
Added new APIs for new feature FSL_FEATURE_RTC_HAS_SUBSYSTEM.
Added new APIs for TAMPER, TAMPER QUEUE status get and clear.
Added new API to enable/disable 32 kHz RTC OSC clock during RTC register write.
Updated IRTC_SetTamperParams to support new feature FSL_FEATURE_RTC_HAS_FILTER23_CFG
Updated irtc_config_t to exclude member wakeupSelect for new feature FSL_FEATURE_RTC_HAS_NO_CTRL2_WAKEUP_MODE.
[2.0.2]#
Bug Fixes
MISRA C-2012 issue check.
Fixed rules, containing: rule-10.1, rule-10.3, rule-10.4, rule-10.6, rule-10.8, rule-11.9, rule-12.2, rule-15.5, rule-16.4, rule-17.7.
[2.0.1]#
Bug Fixes
Fixed the issue of hard code in IRTC_Init.
[2.0.0]#
Initial version.
LLWU#
[2.0.5]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules 10.3.
Fixed the issue that function LLWU_SetExternalWakeupPinMode() does not work on 32-bit width platforms.
[2.0.4]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules 10.3, 10.4, 10.6, 10.7, 11.3.
Fixed issue that LLWU_ClearExternalWakeupPinFlag may clear other filter flags by mistake on platforms with 32-bit LLWU registers.
[2.0.3]#
Bug Fixes
Fixed MISRA-2012 rules.
Rule 16.4.
[2.0.2]#
Improvements
Corrected driver function LLWU_SetResetPinMode parameter name.
Bug Fixes
Fixed MISRA-2012 rules.
Rule 14.4, 10.8, 10.4, 10.3.
[2.0.1]#
Other Changes
Updates for KL8x.
[2.0.0]#
Initial version.
LPTMR#
[2.2.1]#
Bug Fixes
Fix CERT INT31-C issues.
[2.2.0]#
Improvements
Updated lptmr_prescaler_clock_select_t, only define the valid options.
[2.1.1]#
Improvements
Updated the characters from “PTMR” to “LPTMR” in “FSL_FEATURE_PTMR_HAS_NO_PRESCALER_CLOCK_SOURCE_1_SUPPORT” feature definition.
[2.1.0]#
Improvements
Implement for some special devices’ not supporting for all clock sources.
Bug Fixes
Fixed issue when accessing CMR register.
[2.0.2]#
Bug Fixes
Fixed MISRA-2012 issues.
Rule 10.1.
[2.0.1]#
Improvements
Updated the LPTMR driver to support 32-bit CNR and CMR registers in some devices.
[2.0.0]#
Initial version.
MCM#
[2.2.1]#
Improvements
Add feature to support platforms that do not have the MCM CPCR (Core Platform Control Register).
[2.2.0]#
Improvements
Support platforms with less features.
[2.1.0]#
Others
Remove byteID from mcm_lmem_fault_attribute_t for document update.
[2.0.0]#
Initial version.
PIT#
[2.2.0]#
Bug Fixes
According to ERR050763, PIT_LDVAL_STAT register is not reliable in dynamic load mode, so remove the status check in PIT_SetRtiTimerPeriod which added since 2.1.1.
Removed not used bit PIT_RTI_TCTRL_CHN_MASK.
Improvements
Added more guide about get RTI load status in PIT_SetRtiTimerPeriod’s API comment.
Change PIT_RTI_Deinit to inline API.
Ensure PIT peripheral clock enabled in PIT_RTI_Init.
New Features
Added PIT_ClearRtiSyncStatus API to clear the RTI_LDVAL_STAT register.
[2.1.1]#
Bug Fixes
Enable PIT when using RTI to ensure RTI can work properly in debug mode.
Improvements
Added status check in PIT_SetRtiTimerPeriod to ensure the load value is synchronized into the RTI clock domain.
Added note for PIT_RTI_Init to remind users wait RTI sync.
[2.1.0]#
New Features
Support RTI (Real Time Interrupt) timer.
[2.0.5]#
Improvements
Support workaround for ERR007914. This workaround guarantee the write to MCR register is not ignored.
[2.0.4]#
Bug Fixes
Fixed PIT_SetTimerPeriod implementation, the load value trigger should be PIT clock cycles minus 1.
[2.0.3]#
Bug Fixes
Clear all status bits for all channels to make sure the status of all TCTRL registers is clean.
[2.0.2]#
Bug Fixes
Fixed MISRA-2012 issues.
Rule 10.1.
[2.0.1]#
Bug Fixes
Cleared timer enable bit for all channels in function PIT_Init() to make sure all channels stay in disable status before setting other configurations.
Fixed MISRA-2012 rules.
Rule 14.4, rule 10.4.
[2.0.0]#
Initial version.
PMC#
[2.0.4]#
Bug Fixes
Add validation before narrowing uint32_t to uint8_t conversions using assert
Replace direct boolean to integer casts with explicit ternary operators
Add INT31-C compliance comments for safe narrowing conversions
Apply fixes to PMC_ConfigureLowVoltDetect, PMC_ConfigureLowVoltWarning, and PMC_ConfigureBandgapBuffer functions
[2.0.3]#
Bug Fixes
Fixed the violation of MISRA C-2012 rule 11.3.
[2.0.2]#
Bug Fixes
Fixed the violations of MISRA 2012 rules:
Rule 10.3.
[2.0.1]#
Bug Fixes
Fixed MISRA issues.
Rule 10.8, Rule 10.3.
[2.0.0]#
Initial version.
PORT#
[2.5.1]#
Bug Fixes
Fix CERT INT31-C issues.
Fixed the violations of MISRA C-2012 rules: 10.1.
[2.5.0]#
Bug Fixes
Correct the kPORT_MuxAsGpio for some platforms.
[2.4.1]#
Bug Fixes
Fixed the violations of MISRA C-2012 rules: 10.1, 10.8 and 14.4.
[2.4.0]#
New Features
Updated port_pin_config_t to support input buffer and input invert.
[2.3.0]#
New Features
Added new APIs for Electrical Fast Transient(EFT) detect.
Added new API to configure port voltage range.
[2.2.0]#
New Features
Added new api PORT_EnablePinDoubleDriveStrength.
[2.1.1]#
Bug Fixes
Fixed the violations of MISRA C-2012 rules: 10.1, 10.4,11.3,11.8, 14.4.
[2.1.0]#
New Features
Updated the driver code to adapt the case of the interrupt configurations in GPIO module. Will move the pin configuration APIs to GPIO module.
[2.0.2]#
Other Changes
Added feature guard macros in the driver.
[2.0.1]#
Other Changes
Added “const” in function parameter.
Updated some enumeration variables’ names.
QTMR#
[2.0.2]#
Bug Fixes
Fix CERT INT30-C and CERT INT31-C violations.
[2.0.1]#
Bug Fixes
MISRA C-2012 issue check.
Fixed rules, containing: rule-10.1, rule-10.3, rule-10.4, rule-11.9, rule-14.4, rule-15.5, rule-17.7.
Changed FSL_COMPONENT_ID as platform.drivers.qtmr_2.
[2.0.0]#
Initial version.
RCM#
[2.0.5]#
Bug Fixes
Replace direct boolean to integer casts with explicit ternary operators for INT31-C compliance.
Add validation before narrowing uint32_t to uint8_t conversion using assert.
Add INT31-C compliance comments for safe type handling.
Apply fixes to RCM_ConfigureResetPinFilter and RCM_SetForceBootRomSource functions.
[2.0.4]#
Bug Fixes
Fixed violation of MISRA C-2012 rule 10.3
[2.0.3]#
Bug Fixes
Fixed violation of MISRA C-2012 rules.
[2.0.2]#
Bug Fixes
Fixed MISRA issue.
Rule 10.8, rule 10.1, rule 13.2, rule 3.1.
[2.0.1]#
Bug Fixes
Fixed kRCM_SourceSw bit shift issue.
[2.0.0]#
Initial version.
RNGA#
[2.0.2]#
Bug fix:
Fix MISRA issue.
[2.0.1]#
Bug fix:
Fixed C++ build warning in RNGA driver.
[2.0.0]#
Initial version.
SIM#
[2.2.0]#
Improvements
Added API to trigger TRGMUX.
[2.1.3]#
Improvements
Updated function SIM_GetUniqueId to support different register names.
[2.1.2]#
Bug Fixes
Fixed SIM_GetUniqueId bug that could not get UIDH.
[2.1.1]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules 10.1, 10.4
[2.1.0]#
Improvements
Added new APIs: SIM_GetRfAddr() and SIM_EnableSystickClock().
[2.0.0]#
Initial version.
SLCD#
[2.1.1]#
Improvements
Update slcd_duty_cycle_t, slcd_phase_type_t and slcd_phase_index_t, MCXA3xx SoCs only have 48 pins and 4 pack plane phases.
Added check for front plane pin index and back plane phase index.
[2.1.0]#
New Features
Added new enumerations, updated SLCD_Init and SLCD_GetDefaultConfig to support new low power IP on new SoCs.
[2.0.4]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules 10.4.
[2.0.3]#
Bug Fixes
Fixed SLCD_Init bug that some bit-fileds are cleared by mistake.
[2.0.2]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules 3.1, 10.1, 10.3, 10.3, 10.4 11.4, 17.7
[2.0.1]#
Bug Fixes
Changed the Blink mode start setting flow.
Other Changes
Added static to SLCD global variables.
[2.0.0]#
Initial version.
SMC#
[2.0.9]#
Bug Fixes
Replace width-unsafe register mask inversion with a
smc_reg_t-aware helper for INT31-C compliance
[2.0.8]#
Bug Fixes
Replace direct boolean to integer casts with explicit ternary operators for INT31-C compliance
Add validation before narrowing uint32_t to uint8_t conversion using assert
Add INT31-C compliance comments for safe type handling
Apply fixes to RCM_ConfigureResetPinFilter and RCM_SetForceBootRomSource functions
[2.0.7]#
Bug Fixes
Fixed MISRA-2012 issue 10.3.
[2.0.6]#
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule 10.3, rule 11.3.
[2.0.5]#
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule 15.7, rule 14.4, rule 10.3, rule 10.1, rule 10.4.
[2.0.4]#
Bug Fixes
When entering stop modes, used RAM function for the flash synchronization issue. Application should make sure that, the RW data of fsl_smc.c is located in memory region which is not powered off in stop modes.
[2.0.3]#
Improvements
Added APIs SMC_PreEnterStopModes, SMC_PreEnterWaitModes, SMC_PostExitWaitModes, and SMC_PostExitStopModes.
[2.0.2]#
Bug Fixes
Added DSB before WFI while ISB after WFI.
Other Changes
Updated SMC_SetPowerModeVlpw implementation.
[2.0.1]#
Other Changes
Updated for KL8x.
[2.0.0]#
Initial version.
SPI#
[2.1.5]#
New Features
Added common IRQ handler entry SPI_DriverIRQHandler.
[2.1.4]#
Bug Fixes
Fixed coverity issues.
[2.1.3]#
Bug Fixes
Fixed the txData from void * to const void * in transmit API.
[2.1.2]#
Improvements
Changed SPI_DUMMYDATA to 0x00.
[2.1.1]#
Bug Fixes
Fixed MISRA 10.3 violation.
[2.1.0]#
Improvements
Added timeout mechanism when waiting certain states in transfer driver.
Bug Fixes
Fixed the bug that, when working as a slave, instance that does not have FIFO may miss some rx data.
Fixed master RX data overflow issue by synchronizing transmit and receive process.
Fixed issue that slave should not share the same non-blocking initialization API and IRQ handler with master to prevent dead lock issue.
Fixed issue that callback should be invoked after all data is sent out to bus.
Added code in SPI_SlaveTransferNonBlocking to empty rx buffer before initializing transfer.
[2.0.5]#
Bug Fixes
Eliminated Pa082 warnings from SPI_WriteNonBlocking and SPI_GetStatusFlags.
Fixed MISRA issues.
Fixed issues 10.1, 10.3, 10.4, 10.7, 10.8, 11.9, 14.4, 17.7.
[2.0.4]#
New Features
Supported 3-wire mode for SPI driver. Added new API SPI_SetPinMode() to control the transfer direction of the single wire. For master instance, MOSI is selected as I/O pin. For slave instance, MISO is selected as I/O pin.
Added dummy data setup API to allow users to configure the dummy data to be transferred.
[2.0.3]#
Bug Fixes
Fixed the potential interrupt race condition at high baudrate when calling API SPI_MasterTransferNonBlocking.
[2.0.2]#
New Features
Allowed users to set the transfer size for SPI_TransferNoBlocking non-integer times of watermark.
Allowed users to define the dummy data. Users only need to define the macro SPI_DUMMYDATA in applications.
[2.0.1]#
Bug Fixes
Fixed SPI_Enable function parameter error.
Set the s_dummy variable as static variable in fsl_spi_dma.c.
Improvements
Optimized the code size while not using transactional API.
Improved performance in polling method.
Added #ifndef/#endif to allow users to change the default tx value at compile time.
[2.0.0]#
Initial version.
SPI DMA Driver#
[2.1.1]#
Bug Fixes
Fixed the bug that TX data not sent to bus when transfer finish callback is called.
[2.1.0]#
Improvements
Added timeout mechanism when waiting certain states in transfer driver.
Bug Fixes
Fixed the bug that, when working as a slave, instance that does not have FIFO may miss some rx data.
Fixed master RX data overflow issue by synchronizing transmit and receive process.
Fixed issue that slave should not share the same non-blocking initialization API and IRQ handler with master to prevent dead lock issue.
Fixed issue that callback should be invoked after all data is sent out to bus.
Added code in SPI_SlaveTransferNonBlocking to empty rx buffer before initializing transfer.
[2.0.5]#
Bug Fixes
Eliminated Pa082 warnings from SPI_WriteNonBlocking and SPI_GetStatusFlags.
Fixed MISRA issues.
Fixed issues 10.1, 10.3, 10.4, 10.7, 10.8, 11.9, 14.4, 17.7.
[2.0.4]#
New Features
Supported 3-wire mode for SPI driver. Added new API SPI_SetPinMode() to control the transfer direction of the single wire. For master instance, MOSI is selected as I/O pin. For slave instance, MISO is selected as I/O pin.
Added dummy data setup API to allow users to configure the dummy data to be transferred.
[2.0.3]#
Bug Fixes
Fixed the potential interrupt race condition at high baudrate when calling API SPI_MasterTransferNonBlocking.
[2.0.2]#
New Features
Allowed users to set the transfer size for SPI_TransferNoBlocking non-integer times of watermark.
Allowed users to define the dummy data. Users only need to define the macro SPI_DUMMYDATA in applications.
[2.0.1]#
Bug Fixes
Fixed SPI_Enable function parameter error.
Set the s_dummy variable as static variable in fsl_spi_dma.c.
Improvements
Optimized the code size while not using transactional API.
Improved performance in polling method.
Added #ifndef/#endif to allow users to change the default tx value at compile time.
[2.0.0]#
Initial version.
SYSMPU#
[2.2.4]#
Bug Fixes
Fixed CERT INT30-C and CERT INT31-C violations.
[2.2.3]#
Bug Fixes
Fixed violation of MISRA C-2012 Rule 10.4, a part of issues is ignored before.
[2.2.2]#
Bug Fixes
Fixed violation of MISRA C-2012 Rule 10.1, 10.3, 10.4, 10.7, 10.6, 10.8, 12.2.
[2.2.1]#
Bug Fixes
Fixed MISRA issue.
[2.2.0]#
Improvements
Renamed MPU to SYSMPU.
Changed macro definition for slave number and fixed the get error status calculation.
[2.1.1]#
Improvements
Added the feature file macro definition limitation for the MPU_SetRegionRwMasterAccessRights().
[2.1.0]#
Other Changes
API changes:
Changed the mpu_region_num_t and mpu_master_t to uint32_t.
Changed the mpu_low_masters_access_rights_t, mpu_high_masters_access_rights_t to mpu_rwxrights_master_access_control_t, mpu_rwrights_master_access_control_t.
Changed the MPU_SetRegionLowMasterAccessRights(), MPU_SetRegionHighMasterAccessRights() to MPU_SetRegionRwxMasterAccessRights(), MPU_SetRegionRwMasterAccessRights().
[2.0.0]#
Initial version.
UART#
[2.5.2]#
New Features
Added common IRQ handler entry UART_DriverIRQHandler.
[2.5.1]#
Improvements
Use separate data for TX and RX in uart_transfer_t.
Bug Fixes
Fixed bug that when ring buffer is used, if some data is received in ring buffer first before calling UART_TransferReceiveNonBlocking, the received data count returned by UART_TransferGetReceiveCount is wrong.
[2.5.0]#
New Features
Added APIs UART_GetRxFifoCount/UART_GetTxFifoCount to get rx/tx FIFO data count.
Added APIs UART_SetRxFifoWatermark/UART_SetTxFifoWatermark to set rx/tx FIFO water mark.
Bug Fixes
Fixed bug of race condition during UART transfer using transactional APIs, by disabling and re-enabling the global interrupt before and after critical operations on interrupt enable registers.
Fixed DMA/eDMA transfer blocking issue by enabling tx idle interrupt after DMA/eDMA transmission finishes.
[2.4.0]#
New Features
Added APIs to configure 9-bit data mode, set slave address and send address.
[2.3.0]#
Bug Fixes
Fixed the bug that, when framing/parity/noise/overflow flag or idle line detect flag is set, receive FIFO should be flushed to avoid FIFO pointer being in unknown state, since FIFO has no valid data.
Improvements
Modified UART_TransferHandleIRQ so that txState will be set to idle only when all data has been sent out to bus.
Modified UART_TransferGetSendCount so that this API returns the real byte count that UART has sent out rather than the software buffer status.
Added timeout mechanism when waiting for certain states in transfer driver.
[2.2.0]#
New Features
Added UART hardware FIFO enable/disable API.
Improvements
Added check for kUART_TransmissionCompleteFlag in UART_TransferHandleIRQ, UART_SendEDMACallback and UART_TransferSendDMACallback to ensure all the data would be sent out to bus.
Bug Fixes
Eliminated IAR Pa082 warnings from UART_TransferGetRxRingBufferLength, UART_GetEnabledInterrupts, UART_GetStatusFlags and UART_TransferHandleIRQ.
Added code in UART_ReadBlocking so that if more than one receiver errors occur, all status flags will be cleared and the most severe error status will be returned.
Fixed MISRA issues.
Fixed rules 10.1, 10.3, 10.4, 14.4, 11.6, 17.7.
[2.1.6]#
Bug Fixes
Fixed the issue of register’s being in repeatedly reading status while performing the IRQ routine.
[2.1.5]#
Improvements
Added hardware flow control function support.
Added idle-line-detecting feature in UART_TransferNonBlocking function. If an idle line is detected, a callback will be triggered with status kStatus_UART_IdleLineDetected returned. This feature may be useful when the number of received bytes is less than the expected receive data size. Before triggering the callback, data in the FIFO is read out (if it has FIFO), and no interrupt will be disabled except for the case that the receive data size reaches 0.
Enabled the RX FIFO watermark function. With the idle-line-detecting feature enabled, you can set the watermark value to whatever you want (should not be bigger than the RX FIFO size). Data is then received and a callback will be triggered when data receive ends.
[2.1.4]#
Improvements
Changed parameter type in UART_RTOS_Init() struct rtos_uart_config –> uart_rtos_config_t.
Bug Fixes
Disabled UART receive interrupt instead of global interrupt when reading data from ring buffer. With ring buffer used, receive nonblocking will disable global interrupt to protect the ring buffer. This has a negative effect on other IPs using interrupt.
[2.1.3]#
New Features
Added RX framing error and parity error status check when using interrupt transfer.
[2.1.2]#
Bug Fixes
Fixed baud rate fine adjust bug to make the computed baud rate more accurate.
[2.1.1]#
Bug Fixes
Removed needless check of event flags and assert in UART_RTOS_Receive.
Always waited for RX event flag in UART_RTOS_Receive.
[2.1.0]#
Improvements
Added transactional API.
[2.0.0]#
Initial version.
UART_DMA#
[2.5.0]#
Refer UART driver change log 2.1.0 to 2.5.0
VREF#
[2.1.3]#
Improvements
Add timeout for APIs with dfmea issues.
[2.1.2]#
Bug Fixes
Fixed the violation of MISRA-2012 rule 10.3.
Fixed MISRA C-2012 rule 10.3, rule 10.4 violation.
[2.1.1]#
Bug Fixes
MISRA-2012 issue fixed.
Fixed rules containing: rule-10.4, rule-10.3, rule-10.1.
[2.1.0]#
Improvements
Added new functions to support L5K board: added VREF_SetTrim2V1Val() and VREF_GetTrim2V1Val() functions to supply 2V1 output mode.
[2.0.0]#
Initial version.
WDOG#
[2.0.3]#
Bug Fixes
Fixed CERT INT31-C violations in WDOG_Init, WDOG_Disable, WDOG_EnableInterrupts and WDOG_DisableInterrupts (MCUX-87729).
[2.0.2]#
Improvements
WDG_Init() adds a 256 bus clock delay for WCT window finish.
[2.0.1]#
Bug Fixes
MISRA C-2012 issue fixed: rule 10.3, 10.4, 10.6, 10.7 11.9 and 17.7.
[2.0.0]#
Initial version.
XBAR#
[2.1.1]#
Bug Fixes
Fixed CERT-C issues.
[2.1.0]#
Improvements
Improved to support XBAR which has less than 4 interrupt output.
Bug Fixes
Fixed violations of MISRA C-2012 rule 12.2.
[2.0.5]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules 10.1, 10.3, 10.4, 10.6, 10.7, 10.8, 12.2, 18.1, 20.7.
[2.0.4]#
Bug Fixes
Fixed IAR build warning Pa082.
[2.0.3]#
Improvements
Optimized XBAR_SetOutputSignalConfig.
[2.0.2]#
Bug Fixes
Corrected configuration for function XBAR_SetOutputSignalConfig.
[2.0.1]#
Bug Fixes
Fixed w1c bits for XBAR_SetOutputSignalConfig function.
[2.0.0]#
Initial version.