MCUXpresso SDK Documentation

pit

pit#

Overview#

The PIT project is a simple demonstration program of the SDK PIT driver. It sets up the PIT hardware block to trigger a periodic interrupt after every 1 second. When the PIT interrupt is triggered, a message will be printed on the UART terminal and an LED toggled on the board.

Supported Boards#